Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The real-time OS aware debugging presented herein supports task-level debugging of real-time OS applications in the Integrated Development Environment High-performance Embedded Workshop. This function comes standard with High-performance Embedded Workshop. There is no need to rebuild the real-time OS, nor will overhead be incurred. (Debug patches, etc. are not necessary.)

Features

  • Object status reference (OS object window)
  • Graphical display of task execution history (task trace window)
  • Graphical display of task execution time (task analyze window)
  • Functions for the E100 emulator
  • Learn more

Release Information

Target Devices

Type Title Date
Upgrade - OS
Log in to Download ZIP 197 KB 日本語
1 item
Type Title Date
Application Note PDF 750 KB 日本語
AI-generated Summary: Real-time OS aware debugging supports various real-time operating systems including HI7200/MP, ThreadX, uC/OS-II, and TOPPERS variants. It operates within High-performance Embedded Workshop on Windows platforms and integrates with SuperH Family RISC engine simulators/debuggers. The document details environment setup, program downloading, OS definition selection, task state monitoring, execution history, and timing display functions.
1 item

Functions

  • Object status reference (OS object window)
Image
hew-ecxos1-e
  • Allows you to inspect the execution status of objects such as tasks and semaphores
  • RAM monitor supported
  • Capable of a mixed display of multiple objects such as task priority and event flag value


When using Renesas real-time OSs, you can make use of extended debugger options that permit more detailed object status references (real-time OS debugger [Debugging Extension] task window, etc. and MR window of the PC7501 emulator, etc.). These windows include the items normally displayed in the OS object window. (The relationship between these windows and the OS object window is similar to the relationship between a watch window and local window.)

  • Graphical display of task execution history (task trace window)
    • Execution history display making use of trace data
Image
hew-tasc-trace-e
  • Graphical display of task execution time (task analyze window)
    • Execution time and CPU occupancy rate display making use of trace data
Image
hew-task-analyze-e
  • Functions for the E100 emulator
    • Real-time profile (shows the CPU occupancy rate over a long time without interruption)
    • Task specification for each condition (break, performance, trace and trace filter)
    • Currently executed task display in the status bar
    • Task execution history display in text form (execution history display making use of trace data)
    • Task stack coverage (graphical display of the task stack used)
    • Memory protection (illegal accesses to the task stack and OS area detected)
    • Step execution aiming at a specific task
    • Dispatch detection and break
Image
hew-ecxos2-e
Real-time Profile
Image
hew-ecxos3-e
Task Stack Coverage
Image
hew-ecxos4-e.
Memory Protection

Refer to the help file of the E100 emulator for more information about the functionality.

Function Relationship

[Real-time OS] Table 1

FunctionHI7200/MP,
HI7750/4,
HI7700/4,
HI7000/4
RI600/4M3T-MR30/4,
M3T-MR30
HI1000/4MR8C/4,
Smalight OS
OS object
Task trace
Task analyze
OS trace---
OS analyze---
Task step-
Currently executed task display-
Execution history display-
Realtime profile-
Task specification-
Stack coverage--
Memory protection-

-

Detection of dispatch-

[Real-time OS] Table 2

FunctionThreaX, TOPPERS/JSPembOSNORTi, uC/OSⅡ, uT-KernelosCAN, TOPPERS/ASPRTA-OSEK
OS object-
Task trace
Task analyze
OS trace-----
OS analyze-----
Task step-----
Currently executed task display--
Execution history display---
Realtime profile---
Task specification---
Stack coverage----
Memory protection

-

-

-

-

-

Detection of dispatch-----

[Debugger]

FunctionSimulatorE1E20E10A-USBE8aE100E200F
OS object
(RAM monitor supported2)

(RAM monitor supported)
Task trace55
(Large capacity2)
1-
(Large capacity)
Task analyze55
(Large capacity2)
1-
(Large capacity)
OS trace3----4-
OS analyze3----4-
Task step----
Currently executed task display----
Execution history display------
Real-time profile------
Task specification------
Stack coverage------
Memory protection------
Detection of dispatch------
  • 1. Use 36-pin or 38-pin cable. (14-pin cable can not use.) Time is not displayed. (except for SH2A-DUAL)
  • 2. Use 38-pin cable. (14-pin cable can not use.)
  • 3. apply only when Simulator debugger for RX family V.1.02.00 or later is in use.
  • 4. apply only when M16C R8C E100 Emulator Software V.1.03 Release 00 or later and M16C/60 or M16C/50 series are in use.
  • 5. apply only when E1 or E20 emulator debugger for RX family is in use.

Operating Environment

Corresponding Real-Time OS

Real-time OSMicrocontrollers
Renesas HI7200/MPV.1.00 Release 03 or laterSH2A-DUAL
Renesas HI7750/4V.2.02 Release 04 or laterSH-4, SH-4A
Renesas HI7700/4V.2.03 Release02 or laterSH4AL-DSP, SH-3, SH3-DSP
Renesas HI7000/4V.2.02 Release 04 or laterSH-2, SH2-DSP, SH-2A, SH-1
Renesas RI600/4V.1.00 Release 00 or laterRX Family
Renesas M3T-MR30/4V.4.00 Release 00 or laterM16C/60, M16C/50, M16C/30, M16C/20, M16C/10, M16C/Tiny Series
R8C Family
Renesas M3T-MR30V.3.30 Release 2 or laterM16C/60, M16C/50, M16C/30,M16C/20, M16C/10, M16C/Tiny Series
Renesas MR8C/4V.1.00 Release 00 or laterR8C Family
Renesas HI1000/4v1.05 Release01 or laterH8SX Family
H8S Family
Smalight OS made by Maxell System Tech Co., Ltd.V3.10 or laterSH-2, SH-2A
RX Family
M16C/Tiny, M16C/30 and M16C/60 Series
R8C Family
H8SX Family
H8S Family
H8 Family
ThreadX made by Express Logic, Inc.G5.1.5.0SH-2A
NORTi made by MiSPO Co., Ltd.Version4 Release 1.20SH-4A, SH-2A
Version4 Release 4.3GRX Family
Version4 Release 1.14H8SX Family
H8S Family
osCAN made by Vector Informatik GmbH.Version 3.05M16C/60, M16C/Tiny Series
RTA-OSEK made by ETAS Co., Ltd.Version 4.0.0SH-2A
uC/OS-II made by Micrium Inc.V.2.86 (AN-Renesas-SH7201)SH-2A
V.2.89RX Family
V2.83 (AN-1662)M16C/60 Series
V.2.86 (AN-Renesas-H8S2215R, AN-Renesas-H8S2472, AN-Renesas-H8SX1664)H8SX Family
H8S Family
embOS made by Microcontroller GmbH & Co. KGVersion 3.80gSH-2A
Version 3.82bRX Family
CMX-RTX made by CMX Systems Inc.Version 5.30RX Family
TRON Forum uT-Kernelv1.00.00M16C/62P Group
TOPPERS Project TOPPERS/ASPRelease 1.3.1SH-2A
Release 1.3.2M16C/60 Series
TOPPERS Project TOPPERS/JSPRelease 1.4.3H8/3048 Group
H8S/2350 Group

Corresponding Debuggers

DebuggerSupported microcontrollersSupported debugger version
Simulator debuggerSuperH FamilyV.9.08.00 or later
RX FamilyV.1.00.00 ot later
H8SX, H8S and H8 FamilyV.5.07.00 or later
E1 emulator debuggerRX Family, R8C FamilyV.1.00 Release 00 or later
E20 emulator debuggerRX Family, R8C FamilyV.1.00 Release 00 or later
E10A-USB emulatordebuggerSH-2A, SH-4A, SH4AL-DSP, H8SX Family,V.3.00 Release 00 or later
H8S Family
SH2A-DUAL, SH4A-MULTIV.2.00 Release 00
E8a emulator debuggerM16C Family, R8C Family, H8 FamilyV.1.02 Release 00 or later
E100 emulator debuggerRX Family, M16C Family, R8C Family,V.1.00 Release00 or later
H8SX Family
E200F emulator debuggerSH-2AV.3.00 Release 00

*. Please refer to the Emulator pages linked above to get to know the detailed supported MCUs.

Corresponding Compilers

*TRON Forum holds the copyright on the uITRON Specification and the uT-Kernel specifications.
*The OSEK/VDX steering committee holds the copyright on the OSEK/VDX specifications.
*TOPPERS is a registered trademark of TOPPERS Project.
*OSEK is a registered trademark of Siemens AG.
*ThreadX is a registered trademark of Express Logic, Inc.
*NORTi is a registered trademark of MiSPO Co., Ltd.
*osCAN is a registered trademark of Vector Informatik GmbH.
*RTA-OSEK is a registered trademark of LiveDevices Co., Ltd.
*Smalight is a registered trademark of Maxell System Tech Co., Ltd.
*uC/OS-II is a trademark of Micrium, Inc.
*embOS is a registered trademark of SEGGER Microcontroller GmbH & Co. KG.
*CMX-RTX is a trademark of CMX Systems Inc.
*The other system names and product names referred to in this document are trademarks or registered trademarks of the respective proprietary companies.
*TRON, ITRON, uITRON, uT-Kernel and OSEK/VDX do not refer to any specific product or products.

Design Support

High-performance Embedded Workshop Real-Time OS Aware Debugging Information for Users

Knowledge Base

  1. How to display time in task trace window and task analyze window?

    Time is not displayed if you use E10A-USB. (except SH2A-DUAL)

    Dec 7, 2009
  2. Why are Task trace window and task analyze window not displayed?

    E8a emulator does not support task trace window and task analyze window. Also if you use E10A-USB emulator with a cable for 14 pins connector, task trace window and task analyze window are not displayed.You can display task trace window when using a cable for 36 or 38 ...

    Dec 7, 2009