Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Renesas Flash Programmer V3

Topics

  • The Renesas Flash Programmer supports the new device RX14T.

Renesas Flash Programmer V3 provides usable and functional support for programming the on-chip flash memory of Renesas microcontrollers in each phase of development and mass production.

Features

  • A simple GUI makes operations easy, even for first-time developers
  • PC-controlled programming via the E2 emulator, E2 emulator Lite, E20 emulator, Segger J-Link debug probes, a serial or USB connection
  • Interoperation with other software.
    • The efficiency of work can be improved by, for example, writing data to many boards consecutively and retaining logs of the written data in files.
  • Auto-programming from the command line
    • In the mass-production phase, a programming instruction can be easily run repeatedly from the command line (rather than using the GUI) for efficient mass production.
  • Programming a unique code to a designated area of flash memory
  • Enhanced security against theft through the encryption of program files [Learn More]
  • Easier creation of projects (compared with V2) [Learn More]
    • Easy selection of type names. No need to select detailed type names for products of the RL78 family.
    • Easy setting of mode pins for RX family products.
  • Improvements in processing speed (compared with V2)
    • The programming time has been shortened by approximately 10 percent.
    • In the case of the RL78 family, programming times have been shortened by up to 50 percent.(These data were gathered under specific conditions, and we do not guarantee a specific increase in speed.)
  • Learn More

Release Information

Number of licensesOrderable part nameRelease dateDownload
1RTCZZZZZZFD0AWNJLatest Ver. : V3.23.00 
Released : Apr 20, 2026 
Details of upgrade (Tool News)
evaluation software
5RTCZZZZZZFD0AWNJ#L5

Note:

  1. Each license is for use of the software on a single PC.
  2. From V3.08.02, the free-of-charge edition and upgrade program of the Renesas Flash Programmer are consolidated in a single file for downloading that serves as the form of delivery for the evaluation software. You can download the evaluation software from this link whether you are trying out the Renesas Flash Programmer for the first time or are already using an older version of the Renesas Flash Programmer.
  3. V3.09.00 and later versions of the Renesas Flash Programmer are no longer provided on a CD-ROM as the medium. The type names for ordering have been changed to reflect this change in the product configuration.
  4. The function to activate/deactivate license has been removed from V3.09.00 and later versions of the Renesas Flash Programmer. In addition, the users are eligible to receive the technical support by showing the PID in the product license certificate.
     

Software Licenses and Technical Support

The Renesas Flash Programmer is available for download as free evaluation software. 
We do not provide technical support for the free version, so will not be able to answer any questions you may have regarding the evaluation software and send to our technical support center via the Renesas web site. 
If you require technical support, we recommend that you purchase a software license through one of our sales offices or distributors.

 Before purchasing a licenseAfter purchasing a license
Technical SupportNot availableAvailable
Function and PerformanceNo difference (Renesas Flash Programmer can be used not only for evaluation, but also for programming finished products through the product development.)

FAQ

See all related FAQs

See also Error Guide.

See Error Guide

Target Devices

Target Family

Note:

  1. The V3 does not support the V850 family, 78K0, and 78K0R. Use Renesas Flash Programmer V2 if you are using products of these families.
  2. For details of support for individual device part numbers, see List of MCUs supported by Renesas Flash Programmer V3 (PDF | English, 日本語).
Type Title Date
Software & Tools - Software
Log in to Download TGZ 48.35 MB 日本語
Software & Tools - Software
Log in to Download TGZ 49.76 MB 日本語
Software & Tools - Software
Log in to Download TGZ 50.91 MB 日本語
Software & Tools - Software
Log in to Download ZIP 96.23 MB 日本語
Software & Tools - Software
Log in to Download ZIP 49.38 MB 日本語
Software & Tools - Evaluation Software
Log in to Download ZIP 47.64 MB 日本語
Upgrade - Programmer
Log in to Download ZIP 47.64 MB 日本語
Upgrade - Debugger
Log in to Download ZIP 163 KB 日本語
8 items
Type Title Date
Manual - Development Tools PDF 1.48 MB 日本語
The Renesas Flash Programmer is a flash memory programmer for Mmicrocontrollers from Renesas Electronics. This manual describes Renesas Flash Programmer V3 functions, operations, troubleshooting, and precautions.
Flyer PDF 238 KB 日本語 , 简体中文
Release Note PDF 629 KB 日本語
This document covers release information on the Renesas Flash Programmer V3 products. It describes addition of supported devices, and improved functionality and change.
Manual - Development Tools PDF 145 KB 日本語
The Renesas Flash Programmer is a flash memory programmer for Mmicrocontrollers from Renesas Electronics. The microcontrollers, tools, interfaces, and selected product names supported by Renesas Flash Programmer V3 are listed.
Manual - Development Tools PDF 861 KB 日本語
The PG-FP6, Renesas Flash Programmer are flash memory programmer for Mmicrocontrollers from Renesas Electronics. This manual describes the recommended circuitry for connecting PG-FP6, Renesas Flash Programmer to the microcontroller.
Tool News - Note PDF 341 KB 日本語
This notice provides important information regarding the use of Renesas emulator products and flash memory programmer products equipped with a USB interface, as outlined below. 1. Products Not Affected by the Windows Driver Policy Change 2. Impact of the Windows Driver Policy Change on the E2 Emulator, E2 Emulator Lite, and IE850A, and Recommended Actions 3. Impact of the Windows Driver Policy Change on Other Emulator Products and Flash Memory Programmer Products
Tool News - Release PDF 153 KB 日本語
Application Note PDF 1.19 MB 日本語
This application note describes a library for controlling external flash memory connected to an RAmicrocontroller (hereafter referred to as “MCU”). By using the library introduced in this document, you canperform write and debug operations on the. external flash memory through an on-chip debugging emulator. A sample project named “r20an0822ref0100-ra-refl.zip” (hereinafter referred to as “the Sample Project”) isavailable to facilitate the use of External Flash Library
Tool News - Release PDF 151 KB 日本語
Tool News - Release PDF 140 KB 日本語
This is a tool news to announce the upgrade to revision to the Renesas Flash Programmer V3.21.00. It describes addition of supported devices, improved functionality and change, and updating the Product. The main upgrade to revision are RL78/L23 group support, support for block-level erasure of the flash memory on DA148xx devices, and addition of DA148xx devices as target devices for the [Create and write product/image headers] option.
Tool News - Release PDF 151 KB 日本語
Tool News - Release PDF 151 KB 日本語
Tool News - Release PDF 143 KB 日本語
Tool News - Release PDF 142 KB 日本語
Tool News - Release PDF 153 KB 日本語
Tool News - Release PDF 137 KB 日本語
Tool News - Release PDF 146 KB 日本語
Tool News - Release PDF 138 KB 日本語
Tool News - Release PDF 138 KB 日本語
Application Note PDF 541 KB 日本語
AI-generated Summary: The document explains how to perform debugging on RL78 microcontrollers using a USB-to-serial conversion adapter connected via the COM port. It details the connection setup, including signal line considerations such as RESET#, TOOL pins, GND, and power supply voltage. The guide covers securing MCU resources like debug monitor and stack areas, setting debug options, and managing reset behavior. It also describes debugging functions such as memory reference, breakpoints, trace functions, and communication baud rate adjustment. The document supports RL78 devices compatible with COM Port debugging and highlights practical usage notes for effective debugging.
Tool News - Release PDF 145 KB 日本語
Tool News - Release PDF 143 KB 日本語
Tool News - Featured Tool PDF 864 KB 日本語
Tool News - Release PDF 166 KB 日本語
Tool News - Notification PDF 502 KB 日本語
Manual - Development Tools PDF 206 KB
Tool News - Release PDF 163 KB 日本語
Tool News - Release PDF 143 KB 日本語
Tool News - Release PDF 202 KB 日本語
Tool News - Note PDF 143 KB 日本語
Tool News - Release PDF 104 KB 日本語
Tool News - Notification PDF 92 KB 日本語
Tool News - Release PDF 225 KB 日本語
Tool News - Release PDF 229 KB 日本語
Tool News - Note PDF 29 KB 日本語
Tool News - Release PDF 81 KB 日本語
Application Note PDF 328 KB 日本語
AI-generated Summary: The Renesas Flash Programmer (RFP) supports automated programming control via command lines, offering two methods: using project files on Windows and using rfp-cli on Windows and Linux. The document explains basic procedures for setting up programming with project files using an RL78/G14 MCU example, including system connection, project creation, and batch file execution. It details connecting the host PC to the tool, linking the target system, and configuring project settings such as MCU type, tool, interface, and power supply.
Tool News - Featured Tool PDF 193 KB 日本語
Tool News - Notification PDF 306 KB 日本語
Tool News - Notification PDF 304 KB 日本語
Tool News - Notification PDF 352 KB 日本語
Tool News - Notification PDF 29 KB 日本語
Tool News - Release PDF 83 KB 日本語
Tool News - Note PDF 118 KB 日本語
Tool News - Note PDF 147 KB 日本語
Application Note PDF 2.89 MB
Manual - Development Tools PDF 202 KB 日本語
Tool News - Note PDF 147 KB 日本語
Tool News - Note PDF 83 KB 日本語
Tool News - Release PDF 111 KB 日本語
Manual - Development Tools PDF 1.09 MB 日本語
Manual - Development Tools PDF 744 KB 日本語
Release Note PDF 164 KB 日本語
Tool News - Note PDF 41 KB 日本語
Tool News - Note PDF 119 KB 日本語
Manual - Development Tools PDF 874 KB 日本語
Manual - Development Tools PDF 1.13 MB 日本語
Tool News - Note PDF 202 KB 日本語
Tool News - Note PDF 204 KB 日本語
Tool News - Release PDF 316 KB 日本語
60 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 3.23 MB 日本語
Sample Code
[Software=RA Flexible Software Package|v6.3.0],[Toolchains=GNU Arm Embedded|13.2.rel1]
Log in to Download ZIP 22 KB Compiler: GNU ARM Embedded Function: Debugging, Emulator, Memory, Programmer IDE: e2 studio
2 items

Functions

  • Supported file formats for programming: Intel HEX for HEX and HCUHEX files, Motorola S for HEX and HCUHEX files, binary, and RPI for RPI file
  • Check sum of program files
  • Execute commands such as erase, writing, verification, read-out, setup and acquisition of flash options, and acquisition of checksum
  • Sequential execution of multiple commands (for erasure, programming, verification, etc.)
  • Multiple files for programming selectable simultaneously

 

 

Enhanced security against theft through the encryption of program files

The new function for encrypting program files enhances security against theft.   
You can run this function by using the encryption utility program (RPE.exe) from the command line. The file is among those installed by the Renesas Flash Programmer installer.

Image
rfp_key-en

 

 

Easier Creation of Projects

Easy selection of type names

No need to select detailed type names for products of the RL78 family.

Image
easyselection

Easy setting of mode pins for RX family products

No need for mode pin setting, when the recommended connection examples are used.

Image
easysetting

 

System Configuration

The system configuration in programming with Renesas Flash Programmer V3 is as follows.

Image
rfp_config202206-en

Note:

  1. The E1 emulator is also usable.
  2. Renesas Flash Programmer can use certain models of Segger J-Link to provide a serial communication with the boot mode functionality of RA Family MCUs. Please refer to the Renesas Flash Programmer Information for Users for applicable hardware, recommended firmware, appropriate debug connection to the target MCUs.

 

Target Devices by Connection Methods

For details, refer to the List of MCUs supported by Renesas Flash Programmer V3 (PDF | English, 日本語).

 Connections
Supported devicesThrough on-chip debugging emulators Note1Serial   
(RS-232C)
USB
E2 emulatorE2 emulator LiteE20 emulatorSegger   
J-Link debug probes
RAlenslens—lenslenslens   
MCUs with USB boot
RL78lenslenslensNote2—lens—
RXlenslenslens—lenslens   
MCUs with USB boot
RH850lens—lensNote2—lensNote2—
RISC-V MCU(R9A02G020, R9A06G150)————lens—
RISC-V MCU(R9A02G021)lenslens—lenslens—
Renesas Synergy————lenslens   
MCUs with USB boot
DA1453x, DA1459x, DA1469x, DA1470x, DA148xx———lens——
RElens———lenslens   
MCUs with USB boot
Battery Fuel Gauge ICslenslenslens—lens—
Renesas USB Power Deliverylenslenslens—lens—
ICs for Motor Driver/Actuator Driverlenslenslens—lens—

lens Available | — Not Available

Note:

  1. When using with the on-chip debugging emulators, conversion adapter is required depending on the number of pins on the target board.
  2. Some devices of this product family are not supported. For details, refer to the List of MCUs supported by Renesas Flash Programmer V3 (PDF | English, 日本語).

 

Information on the discontinuation of E1 emulator production and on its successor products

We have already discontinued production of the E1 emulator due to components of the product having reached their EOL (end of life, i.e. end of production). Please click on the following link to confirm the details and our successor products.

[Notification] End of Life (EOL) Notice for E1 Emulator (PDF | English, 日本語)

Support Communities

  1. PE-MHI and Renesas Flash Tools GUI

    I'have ordered a PE-MHI and want to use Renesas Flash Tools GUI to download example. Normaly the GUI should connect using the uart (or throught the jliink provided). when creating a new projet from the Flash Tools GUI, I only see a uart over Bluetooth. According to the ...

    Jan 15, 2018
  2. Enabling Renesas Flash Programmer for J Link

    Hi team, We are trying to flash the Renesas RA6M1 controller using J-Link with Renesas Flasher tool... But could not succeed in doing it.... Please find the error details mentioned below : Connecting the toolError(E30002FE): This tool is not supported.Operation failed. Kindly help us on how it solve ...

    Feb 21, 2023
  3. The Renesas Flash Programmer: Setting up the hardware and software

    ... Renesas Flash Programmer V3.03.00 Home Page: https://www.renesas.com/en-us/products/software-tools/tools/programmer/renesas-flash-programmer-programming-gui.htmlRenesas Flash Programmer V3.03.00 User’s Manual: https://www.renesas.com/en ...

    Nov 11, 2017
View All Results from Support Communities (339)

Knowledge Base

  1. CS+ Update Manager is Terminated While Updating is in Progress

    ... RLhttps://www.renesas.com/rl78-c-download CC-RHhttps://www.renesas.com/rh850-c-downloadSmart Configuratorhttps://www.renesas.com/software-tool/smart-configuratorRenesas Flash Programmerhttps://www.renesas.com/software-tool/renesas-flash-programmer-programming-gui# ...

    Mar 9, 2023
  2. eFLASHLOAD Error [0x0100]

    The E2 emulator is not supported by the eFlashLoad, and thus the error message. Could you use latest version of renesas flash programmer : Renesas Flash Programmer (Programming GUI) | Renesas to update the firmware. RFP cannot be used to update external serial flash. In that case you can use E1 Emulator ...

    Jan 18, 2024
  3. What support does the Synergy Platform offer for secure boot?

    https://www.renesas.com/us/en/software-tool/renesas-flash-programmer-programming-gui#documents    [Tags]   secure boot, boot, SSP,  RFP,  Synergy

View All Results from Knowledge Base (22)