Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Topics

  • The E2 emulator supports the new device RX14T.

The E2 emulator is an advanced on-chip debugging emulator and flash programmer developed with the concept of greater efficiency in development. The combination of its high-speed downloading and various software and hardware solutions will contribute to reducing development times.

Features

  • High-speed download up to twice as fast as E1
    The download speed is up to twice as fast as the E1 emulator. This substantially reduces waiting time for downloading the control programs to one-half at a maximum.
  • Hot plug-in function available without an optional adapter
    Although the E1 emulator required an optional hot plug adapter sold separately to use the hot plug-in function, the E2 emulator does not need it.
  • Board interface compatible with that of E1
    he E2 emulator can be connected to the user system that was designed for the E1 emulator because the pin arrangement to be connected to the user system has compatibility with the E1 emulator. [Learn More : the optional products for E2 ]
  • Support for new MCUs with next-generation cores
    MCUs that have next-generation cores, such as those of the RH850/E2x series (which incorporate the G4MH core) or the RX66T group (which incorporate the new RXv3 core for the RX family) can be debugged.
  • Features for for RL78 and RX Families
    • Support for the input and output of external triggers [Learn More: ToolNews]
      For example, you can set up the stopping of programs or of the measurement of waveforms by simply using the test lead which comes with the E2 emulator to connect the emulator to an external measuring instrument with the CS+ integrated development environment or the e² studio integrated development environment.
    • Current Consumption Tuning Solution
      In conjunction with the QE for Current Consumption, a dedicated tool for measuring current drawn, the E2 emulator is capable of the following items. These shorten the time taken to tune currents.
      • Measuring current with the E2 emulator alone
      • Stopping a program when an excessive current is detected
      • Visualizing the relationship between program operations and current
  • Features for RH850 Family  
    • CAN Communications Time Measurement Solution
      The following CAN-related tasks are possible in conjunction with the CS+ integrated development environment or the MULTI® integrated development environment (GHS MULTI) from Green Hills Software. This eases verifying the speed of CAN communications in terms of system requirements.
      • Measuring the reception processing time in CAN communications with the E2 emulator alone
      • Stopping a program when the reception processing time exceeds the design value
      • Visualizing the history of CAN communications
    • Support for the input and output of external triggers [Learn More: ToolNews]
      For example, you can set up the stopping of programs or of the measurement of waveforms by simply using the test lead which comes with the E2 emulator to connect the emulator to an external measuring instrument with the CS+ integrated development environment or the MULTI® integrated development environment (GHS MULTI) from Green Hills Software.
    • Software Trace Function [Learn More: ToolNews]
      The function enables users to view the execution history of the programs such as the values of the program counter (PC) and the register values together with the debug instructions of MCUs for RH850 family with the CS+ integrated development environment or the MULTI® integrated development environment (GHS MULTI) from Green Hills Software. Using this feature, unlike the conventional method of “tracing data with the settings of events and conditions,” users can generate the execution history data such as the PC values and register values simply by inserting the debug instructions to the location where you like to check in the program.his feature is available in all RH850 family MCUs, including the ones do not have internal trace memory when debugging.
  • Learn More

Release Information

See the latest Release Information of MCUs.

RA Family   RL78 Family   RX Family   RH850 Family   R-Car Family   RISC-V MCU

*Please contact Renesas sales division for RE Family.

 

Release Information for RA Family

The E2 emulator supports the RA8D2 and RA8M2 groups.
Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip Debugginge² studio(64-bit version) 2025-10Oct. 20, 2025Operating Environment
(32-bit version) V7.8.0Apr. 20, 2020
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025
Precautions when using "RA Family"
Please be aware that a User-system interface cable will need to be purchased separately to support RA device debug with E2 using 20-10 pins. Please see Optional Products for RA Family for details.

 

Release Information for RL78 Family

The E2 emulator supports the RL78/F25 group, next-generation super-low power automotive microcontrollers.
Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip DebuggingCS+ (CS+ for CC)V8.14.00Note1Jul. 22, 2025Operating Environment
e² studio(64-bit version) 2025-10Oct. 20, 2025
(32-bit version) V7.8.0Apr. 20, 2020
IAR Embedded WorkbenchA tool produced by Partner. For the details of support for E2, contact IAR Systems directly.
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025Operating Environment

Release Information for RX Family

The E2 emulator supports the new device RX261 group and RX260 group, Microcontrollers with Outstanding Power Efficiency, Advanced Touch Functions, and Security.
Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip DebuggingCS+ (CS+ for CC)V8.14.00Note1Jul. 22, 2025Operating Environment
e² studio(64-bit version) 2025-10Oct. 20, 2025
(32-bit version) V7.8.0Apr. 20, 2020
IAR Embedded WorkbenchA tool produced by Partner.  For the details of support for E2, contact IAR Systems directly.
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025Operating Environment

 

Release Information for RH850 Family

Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip DebuggingCS+ (CS+ for CC)V8.14.00Note1Jul. 22, 2025Operating Environment
e² studio(64-bit version) 2025-10Oct. 20, 2025
(32-bit version) V7.8.0Apr. 20, 2020
IAR Embedded WorkbenchA tool produced by Partner.  For the details of support for E2, contact IAR Systems directly.
Green Hills MultiA tool produced by Partner. For the details of support for E2, contact Green Hills Software directly.
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025Operating Environment

 

Release Information for R-Car Family

Purpose of useSoftware to be used
On-chip Debugginge² studio for R-CarNote1

Note

  1. e² studio for the R-Car family is included in the RoX Software Development Kit (SDK).

Release Information for RISC-V MCU

Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip Debugginge² studio(64-bit version) 2025-10Oct. 20, 2025Operating Environment
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025
Precautions when using "RISC-V MCU"
Please be aware that a User-system interface cable will need to be purchased separately to support RISC-V MCU device debug with E2 using 20-10 pins. Please see Optional Products for RISC-V MCU for details.

 

FAQ

See all related FAQs

Target Devices

Type Title Date
Software & Tools - Other
Log in to Download ZIP 3.48 MB 日本語
Software & Tools - Other
Log in to Download ZIP
Upgrade - IDE
Log in to Download ZIP 3.25 MB 日本語
Upgrade - IDE
Log in to Download ZIP 3.09 MB 日本語
Upgrade - Programmer
Log in to Download ZIP 730 KB 日本語
5 items
Type Title Date
Flyer PDF 400 KB 日本語 , 简体中文
Manual - Development Tools PDF 1.09 MB 日本語
This document is the User's Manual for the Renesas E2 emulator. It is intended for developers who use the E2 emulator for program debugging. The manual explains the product specifications, system configuration, connection methods, and usage limitations. It covers the scope required to understand the hardware characteristics and how the E2 emulator is connected and used within its supported environment.
Tool News - Note PDF 341 KB 日本語
This notice provides important information regarding the use of Renesas emulator products and flash memory programmer products equipped with a USB interface, as outlined below. 1. Products Not Affected by the Windows Driver Policy Change 2. Impact of the Windows Driver Policy Change on the E2 Emulator, E2 Emulator Lite, and IE850A, and Recommended Actions 3. Impact of the Windows Driver Policy Change on Other Emulator Products and Flash Memory Programmer Products
Manual - Development Tools PDF 230 KB 日本語
This is a feature list summarizing the capabilities of Renesas' on-chip debuggers for each microcontroller. For the E2 Emulator, E2 Emulator Lite, E1 Emulator, E20 Emulator, MINICUBE2, E10A-USB, and E8a on-chip debuggers, it details the debugging capabilities supported for each corresponding microcontroller, including connection methods, break functions, trace functions, and more.
Manual - Development Tools PDF 2.27 MB 日本語
This is the user's manual for the adapter that converts the user-system interface cable for the E2 emulator into a 14-pin, 2.54 mm pitch connector for connection to the target board. This manual contains information on the appearance, package contents, specifications, and usage.
Manual - Development Tools PDF 1.11 MB 日本語
This is the user's manual for the adapter that converts the 14-pin connector for connecting the emulator's user-system interface cable to a 34-pin external trace connector when using the Emulation Adapter for the RH850 Family. This manual contains information on the appearance, package contents, specifications, etc.
Manual - Development Tools PDF 2.28 MB 日本語
This is the user's manual for the user-system interface cable used to connect the E2 emulator to the 20-pin connector on the target board. This cable can also be used with the E2 emulator Lite and PG-FP6, and is included as standard with the E2 emulator. This manual describes the appearance, package contents, specifications, and usage instructions.
Manual - Development Tools PDF 2.26 MB 日本語
This is the user's manual for the user-system interface cable used to connect the E2 emulator to the 10-pin connector on the target board. This cable can also be used with the E2 emulator Lite and PG-FP6. This manual contains information on the appearance, package contents, specifications, and usage.
Application Note PDF 1.19 MB 日本語
This application note describes a library for controlling external flash memory connected to an RAmicrocontroller (hereafter referred to as “MCU”). By using the library introduced in this document, you canperform write and debug operations on the. external flash memory through an on-chip debugging emulator. A sample project named “r20an0822ref0100-ra-refl.zip” (hereinafter referred to as “the Sample Project”) isavailable to facilitate the use of External Flash Library
Manual - Development Tools PDF 881 KB 日本語
This is a supplementary manual to the emulator user's manual, summarizing important notes when debugging the RH850/U2B-E series using the E2 emulator, IE850A. It covers connection methods to the user system, functional overview, and usage precautions.
Tool News - Note PDF 154 KB 日本語
Tool News - Note PDF 209 KB 日本語
Application Note PDF 1.87 MB 日本語
AI-generated Summary: This document explains how to port projects from CS+ to e2 studio for the Renesas RX family using emulators such as E2 Lite, E2, and E20. It details the differences in emulator settings, connection configurations, and debugging operations within e2 studio. Users learn how to open CS+ projects in e2 studio, configure emulator connections via the Debug Configurations window, and manage target devices. The document covers debugging features including breakpoints, tracing, memory and register manipulation, and performance measurements, facilitating smooth migration and effective debugging in the e2 studio environment.
Manual - Development Tools PDF 2.03 MB 日本語
Manual - Development Tools PDF 1.99 MB 日本語
Tool News - Note PDF 259 KB 日本語
Tool News - Featured Tool PDF 864 KB 日本語
Tool News - Notification PDF 502 KB 日本語
Tool News - Release PDF 205 KB 日本語
Manual - Development Tools PDF 511 KB 日本語
Tool News - Note PDF 142 KB 日本語
Tool News - Note PDF 183 KB 日本語
Tool News - Release PDF 176 KB 日本語
Tool News - Featured Tool PDF 193 KB 日本語
Tool News - Notification PDF 306 KB 日本語
Tool News - Notification PDF 304 KB 日本語
Tool News - Notification PDF 352 KB 日本語
Tool News - Release PDF 92 KB 日本語
Tool News - Featured Tool PDF 260 KB 日本語
Tool News - Note PDF 141 KB 日本語
Tool News - Note PDF 156 KB 日本語
Application Note PDF 1.17 MB 日本語
AI-generated Summary: Main-core debugging enables secure development by separating secure programs running on the ICU-M core from non-secure programs on the main CPU core. It allows debugging of non-secure user programs while keeping secure information confidential. The method uses the E1/E20/E2/IE850A emulator and requires specific system configurations and authentication procedures. Key terminology includes integrated development environment, emulator debugger, host machine, target device, and user system. Manuals for the emulator provide hardware specifications, connection details, and usage notes essential for effective debugging.
Application Note PDF 1.17 MB 日本語
AI-generated Summary: Debugging methods focus on devices with an initially stopped CPU core and those transitioning to standby modes to optimize power consumption. Key capabilities include verifying core activation, measuring execution times for core activation and standby transitions, and restarting debugging at critical points such as core activation or MCU wake-up. Supported devices include various RH850 series MCUs. The document details environment setup, debugging configurations in CS+ and MULTI IDEs, and specific debugging techniques for different standby modes. It also covers precautions and terminology related to debugging and device operation.
Manual - Development Tools PDF 1.17 MB 日本語
Tool News - Note PDF 243 KB 日本語
Manual - Development Tools PDF 647 KB 日本語
Tool News - Note PDF 150 KB 日本語
Tool News - Note PDF 159 KB 日本語
Tool News - Note PDF 92 KB 日本語
Application Note PDF 2.25 MB 日本語
Application Note PDF 1.82 MB 日本語
Tool News - Note PDF 127 KB 日本語
Application Note PDF 2.09 MB 日本語
AI-generated Summary: The document details a CAN communication time measurement solution using the E2 emulator and CS+ integrated development environment. It explains the setup, usage, and notes for measuring CAN bus communication processing times. The solution enables halting program execution when processing time exceeds a set value, aiding early diagnosis by reviewing trace data and communication history. It also defines key terms related to the emulator and development environment.
Application Note PDF 2.07 MB 日本語
Application Note PDF 1.91 MB 日本語
Manual - Development Tools PDF 340 KB 日本語
Manual - Development Tools PDF 954 KB
Manual - Development Tools PDF 1.12 MB
Manual - Development Tools PDF 1.07 MB
Manual - Development Tools PDF 821 KB
Tool News - Release PDF 128 KB 日本語
Manual - Development Tools PDF 683 KB 日本語
Manual - Development Tools PDF 327 KB 日本語
Manual - Development Tools PDF 1.73 MB 日本語
Application Note PDF 573 KB 日本語
AI-generated Summary: The guide addresses common startup issues with the E1/E20 On-Chip Debugging Emulator. It explains warning messages about project file restoration due to version mismatches in CubeSuite+ and advises upgrading to the latest version. It highlights errors caused by missing CC-RX compiler installations and instructs users to install the compiler. The guide also details handling version differences in the CC-RX compiler, allowing debugging to continue if compatible or requiring version adjustments via the property panel.
Manual - Development Tools PDF 2.54 MB 日本語
Manual - Development Tools PDF 178 KB 日本語
Application Note PDF 525 KB 日本語
AI-generated Summary: The External Flash Definition Editor (EFE) enables creation of custom write programs for flash memory devices with unsupported command sets. Users customize sample C source programs, link header and library files, then create RFD and USD files for use with emulator software. The custom program must not exceed 8,192 bytes in memory size and 256 bytes in stack size. The development environment requires specific sample files, a suitable C/C++ compiler, and emulator tools.
Manual - Development Tools PDF 140 KB 日本語
59 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 3.23 MB 日本語
Sample Code
[Software=RA Flexible Software Package|v6.3.0],[Toolchains=GNU Arm Embedded|13.2.rel1]
Log in to Download ZIP 22 KB Compiler: GNU ARM Embedded Function: Debugging, Emulator, Memory, Programmer IDE: e2 studio
Sample Code
Log in to Download ZIP 566 KB 日本語
3 items
Part NumberStatusStockBudgetary Price (USD)Description
RTE0T00020KCAC1000JActiveIn Stock1ku | $25.88User-system Interface Cable for the E2 Emulator(20-10 pins)
RTE0T00020KCE00000RActiveIn Stock1ku | $445.88E2 Emulator

Specifications

The supported facilities differ with the integrated development environment you are using.

ItemDescription
  • Method of connection
  • Break function
  • Tracing
  • Reference to and changing memory contents while a program runs
  • Performance measurement
  • Hot plug-in
Since the method of connection and the functions may differ with the device you are using, refer to On-Chip Debugger Functional Overview (PDF | English, 日本語).
On-board programmingSupported
User interfaces14pin 2.54mm pitch connector
(7614-6002: from 3M Japan, 2514-6002: from 3M Limited)
20pin 1.27mm pitch connector
(FTSH-110-01-L-DV-K: from Samtec)
10pin 1.27mm pitch connector
(FTSH-105-01-L-DV-K: from Samtec, FTSH-105-01-L-DV: from Samtec without a marking for matching the position of the connector; keying shroudNote1)
PC InterfaceUSB 2.0, full speed and high speed
Connection to the systemConnection to the system is via the user system interface cable which comes with the product (signals for connection vary with the type of the target MCU).
Operating voltage range1.8V to 5.5V (depends on the target MCU)
Power supply from EmulatorSupply current: Up to 200mA, Supply voltage: 1.8V to 5.0V
External dimensions
(except for the protruding parts)
105.9 mm×64.0 mm×19.5 mm
Compliance with overseas standardsEuropean Standards: EN 55022 Class A, EN 55024
US FCC Standard: FCC part 15 Class A

Note

  1. When using a connector without a guide marking (keying-shroud type), take care with regard to the direction for insertion of the cable.

 

Components

E2 Emulator Body

USB interface cable
*Bundled

Test lead
*Bundled

User system interface cable 20-20 pins
*Bundled

Conversion adapter 20 to 14 pins
*Bundled

Please be aware that a User-system interface cable will need to be purchased separately to support RA device or RISC-V MCU debug with E2 using 20-10 pins. Please see Optional Products for RA Family or Optional Products for RISC-V MCU for details.

Purchasing FAQ : Which user-system interface cable should be purchased when introducing an emulator? (E2 Lite/E2)

 

System Configuration

Image
Image

Refer to the Release Information in this page for information of software on PC.

Note

  1. Connection to the 20-pin connector of the E2 emulator is not supported. Use the 20-pin to 14-pin conversion adapter that comes with the E2 for connection to the 14-pin connector on the user system.

 

 

Optional Products

The following optional products are provided to facilitate the use of the E2 emulator in various ways. Please check which products are supported by your MCU..

RA Family   RL78 Family   RX Family   RH850 Family   R-Car Family   RISC-V MCU

  • Please contact Renesas sales division for RE Family.
  • Please read references to "E1 emulator" in the manuals for optional products as also meaning "E2 emulator".

 

Optional Products for RA Family

TypeDescriptionProduct name / Manual
User-system Interface CableThis cable is used to connect the E2 emulator. It can also be used for the E2 emulator Lite and PG-FP6.User-system Interface Cable for the E2 Emulator (20-20 pins)
RTE0T00020KCAC0000J (Bundled with the E2 Emulator)
RTE0T00020KCAC0000J User's Manual User-system Interface Cable for the Emulator (20-20 pins) (PDF | English, 日本語)
User-system Interface Cable for the E2 Emulator (20-10 pins)
RTE0T00020KCAC1000J
RTE0T00020KCAC1000J User's Manual User-system Interface Cable for the Emulator(20-10 pins) (PDF | English, 日本語)
IsolatorEnables debugging in environments where the grounds of the user system and the host PC are not the same.Isolator for the E2 Emulator (E2 Emulator Lite) of RA/RE
RTE0T00020KCAA0000J
RTE0T00020KCAA0000J User's Manual (Isolator for E2 Emulator) (PDF | English, 日本語)

 

Optional Products for RL78 Family

TypeDescriptionProduct name / Manual
User-system Interface CableThis cable is used to connect the E2 emulator. It can also be used for the E2 emulator Lite and PG-FP6.User-system Interface Cable for the E2 Emulator (20-20 pins)
RTE0T00020KCAC0000J (Bundled with the E2 Emulator)
RTE0T00020KCAC0000J User's Manual User-system Interface Cable for the Emulator (20-20 pins) (PDF | English, 日本語)
Conversion AdapterConverts the number and pitch of pins of the connector for connecting the emulator.Small Connector Conversion Adapter for the E1 Emulator
R0E000010CKZ11
R0E000010CKZ11 User's Manual (Small Connector Conversion Adapter for E1 Emulator) (PDF | English, 日本語)
20-Pin to 14-Pin Conversion Adapter for the E2 Emulator
RTE0T00020KCA00000R (Bundled with the E2 Emulator)
RTE0T00020KCA00000R User's Manual (20-Pin to 14-Pin Conversion Adapter for the E2 emulator) (PDF | English, 日本語)
IsolatorEnables debugging in environments where the grounds of the user system and the host PC are not the same.Isolator for the E1 Emulator
R0E000010ACB20
R0E000010ACB20 User's Manual (Isolator for E1 Emulator) (PDF | English, 日本語)
Low voltage OCD BoardNote1Enables debugging of an MCU with a power-supply voltage such that the on-chip flash ROM cannot be reprogrammed.This product is used between the emulator and a user's system, and is united by the in-circuit connection with the user's system.Low voltage OCD Board for RL78/G10 (10-pin/16-pin)
R0E510Y47LVB00
Low voltage OCD Board for RL78/G10 (10pin, 16pin) Rev.1.00 (PDF | English, 日本語)
An OCD board for debugging an RL78/G10 MCU (10-pin or 16-pin) with an adapter voltage below 4.5 V

Note

  1. Target device: RL78/G10

 

Optional Products for RX Family

TypeDescriptionProduct name / Manual
User-system Interface CableThis cable is used to connect the E2 emulator. It can also be used for the E2 emulator Lite and PG-FP6.User-system Interface Cable for the E2 Emulator (20-20 pins)
RTE0T00020KCAC0000J (Bundled with the E2 Emulator)
RTE0T00020KCAC0000J User's Manual User-system Interface Cable for the Emulator (20-20 pins) (PDF | English, 日本語)
Conversion AdapterConverts the number and pitch of pins of the connector for connecting the emulator.14-Pin to 38-Pin Conversion Adapter for the E1 Emulator
R0E000010CKZ00
R0E000010CKZ00 User's Manual (14-Pin to 38-Pin Conversion Adapter for E1 Emulator) (PDF | English, 日本語)
An adapter for converting the 14-pin/2.54-mm pitch connector on the head of the emulator user interface cable to a 38-pin/0.5-mm pitch connector
Small Connector Conversion Adapter for the E1 Emulator
R0E000010CKZ11
R0E000010CKZ11 User's Manual (Small Connector Conversion Adapter for E1 Emulator) (PDF | English, 日本語)
20-Pin to 14-Pin Conversion Adapter for the E2 Emulator
RTE0T00020KCA00000R (Bundled with the E2 Emulator)
RTE0T00020KCA00000R User's Manual (20-Pin to 14-Pin Conversion Adapter for the E2 emulator) (PDF | English, 日本語)
IsolatorEnables debugging in environments where the grounds of the user system and the host PC are not the same.Isolator for the E1 Emulator
R0E000010ACB10
R0E000010ACB10 User's Manual (Isolator for E1 Emulator) (PDF | English, 日本語)

 

Optional Products for RH850 Family

TypeDescriptionProduct name / Manual
User-system Interface CableThis cable is used to connect the E2 emulator. It can also be used for the E2 emulator Lite and PG-FP6.User-system Interface Cable for the E2 Emulator (20-20 pins)
RTE0T00020KCAC0000J (Bundled with the E2 Emulator)
RTE0T00020KCAC0000J User's Manual User-system Interface Cable for the Emulator (20-20 pins) (PDF | English, 日本語)
Conversion AdapterConverts the number and pitch of pins of the connector for connecting the emulator.Small Connector Conversion Adapter for the E1 Emulator
R0E000010CKZ11
R0E000010CKZ11 User's Manual (Small Connector Conversion Adapter for E1 Emulator) (PDF | English, 日本語)
20-Pin to 14-Pin Conversion Adapter for the E2 Emulator
RTE0T00020KCA00000R (Bundled with the E2 Emulator)
RTE0T00020KCA00000R User's Manual (20-Pin to 14-Pin Conversion Adapter for the E2 emulator) (PDF | English, 日本語)
14-Pin to 34-Pin Conversion Adapter for E2 emulator
RTE0T00020KCA30000J
RTE0T00020KCA30000J 14-Pin to 34-Pin Conversion Adapter (PDF | English, 日本語)
Conversion Adapter included with Emulation Adapters
IsolatorEnables debugging in environments where the grounds of the user system and the host PC are not the same.Isolator for the E1 Emulator
R0E000010ACB20
R0E000010ACB20 User's Manual (Isolator for E1 Emulator) (PDF | English, 日本語)
Debug MCU Board / Emulation AdapterEnables the in-circuit connection of the emulator with the user's system. Enables the use of enhanced debugging functions.Debug MCU Board for RH850 
Supported devices for Debug MCU Board for RH850 Family [On-chip Debugger] (PDF | English, 日本語)
This board enables use of the trace function even if the target MCU does not have a trace function. The Debug MCU Board is for use in combination with a separately available 176-pin (with internal trace function) MCU of the RH850/F1L group.
Emulation Adapter for RH850 
List of Emulation Adapter for RH850 Family (PDF | English, 日本語)
This is an adapter mounting an emulation chip for G4MH Core RH850-family devices. In emulation of the device as a stand-alone unit, the internal tracing RAM is supported. Note that the E2 emulator does not support tracing via an Aurora interface.

 

Optional Products for R-Car Family

TypeDescriptionProduct name / Manual
Conversion AdapterConverts the number and pitch of pins of the connector for connecting the emulator.20-Pin(1.27mm) to 20-Pin(2.54mm) Conversion Adapter for the E2 Emulator
RTE0T00020KCA10000R
RTE0T00020KCA10000R User's Manual (20-Pin (1.27-mm Pitch) to 20-Pin (2.54-mm Pitch) Connector Conversion Adapter for the E2 Emulator (PDF | English, 日本語)
An adapter for converting the 20-pin/1.27-mm pitch connector on the head of the emulator user interface cable to a 20-pin/2.54-mm pitch connector

 

Optional Products for RISC-V MCU Family

TypeDescriptionProduct name / Manual
User-system Interface CableThis cable is used to connect the E2 emulator. It can also be used for the E2 emulator Lite and PG-FP6.User-system Interface Cable for the E2 Emulator (20-20 pins)
RTE0T00020KCAC0000J (Bundled with the E2 Emulator)
RTE0T00020KCAC0000J User's Manual User-system Interface Cable for the Emulator (20-20 pins) (PDF | English, 日本語)
User-system Interface Cable for the E2 Emulator (20-10 pins)
RTE0T00020KCAC1000J
RTE0T00020KCAC1000J User's Manual User-system Interface Cable for the Emulator(20-10 pins) (PDF | English, 日本語)

 

Design Support

E2 emulator [RTE0T00020KCE00000R] Information for Users

Support Communities

  1. E2 emulator

    Hi, I was using E2 emulator in my test system project.  i have 3 number E2 emulator in my hand. i am try to flash with E2 emulator only one Emulator is properly working. other 2 emulator is not flashing properly. in that Renesas programmer says below error so if ...

    Feb 23, 2024
  2. E2 Self Check FAILED (error 2200)

    Hello Team, My E2 Self Check FAILED with below error, what could be the problem? *** E2 Self Check Program Log *** [Emulator] E2 [Serial Number] 3CS014456D [EML Board Ver.] 05 [E2_SCP Ver.] 1.02.00.000 [RFW Ver.] 1.01.00.000 [BFW Level0 Ver.] 1.06.00.000 [BFW ...

    Jul 17, 2025
  3. Regarding choosing a emulators and debuggers for the development boards

    Hi ,This is Amar and I am totally new to  Renesas.I am working for a project which requires Renesas MCU and I wanted to get a clarification for purchasing emulators and debuggers for the following Renesas development boards.1.Renesas RL78/G13  2.Renesas RA4M2 development board and ...

    Jun 30, 2025
View All Results from Support Communities (14)

Knowledge Base

  1. Why Does the Emulator Not Start on a Lower Power Supply Voltage? (E2, E2 Lite, E1) [RL78]

    The possible cause is that the reset of the RL78 is not released because the LVD voltage set by the option bytes of the RL78 mounted on the target is higher than the new voltage. Start the emulator with the higher power supply voltage that was previously used. Then, write ...

    Jun 13, 2022
  2. Error message: After connecting E1 emulator to RX MCU in CS+. (E2, E2 Lite, E1, E20)

    This error message is displayed when the MCU is in the reset state and the RES# pin of the emulator connection connector is high. Check that the correct voltage is being supplied to the MCU (e.g. 3.3 V is not being input to an MCU which operates ...

    Mar 3, 2021
  3. Unable to debug or write using the E2 Emulator (E2, E2 Lite, E1)

    Check the switch of the 20-pin (1.27-mm pitch)/14-pin (2.54-mm pitch) connector conversion adapter. When using RH850, RX, set the switch to“1”. When using RL78, set the switch to “3”.

    Mar 8, 2021
View All Results from Knowledge Base (53)