Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Topics

  • The E2 emulator Lite supports the new device RX14T.

The E2 emulator Lite (abbreviated as "E2 Lite") is an on-chip debugging emulator and flash programmer for MCUs of the RX, RA, RL78 families and RISC-V MCU.
The E2 Lite offers basic debugging facilities at a low price and is also usable for actual development. This emulator is suitable for various purposes, ranging from education and initial evaluation to professional development.
You can also use the E2 Lite with optional products for the E1 emulator (such as the hot-plug adapter).
Refer to the respective links for more information below
Components | Optional Products (Cables sold separately, etc)

Features

  • Affordable yet powerful debugger functionality that meets actual development needs
    Learn more about the on-chip debugger functionality
  • Optional products that will shorten your debugging periods
    We offer various optional products including a hot-plug adapter, which can be used to connect the E2 Lite to a user system even while the system is running a program.
  • Also usable as an on-board programmer
    You can use the E2 Lite as an on-board programmer on completion of debugging. This will enable smoother evaluation of the MCU in stand-alone operation.
  • Supports serial, JTAG, and SWD communications interfaces
    The E2 Lite can be connected to the MCU through a serial, JTAG, or SWD communications interface.
  • Learn More

Release Information

See the latest Release Information of MCUs.

RA Family   RL78 Family   RX Family   RISC-V MCU

*Please contact Renesas sales division for RE Family.

 

Release Information for RA Family

The E2 emulator Lite supports the RA8D2 and RA8M2 groups.
Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip Debugginge² studio(64-bit version) 2025-10Oct. 20, 2025Operating Environment
(32-bit version) V7.8.0Apr. 20, 2020
Arm Keil MDK
cloud_download Renesas RA family E2 Lite Debug Driver for Keil uVision V1.00 (ZIP | English, 日本語) required.
A tool produced by Partner. For the details of Keil MDK, contact Arm directly
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025Operating Environment
Precautions when using "RA Family"
Please be aware that a User-system interface cable will need to be purchased separately to support RA device debug with E2 Lite using either 20-20 pins or 20-10 pins. Please see Optional Products for RA Family for details.

 

Release Information for RL78 Family

The E2 emulator Lite supports the RL78/F25 group, next-generation super-low power automotive microcontrollers.
Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip DebuggingCS+ (CS+ for CC)V8.14.00Note1Jul. 22, 2025Operating Environment
e² studio(64-bit version) 2025-10Oct. 20, 2025
(32-bit version) V7.8.0Apr. 20, 2020
IAR Embedded WorkbenchA tool produced by Partner. For the details of support for E2 Lite, contact IAR Systems directly.
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025Operating Environment

 

Release Information for RX Family

The E2 emulator Lite supports the new device RX261 group and RX260 group, Microcontrollers with Outstanding Power Efficiency, Advanced Touch Functions, and Security.
Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip DebuggingCS+ (CS+ for CC)V8.14.00Note1Jul. 22, 2025Operating Environment
e² studio(64-bit version) 2025-10Oct. 20, 2025
(32-bit version) V7.8.0Apr. 20, 2020
IAR Embedded WorkbenchA tool produced by Partner.  For the details of support for E2 Lite, contact IAR Systems directly.
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025Operating Environment

 

Release Information for RISC-V MCU

Purpose of useSoftware to be usedLatest VersionReleasedOperating Environment
On-chip Debugginge² studio(64-bit version) 2025-10Oct. 20, 2025Operating Environment
Flash ProgrammingRenesas Flash Programmer V3V3.21.00Oct. 20, 2025
Precautions when using "RISC-V MCU"
Please be aware that a User-system interface cable will need to be purchased separately to support RA device debug with E2 Lite using either 20-20 pins or 20-10 pins. Please see Optional Products for RISC-V MCU for details.

FAQ

See all related FAQs

Target Devices

Target Family

Precautions when using "RA Family" and "RISC-V MCU"
Please be aware that a User-system interface cable will need to be purchased separately to support RA device debug with E2 Lite using either 20-20 pins or 20-10 pins. Please see Optional Products for RA Family or Optional Products for RISC-V MCU for details.
Type Title Date
Upgrade - Debugger
Log in to Download ZIP 6.54 MB 日本語
Software & Tools - Other
Log in to Download ZIP
Software & Tools - Other
Log in to Download ZIP 4.91 MB 日本語
Upgrade - IDE
Log in to Download ZIP 3.25 MB 日本語
Upgrade - IDE
Log in to Download ZIP 3.09 MB 日本語
5 items
Type Title Date
Flyer PDF 205 KB 日本語 , 简体中文
Manual - Development Tools PDF 842 KB 日本語
Tool News - Note PDF 341 KB 日本語
This notice provides important information regarding the use of Renesas emulator products and flash memory programmer products equipped with a USB interface, as outlined below. 1. Products Not Affected by the Windows Driver Policy Change 2. Impact of the Windows Driver Policy Change on the E2 Emulator, E2 Emulator Lite, and IE850A, and Recommended Actions 3. Impact of the Windows Driver Policy Change on Other Emulator Products and Flash Memory Programmer Products
Manual - Development Tools PDF 230 KB 日本語
This is a feature list summarizing the capabilities of Renesas' on-chip debuggers for each microcontroller. For the E2 Emulator, E2 Emulator Lite, E1 Emulator, E20 Emulator, MINICUBE2, E10A-USB, and E8a on-chip debuggers, it details the debugging capabilities supported for each corresponding microcontroller, including connection methods, break functions, trace functions, and more.
Manual - Development Tools PDF 2.28 MB 日本語
This is the user's manual for the user-system interface cable used to connect the E2 emulator to the 20-pin connector on the target board. This cable can also be used with the E2 emulator Lite and PG-FP6, and is included as standard with the E2 emulator. This manual describes the appearance, package contents, specifications, and usage instructions.
Manual - Development Tools PDF 2.26 MB 日本語
This is the user's manual for the user-system interface cable used to connect the E2 emulator to the 10-pin connector on the target board. This cable can also be used with the E2 emulator Lite and PG-FP6. This manual contains information on the appearance, package contents, specifications, and usage.
Application Note PDF 1.19 MB 日本語
This application note describes a library for controlling external flash memory connected to an RAmicrocontroller (hereafter referred to as “MCU”). By using the library introduced in this document, you canperform write and debug operations on the. external flash memory through an on-chip debugging emulator. A sample project named “r20an0822ref0100-ra-refl.zip” (hereinafter referred to as “the Sample Project”) isavailable to facilitate the use of External Flash Library
Tool News - Note PDF 154 KB 日本語
Tool News - Note PDF 209 KB 日本語
Application Note PDF 1.87 MB 日本語
AI-generated Summary: This document explains how to port projects from CS+ to e2 studio for the Renesas RX family using emulators such as E2 Lite, E2, and E20. It details the differences in emulator settings, connection configurations, and debugging operations within e2 studio. Users learn how to open CS+ projects in e2 studio, configure emulator connections via the Debug Configurations window, and manage target devices. The document covers debugging features including breakpoints, tracing, memory and register manipulation, and performance measurements, facilitating smooth migration and effective debugging in the e2 studio environment.
Application Note PDF 1.05 MB 日本語
AI-generated Summary: The hot plug-in function enables debugging of an RL78 microcontroller during system operation without resetting or modifying the program. It retains failure status, uses ID code authentication for security, and allows RAM monitoring via a dedicated Data Transfer Controller (DTC) without stopping the CPU. Debugging proceeds through Real-time RAM Monitor (RRM) and Dynamic Memory Modification (DMM), accessing RAM, SFRs, and other memory areas. The debugging procedure involves creating a program with hot plug-in initialization, setting build options, programming via Renesas Flash Programmer, connecting with the E1 emulator, and performing debugging.
Tool News - Note PDF 259 KB 日本語
Tool News - Featured Tool PDF 864 KB 日本語
Tool News - Notification PDF 502 KB 日本語
Tool News - Release PDF 205 KB 日本語
Manual - Development Tools PDF 511 KB 日本語
Tool News - Note PDF 142 KB 日本語
Tool News - Note PDF 183 KB 日本語
Tool News - Featured Tool PDF 193 KB 日本語
Tool News - Notification PDF 306 KB 日本語
Tool News - Notification PDF 304 KB 日本語
Tool News - Notification PDF 352 KB 日本語
Tool News - Release PDF 83 KB 日本語
Tool News - Note PDF 150 KB 日本語
Tool News - Note PDF 147 KB 日本語
Tool News - Note PDF 92 KB 日本語
Tool News - Note PDF 127 KB 日本語
Tool News - Note PDF 168 KB 日本語
Tool News - Note PDF 234 KB 日本語
Tool News - Note PDF 83 KB 日本語
Tool News - Release PDF 263 KB
Manual - Development Tools PDF 683 KB 日本語
Manual - Development Tools PDF 327 KB 日本語
Manual - Development Tools PDF 1.73 MB 日本語
Application Note PDF 573 KB 日本語
AI-generated Summary: The guide addresses common startup issues with the E1/E20 On-Chip Debugging Emulator. It explains warning messages about project file restoration due to version mismatches in CubeSuite+ and advises upgrading to the latest version. It highlights errors caused by missing CC-RX compiler installations and instructs users to install the compiler. The guide also details handling version differences in the CC-RX compiler, allowing debugging to continue if compatible or requiring version adjustments via the property panel.
Manual - Development Tools PDF 2.54 MB 日本語
Manual - Development Tools PDF 178 KB 日本語
Manual - Development Tools PDF 153 KB 日本語
Application Note PDF 525 KB 日本語
AI-generated Summary: The External Flash Definition Editor (EFE) enables creation of custom write programs for flash memory devices with unsupported command sets. Users customize sample C source programs, link header and library files, then create RFD and USD files for use with emulator software. The custom program must not exceed 8,192 bytes in memory size and 256 bytes in stack size. The development environment requires specific sample files, a suitable C/C++ compiler, and emulator tools.
Manual - Development Tools PDF 140 KB 日本語
40 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 3.23 MB 日本語
Sample Code
[Software=RA Flexible Software Package|v6.3.0],[Toolchains=GNU Arm Embedded|13.2.rel1]
Log in to Download ZIP 22 KB Compiler: GNU ARM Embedded Function: Debugging, Emulator, Memory, Programmer IDE: e2 studio
Sample Code
Log in to Download ZIP 566 KB 日本語
3 items
Part NumberStatusStockBudgetary Price (USD)Description
RTE0T00020KCAC0000JActiveIn Stock1ku | $25.88User-system Interface Cable for the E2 Emulator (20-20 pins)
RTE0T00020KCAC1000JActiveIn Stock1ku | $25.88User-system Interface Cable for the E2 Emulator(20-10 pins)
RTE0T0002LKCE00000RActiveIn Stock1ku | $60E2 Emulator Lite

Specifications

Note that some functions shown here may not be supported under the IDE you use. Performance property and Connection system also vary depending on the MCU type.

ItemDescription
  • Connection system
  • Break function
  • Trace function
  • Memory reference and change while executing the program
  • Performance measurement
  • Hot plug-in
See On-Chip Debugger Functional Overview (PDF | English, 日本語).
On-board programmingSupportedNote1
User interface14pin 2.54mm pitch connector
(7614-6002: from 3M Japan, 2514-6002: from 3M Limited)
20pin 1.27mm pitch connector
(FTSH-110-01-L-DV-K: from Samtec)
10pin 1.27mm pitch connector
(FTSH-105-01-L-DV-K: from Samtec, FTSH-105-01-L-DV: from Samtec without a marking for matching the position of the connector; keying shroudNote2)
PC InterfaceUSB 2.0, full speed
Target board connectionVia attached user I/F cable (Connection signals vary by the target MCU type.)
Operating voltage range1.8V to 5.5V (depends on the target MCU)
Power supply from EmulatorSupply current: Up to 200mA, Supply voltage: 3.3V only
External dimension
(Except the protruding parts)
96.2 mm×52.7 mm×17.2 mm
Conformance with overseas standardsEuropean Standards: EN 55022 Class A, EN 55024
US FCC Standard: FCC part 15 Class A

Note:

  1. The E2 emulator Lite can support bit rates up to 1.5 Mbps. However, only bit rates which are selectable for the external clock of the target MCU or system of the RX family are displayed. Note that in some cases the bit rate selected for the E1 or E20 emulator will not be selectable.
  2. When using a connector without a guide marking (keying-shroud type), take care with regard to the direction for insertion of the cable.

Components

E2 emulator Lite body

USB interface cable
*Bundled

User system interface cable 14-14 pins 
*Bundled

Please be aware that a User-system interface cable will need to be purchased separately to support RA device and RISC-V MCU device debug with E2 Lite using either 20-20 pins or 20-10 pins. Please see Optional Products for RA Family or Optional Products for RISC-V MCU for details.

Purchasing FAQ : Which user-system interface cable should be purchased when introducing an emulator? (E2 Lite/E2)

System Configuration

Image
Image

Refer to the Release Information in this page for information of software on PC.

Note

  1. Optional products

Optional Products(Sold Separately)

The following optional products are provided to facilitate the use of the E2 emulator Lite in various ways. Please check which products are supported by your MCU.

RA Family   RL78 Family   RX Family   RISC-V MCU

  • Please contact Renesas sales division for RE Family.
  • Please read references to "E1 emulator" in the manuals for optional products as also meaning "E2 emulator Lite".

 

Optional Products for RA Family

TypeDescriptionProduct name / Manual
User-system Interface CableThis cable is used to connect the E2 emulator. It can also be used for the E2 emulator Lite and PG-FP6.User-system Interface Cable for the E2 Emulator (20-20 pins)
RTE0T00020KCAC0000J
RTE0T00020KCAC0000J User's Manual User-system Interface Cable for the Emulator (20-20 pins) (PDF | English, 日本語)
User-system Interface Cable for the E2 Emulator (20-10 pins)
RTE0T00020KCAC1000J
RTE0T00020KCAC1000J User's Manual User-system Interface Cable for the Emulator(20-10 pins) (PDF | English, 日本語)
IsolatorEnables debugging in environments where the grounds of the user system and the host PC are not the same.Isolator for the E2 Emulator (E2 Emulator Lite) of RA/RE
RTE0T00020KCAA0000J
RTE0T00020KCAA0000J User's Manual (Isolator for E2 Emulator) (PDF | English, 日本語)

 

Optional Products for RL78 Family

TypeDescriptionProduct name / Manual
Conversion AdapterConverts the number and pitch of pins of the connector for connecting the emulator.Small Connector Conversion Adapter for the E1 Emulator
R0E000010CKZ11
R0E000010CKZ11 User's Manual (Small Connector Conversion Adapter for E1 Emulator) (PDF | English, 日本語)
Hot-plug AdapterNote1Allows you to connect the emulator without having to turn off the system (Hot Plugin).Hot-plug Adapter for the E1 Emulator
R0E000010ACB00
R0E000010ACB00 User's Manual (Hot-plug Adapter for E1 Emulator) Rev.1.01 (PDF | English, 日本語)
IsolatorEnables debugging in environments where the grounds of the user system and the host PC are not the same.Isolator for the E1 Emulator
R0E000010ACB20
R0E000010ACB20 User's Manual (Isolator for E1 Emulator) (PDF | English, 日本語)
Low voltage OCD BoardNote2Enables debugging of an MCU with a power-supply voltage such that the on-chip flash ROM cannot be reprogrammed.This product is used between the emulator and a user's system, and is united by the in-circuit connection with the user's system.Low voltage OCD Board for RL78/G10 (10-pin/16-pin)
R0E510Y47LVB00
Low voltage OCD Board for RL78/G10 (10pin, 16pin) Rev.1.00 (PDF | English, 日本語)
An OCD board for debugging an RL78/G10 MCU (10-pin or 16-pin) with an adapter voltage below 4.5 V

Note

  1. Refer to On-Chip Debugger Functional Overview (PDF | English, 日本語) for the applicable MCU groups.
  2. Target device: RL78/G10

 

Optional Products for RX Family

TypeDescriptionProduct name / Manual
Conversion AdapterConverts the number and pitch of pins of the connector for connecting the emulator.14-Pin to 38-Pin Conversion Adapter for the E1 Emulator
R0E000010CKZ00
R0E000010CKZ00 User's Manual (14-Pin to 38-Pin Conversion Adapter for E1 Emulator) (PDF | English, 日本語)
An adapter for converting the 14-pin/2.54-mm pitch connector on the head of the emulator user interface cable to a 38-pin/0.5-mm pitch connector
Small Connector Conversion Adapter for the E1 Emulator
R0E000010CKZ11
R0E000010CKZ11 User's Manual (Small Connector Conversion Adapter for E1 Emulator) (PDF | English, 日本語)
Hot-plug AdapterNote1Allows you to connect the emulator without having to turn off the system (Hot Plugin).Hot-plug Adapter for the E1 Emulator
R0E000010ACB00
R0E000010ACB00 User's Manual (Hot-plug Adapter for E1 Emulator) Rev.1.01 (PDF | English, 日本語)
IsolatorEnables debugging in environments where the grounds of the user system and the host PC are not the same.Isolator for the E1 Emulator
R0E000010ACB10
R0E000010ACB10 User's Manual (Isolator for E1 Emulator) (PDF | English, 日本語)

Note

  1. Refer to On-Chip Debugger Functional Overview (PDF | English, 日本語) for the applicable MCU groups.

 

Optional Products for RISC-V MCU

TypeDescriptionProduct name / Manual
User-system Interface CableThis cable is used to connect the E2 emulator. It can also be used for the E2 emulator Lite and PG-FP6.User-system Interface Cable for the E2 Emulator (20-20 pins)
RTE0T00020KCAC0000J
RTE0T00020KCAC0000J User's Manual User-system Interface Cable for the Emulator (20-20 pins) (PDF | English, 日本語)
User-system Interface Cable for the E2 Emulator (20-10 pins)
RTE0T00020KCAC1000J
RTE0T00020KCAC1000J User's Manual User-system Interface Cable for the Emulator(20-10 pins) (PDF | English, 日本語)

 

Design Support

E2 emulator Lite [RTE0T0002LKCE00000R] Information for Users

Support Communities

  1. Renesas E2 lite emulator flashing issue

    Hi ,  I am using the E2 lite emulator flashing tool few months and now getting no response from the emulation CPU. Please confirm the signal of the CLOCK or RESET, WAIT and so on.(E1200416) while flashing, but last time(yesterday) flashing I am not have this issue .What is ...

    Sep 20, 2024
  2. E2 lite programmer device update.

    Hi team,       can possible to update the E2 lite programmer(debugger) using any Tool (or) application. ASAP.....

    Jan 9, 2025
  3. E2 lite programmer device update.

    Hi team,       can possible to update the E2 lite programmer(debugger) using any Tool (or) application. ASAP.....

    Jan 9, 2025
View All Results from Support Communities (31)

Knowledge Base

  1. Is it possible to use E1/E20 emulator to download into flash memory? (E2 Lite, E1, E20) [RX]

    ... number of waits). Then, register that batch file in the EFE to allow the microcontroller to access the external flash memory.If your IDE is studio or CS+, programming is also possible by using a debugger without creating a batch file. In this case, the debugger performs the same ...

    Jun 17, 2025
  2. Why Does the Emulator Not Start on a Lower Power Supply Voltage? (E2, E2 Lite, E1) [RL78]

    The possible cause is that the reset of the RL78 is not released because the LVD voltage set by the option bytes of the RL78 mounted on the target is higher than the new voltage. Start the emulator with the higher power supply voltage that was previously used. Then, write ...

    Jun 13, 2022
  3. How to Find E2 Emulator Lite Product Page

    ... from Renesas that begin with E2, including an advanced E2 emulator, and e2 studio IDE, in addition to the E2 emulator Lite.Tips- As E2 emulator Lite supports both debugging and programming function, the search results will also show two different pages, “E2 emulator Lite [RTE0T0002LKCE00000R]” and “E2 Emulator Lite ...

    May 12, 2021
View All Results from Knowledge Base (47)