Skip to main content
Renesas Electronics Corporation

Overview

Description

QE for Capacitive Touch is a tool for assisting in the development of embedded systems that include the use of capacitive touch keys.
This tool simplifies the initial settings of the touch user interface and the tuning of the sensitivity.
This product is available free of charge.

 

Features

  • The GUI makes it easy for even a beginner to develop touch user interfaces.
  • Automatic tuning for touch sensor sensitivity
  • Learn More

Release Information

Product NameLatest Ver.ReleasedTarget Device (Note1)Operating Environment
QE for Capacitive TouchV4.4.0Jul 31, 2026RA Family
RL78 Family
RX Family
Renesas SynergyTM
e² studio plug-in(Note2)(Note3)
Operating Environment

Notes

  1. For details on supported MCUs, refer to the section Target Devices.
  2. We recommend using the e² studio installer provided for the RA Family for customers using RA Family. For details, see the GitHub page on the Flexible Software Package (FSP).
  3. For development of Renesas Synergy™, we recommend to install e² studio by platform installer included SSP(Synergy Software Package). 
    For details

Installing This Product

Target Devices

Downloads

Documentation

Design & Development

Explore

Videos & Training

Additional Details

Features

The GUI makes it easy for even a beginner to develop touch user interfaces.

Simple GUI operations allow even a beginner to create the configuration for use with a touch user interface, monitor the state of input through the touch sensors, and adjust parameters.

Furthermore, since this tool can adjust tuning parameters and reflect the results through display in real-time, it is very useful for finding the appropriate parameters in various situations, such as in the presence of much static electricity or in cases of use with wet hands.

Image
QE for Cap Touch_Workflow image
Image
Adjustment Function

Automatic tuning for touch sensor sensitivity

This tool enables automatic tuning for the sensitivity of the capacitive touch sensors. You can complete basic tuning within a few minutes by following the instructions in the pop-up messages.

Image
Automatic tuning for touch sensor sensitivity

 

3D gesture recognition

You can develop a gesture application that reacts "by anyone's hand" without any specialized skills just by actually performing the gesture that you want AI to remember on the capacitance sensor.

Image
AI App Process and Functions

Supported Driver and Middleware

DeviceDriverVersion
RA FamilyCSTU (Capacitive Touch Sensing Unit) Driver
Flexible Software Package (FSP) Component for RA Family
Component name: r_ctsu
V6.5.0
Touch Middleware
Flexible Software Package (FSP) Component for RA Family
Component name: rm_touch
V6.5.0
RX FamilyDriver for capacitive touch sensor unit
RX Family QE CTSU Module Using Firmware Integration Technology
Module name: r_ctsu_qe
V3.30
Middleware for touch sensors
RX Family QE Touch Module Using Firmware Integration Technology
Module name: rm_touch_qe
V3.30
RL78 FamilyDriver for capacitive touch sensor unit
RL78 Family QE CTSU Module Software Integration System
Module name: r_ctsu
V2.30
Middleware for touch sensors
RL78 Family QE Touch Module Software Integration System
Module name: rm_touch
V2.30
Renesas SynergyCTSU (Capacitive Touch Sensing Unit) Driver
Synergy Software Package (SSP) Component for Renesas Synergy
Component name: r_ctsuv2
V2.6.0
Capacitive Touch Framework
Synergy Software Package (SSP) Component for Renesas Synergy
Component name: sf_touch_ctsuv2
V2.6.0

See here for details on adding and setting middleware related to QE for Capacitive Touch

The confirmed debugging tools

DeviceE2 emulatorE2 emulator LiteSEGGER J-Link
RA Family
RX Family
RL78 Family 
Renesas Synergy  

 

Support

Support Communities

  1. New Release QE for Capacitive Touch

    ... Synergy device families to enable capacitive touch on those microcontrollers.    Information on the new tool can be found here: QE for Capacitive Touch: Development Assistance Tool for Capacitive Touch Sensors | Renesas Please visit the Renesas weblink above to get all the latest information on the new QE for Capacitive Touch ...

    Sep 22, 2021
  2. Possibility to access the real time data of cap touch in RA6M1

    Hi, I am currently using the capacitive touch feature on the RA6M1 microcontroller. I have successfully completed the capacitive touch setup and can monitor touch responses using the Cap Touch Workflow Monitor. To further enhance my project, I need access to the real-time raw sensor data even when the ...

    Jun 4, 2026
  3. RL78/G16 Capacitive Touch example code

    Hi,  Is there have any example code for the capacitive touch?  I have try to run the CTSU examples function but it is not working well

    Feb 14, 2024
View All Results from Support Communities (4)

Knowledge Base

  1. An error occurs in e2 studio during project build. (E0520005: "qe_common.h" not found)

    ... 11 or earlier   Please use the latest version of QE for Capacitive Touch as a development support tool for capacitive touch sensors.QE for Capacitive Touch can be downloaded from the following URL.QE for Capacitive Touch: Development Assistance Tool for Capacitive Touch Sensors  Suitable Products e² studioQE for Capacitive ...

    Apr 11, 2024
  2. RL78 Family: Touch development with the RL78 microcontroller

    ... When using CS+, please also install Smart Configurator:https://www.renesas.com/software-tool/rl78-smart-configurator Click here to install QE for Capacitive Touch:https://www.renesas.com/software-tool/qe-capacitive-touch-development-assistance-tool-capacitive-touch-sensors#download

    Aug 27, 2025