Renesas Synergy™ Platform Solutions

Renesas Synergy™ Platform Solutions

Renesas Synergy™ Platform Solutions for the Building Automation Market

Renesas Synergy™ Platform is a complete and qualified system solution for highly sophisticated embedded applications such as the Building Automation (BA).
The platform includes fully integrated software, unified development tools, a scalable family of microcontrollers (MCUs), and a broad ecosystem of partners.

Value Propositions of the Synergy Platform

Accelerate Development

Reduced Total Cost of Ownership

Lower Barriers to Entry

Accelerate Development

Developers have no need to develop low level code and can focus on innovating and differentiating their own end-product above the API.

Reduced Total Cost of Ownership

Creating and maintaining professionalgrade MCU software below the API is expensive over lifetime of product when considering cost of tools, development, testing, updates and documentation. All of this in included in the Synergy Platform.

Lower Barriers to Entry

All the tools and software needed for development are included in the price of the MCU - with no fees and no royalties. Paying large licensing fees before starting a project, as with typical MCU development, is no longer required.

Structure of the Synergy Platform

The Renesas Synergy™ platform is comprised of the Solutions Gallery, software and hardware. The Solutions Gallery provides software, tools, kits, application projects, and services for the Renesas Synergy™ platform provided by Renesas and its partners. The Synergy Software Package (SSP) and development environment (tools) that are the core of the platform are free to use and do not require additional investment if you purchase a Renesas Synergy™ microcontroller.

Structure of the Synergy Platform

Scalable Synergy MCU Series

The Renesas Synergy™ microcontroller family uses the Arm® Cortex®-M core, and are designed to be scalable across the series, allowing you to reuse code. In addition, along with easy to implement connectivity features and a human machine interface, it has robust security and safety features, etc., as well as a wide range of peripheral functions that can be adapted to a variety of embedded systems.

Scalable Synergy MCU Series

Features of SSP: Application Frameworks and VSAs (Verifi ed Software Add-ons)

Application Frameworks

SSP has a rich set of Application Frameworks that provide a set of uniform Application Program Interfaces (APIs) that are useful for the development of target system. These APIs will free developers from worrying about the low-level software such as drivers, middleware or network stacks.
Messaging framework: High-level APIs for inter-thread communication and synchronization that give superior usability than traditional message queueing supported by real-time OS.
GUIX™ interface framework: APIs to leverage the performance advantage of Synergy MCU graphic accelerators while using the GUIX runtime library.
Wi-Fi framework: APIs to easily integrate Wi-Fi connectivity solutions from various module and chipset providers into the user application.
Capacitive touch sensing framework (2Q/2017): APIs to easily access the Capacitive touch sensing unit (CTSU). Also available is a Capacitive Touch Workbench for Renesas Synergy™ software tool to tune sensitivity of the touch sensors.

Application Frameworks

VSAs (Verified Software Add-Ons)

Developers who adopt SSP for BA application can also utilize abundant VSAs from various third-party partners. VSA components are pre-tested and verified by Renesas to be compatible with SSP. VSAs are available from Synergy Gallery at: synergygallery.renesas.com
BACnet Stack: BACnet stack compliant to CiA specifications. Available from CS Lab.
Skkynet ETK: Stack to connect device and cloud. Available from Skkynet.
Secure TLS/SSL Library: Available from Grape System in Japan and Cypherbridge.
Medium One Cloud Agent: Easily connect to cloud and access services. Available from Medium One.

Synergy Solutions - Product Example (PE), Application Example (AE)

Synergy Solutions are examples of actual products that adopt the platform (PE) or demonstrate a group of technologies that are implemented with the platform (AE). Following are solutions useful for BA.

PE-HMI1

PE-HMI1

  • Connected Human Machine Interface
  • S7G2 MCU based
  • WVGA LCD display
  • Wi-Fi, Bluetooth®(BT), & wired connectivity

AE-CLOUD1

AE-CLOUD1

  • Hardware kit for cloud connection evaluation
  • 2 cloud solutions (Synergy Enterprise Cloud Toolbox (SECT) and Renesas IoT Sandbox) are supported, which allows you to connect to the cloud quickly.
  • S5D9 MCU group equipped
  • A wealth of analog input function groups suitable for various sensor inputs

AE-CAP1(3Q/2017)

AE-CAP1(3Q/2017)

  • Capacitive Touch Evaluation and Tuning
  • S124 or S3A7 MCU based
  • Buttons, sliders, wheels

Other Available Synergy Kits:SK-S7G2, DK-S7G2, DK-S3A7, PK-S5D9 , DK-S128, TB-S5D5, TB-S3A1, TB-S3A6, TB-S3A3, DK-S124

The Synergy Platform provides technologies that support the applications demanded by the building automation segment. It makes it possible to quickly deliver optimized solutions to meet constantly changing technology needs such as performance, power efficiency, and design flexibility.

Synergy Platform Technology Matrix for the Building Automation Market

Synergy Platform Technology Matrix for the Building Automation Market

* Refer to the block diagrams below for the recommended Synergy MCU Series for each subsegment.

Synergy MCU Series

1. User Interface Solutions

  • Graphic LCD, segment LCD control [MCU]
  • GUIX™ runtime library [SSP]
  • PE-HMI1, PE-DAQ1[PE]
  • Capacitive touch sensing unit [MCU]
  • Capacitive touch sensing framework [SSP]
  • Touch sensing workbench [SSP]

2. Connectivity Solutions

  • Wired connection: Single/dual Ethernet
  • USB, serial interfaces (SPI, QSPI, I2C, UART), SDIO
  • Wireless connection: Wi-Fi framework [SSP] for connection to various Wi-Fi devices and chipsets
  • BACnet protocol [VSA]

3. Sensing Solutions

  • Interfaces for data collection from analog sensors or digital sensors [MCU]
  • Op-amp, PGA, A/D converter, D/A converter, comparator [MCU]
  • Low-power operating mode for intermittent operation

4. Motor Control Solutions

  • High-precision timer, PGA, A/D converter, and D/A converter for motor control [MCU]
  • Direct access to MCU control registers for real-time control

5. Embedded Security (Common Technology Across Subsegments)

  • Encryption, security key generation and storage [MCU]
  • Security function library [SSP/MCU]
Building Security System Solution Block Diagram
  • Synergy S7 or S5 Series MCU acts as the primary controller for the hub (main controller).
  • Synergy S3 or S1 Series MCU acts as the controller for the nodes.
  • Connectivity to the cloud via Ethernet or Wi-Fi.
  • BLE connectivity between nodes and the hub.

Building Security System Solution Block Diagram

Lighting System Solution Block Diagram
  • Synergy S7 or S5 Series MCU acts as the primary controller for the hub (main controller).
  • Synergy S3 or S1 Series MCU acts as the controller for the nodes.
  • Connectivity to the cloud via Ethernet or Wi-Fi.

Lighting System Solution Block Diagram

HVAC (Air Conditioning) System Solution Block Diagram
  • Synergy S7 or S5 Series MCU acts as primary controller for Zone Control.
  • Synergy S5 or S3 Series MCU for the Thermostat.
  • Synergy S1 Series MCU acts as the controller for the nodes.
  • Connectivity to the supervisory BAS system using BACnet.

HVAC (Air Conditioning) System Solution Block Diagram

Fire and Safety System Solution Block Diagram
  • Synergy S7 or S5 Series MCU acts as the primary controller for the control panel.
  • Synergy S3 or S1 Series MCU acts as the controller for the local sensing nodes.
  • Connectivity to the cloud via Ethernet or Wi-Fi.
  • BLE connectivity between nodes and the hub.

Fire and Safety System Solution Block Diagram