Overview
Description
The Go Configure™ Software Hub provides development support for:
- GreenPAK™ Programmable Mixed-Signal Products under the GreenPAK Designer Built-In Software Tool
- ForgeFPGA Low-density FPGAs under the ForgeFPGA Workshop Built-In Software Tool
In each case, the specific development software package enables a completely graphical design process, requiring no programming language or compiler, allowing a designer to configure, program, and test custom samples in minutes. The ForgeFPGA Workshop, aside from the graphical macrocells mode, also allows the HDL language programming mode.
Release Information
Minimum System Requirements for Go Configure™ Software Hub
- CPU: Dual core 2.5GHz
- RAM: 8GB
- Graphics RAM: 128MB
- Free Hard Disk Space: 2GB
- Operating System: Windows 10/11, macOS 11 or higher, Ubuntu 22.04/24.04, Debian 13/Testing
Target Devices
Videos & Training
News & Blog Posts
Support
Support Communities
- Go Configure Software Hub Update Error
Hello,I recently installed Go Configure Software Hub v6.45 on a Windows 11 machine. Whenever I open the software hub, it prompts me to install v6.46.001 but whenever I press 'Ok' it will be create a folder called 'GPD_Installer' on my desktop and start downloading a ...
Dec 5, 2024 - GreenPAK Go Configure Software Hub for Ubuntu 20.04 OS
Hi Renesas, The latest Go Configure Software available online (Go Configure Software Hub v6.45.001 for Ubuntu (***-bit) requires Ubuntu 22.04 and is not compatible with my system (Ubuntu 20.04). I am unable to update the OS which is beyond my control. Can you please provide a ...
Oct 6, 2024 - Unable to Install Go Configure Software Hub
I am trying to install the "Go Configure Software Hub v.6.27", which I assume is the new GreenPak Designer. During the installation process, I am getting the following prompt: "The feature you are trying to use is on a network resource that is unavailable. Click OK to try ...
Dec 15, 2021
Knowledge Base
- What OS versions does Go Configure™ Software Hub support?
Last Updated: 10/07/2024 Question: What OS versions do you support? Answer: Windows 10/11, macOS 11 or higher, Ubuntu 22.04/24.04, Debian 12/Testing Suitable Products SLG5100X
Oct 7, 2024 - How can I get the Development Software?
Last Updated: 10/07/2024 Question: What is the Development Software I need? How can I get it? Answer: You need Go Configure™ Software Hub. It is free to download. Suitable Products SLG5100X
Oct 7, 2024 - Q&A for GreenPAK Custom Part Order
... or requirements I should be aware of before submitting my order?a. We highly recommend reviewing the design and using the "Rules Checker" in the Go Configure Software Hub when reviewing your design to make sure there are no errors prior to submission. Can I modify or update my order ...
Sep 19, 2023