Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The CS+ Partner OS Aware Debugging Plug-in presented herein supports task-level debugging of real-time OS applications in the Integrated Development Environment CS+. There is no need to rebuild the real-time OS, nor will overhead be incurred. Debug patches, etc. are not necessary.

Features

  • Allows you to inspect the execution status of resources such as tasks and semaphores
  • Real-time RAM monitor supported
  • Capable of a mixed display of multiple resources such as task priority and event flag value
  • Learn More

Release Information

Latest Ver: V3.01.00
Released: Jun 16, 2015

Details of upgrade (See Tool News)
Operating Environment
Corresponding Real-time OS

Target Devices

Type Title Date
Upgrade - OS
Log in to Download ZIP 2.47 MB 日本語
Upgrade - OS
Log in to Download ZIP 2.54 MB 日本語
2 items

Functions

[Confirm the Resource Information from the Partner OS Aware Debugging Plug-in.]

  • Allows you to inspect the execution status of resources such as tasks and semaphores
  • Real-time RAM monitor supported
  • Capable of a mixed display of multiple resources such as task priority and event flag value
     

Operating Environment

ItemDescription
Product nameCubeSuite+ Partner OS Aware Debugging Plug-in V2.01.00CS+ Partner OS Aware Debugging Plug-in V3.01.00
Integrated Development
Environment
CubeSuite+ V2.00.00 through V2.02.00CS+ V.3.00.00 or later
Host machineRefer to Operating Environments of Products.
Corresponding debuggersRenesas Simulator Debugger and On-chip debugging emulators (E1, E20) corresponding to CubeSuite+ V2.00.00 through V2.02.00, or CS+ V3.00.00 or later.
Corresponding compilersRenesas Compilers corresponding to CubeSuite+ V2.00.00 through V2.02.00, or CS+ V3.00.00 or later. (incl. CC-RX compiler V2.00.00 or later)

Corresponding Real-time OS

Real-time OSMCU
Smalight OS from Maxell System Tech Co., Ltd.V3.10 or laterRL78 Family
RX Family
NORTi from MiSPO Co., Ltd.Version4 Release 4.4RX Family
µC3 from eForce Co., Ltd.Release 2.0.7RX Family
UCT uT-Kernel DevKit tuned for RX62N-CubeSuite+Version 1.01.01RX Family
from Ubiquitous Computing Technology Corporation
uC/OS-III from Micrium, Inc.V3.02RX Family
embOS from SEGGER Microcontroller GmbH & Co. KG.Version 3.84RX Family

* Smalight is a registered trademark of Maxell System Tech Co., Ltd.
* NORTi is a registered trademark of MiSPO Co., Ltd.
* µC3 is a registered trademark of eForce Co., Ltd.
* UCT uT-Kernel DevKit tuned is a trademark of Ubiquitous Computing Technology Corporation.
* uC/OS-III is a trademark of Micrium, Inc.
* embOS is a trademark of SEGGER Microcontroller GmbH & Co. KG.
* TRON Forum holds the copyright on the uT-Kernel specifications.

Knowledge Base

  1. Error Message E0202002: Opening a project failed

    ... in, and executing the build not displaying the main window. This may be the cause of the error. Start GUI on the CS+ and select “Plug-in Setting...” in the “Tool” menu of CS+. Uncheck the partner OS aware debugging plug-in in the dialogue for the plug-in setting ...

    Jun 24, 2019