Skip to main content
Renesas Electronics Corporation

Overview

Description

This compiler package makes it possible to code, build and debug (software simulation) any application program for R8C and M16C families. It supports the integrated development environment "High-performance Embedded Workshop". When connecting the emulator (sold separately), you can debug and evaluate on your target system in the same environment "High-performance Embedded Workshop".

Features

Release Information

C/C++ Compiler Package for R8C and M16C Families 2011.04

Latest Ver.: V.6.00 Release 00

Released: 01 Apr. 2011

Details of upgrade (See Tool News)

Operating Environment

Standard life cycle of Compilers (PDF | English, 日本語)

Target Devices

Downloads

Documentation

Design & Development

Sample Code

Additional Details

Components

ComponentsC/C++ Compiler Package for R8C and M16C Families 2011.04 (Upgrades for this package will be charged.)
Compiler for R32C SeriesC Compiler Package for R32C Series V.1.02 Release 01A (No changes have been made to V.1.02 Release 01.)
ToolsVer.
C compilerV.1.02.01
Simulator debuggerV.1.01 Release 00
Integrated development environment "High-performance Embedded Workshop"V.4.07.01 (Note1)
Compiler for M32C SeriesC Compiler Package for M32C Series [M3T-NC308WA] V.5.42 Release 00A (No changes have been made to V.5.42 Release 00.)
ToolsVer.
C compilerV.5.42.00
Simulator debuggerV.1.04 Release 00
Integrated development environment "High-performance Embedded Workshop"V.4.07.01 (Note1)
Compiler for M16C Series and R8C FamilyC/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA] V.6.00 Release 00 (Much-improved in functionality from the previous version)
ToolsVer.
C compilerV.6.00.00
Simulator debuggerV.1.06 Release 00
Integrated development environment "High-performance Embedded Workshop"V.4.09.00 (Note1)
Object formatELF (Included converter converts the objects and libraries written in the IEEE695 format into the ELF format)
Static analysis toolMISRA C Rule Checker SQMlint V.1.03 Release 00C (No changes have been made to V.1.03 Release 00B in functionality.)

Note

  1. The updata to the latest version is still available free.

[How to Upgrade to the Latest Version]

Upgrade to the C/C++ Compiler Package for M16C Series and R8C Family V.6.00 Release 00
Even if you have the previous version, you need to buy the following package. An upgrade service is NOT available.
C/C++ Compiler Package for R8C and M16C Families 2011.04
Upgrade to the latest version of the C Compiler Package for R32C Series
You can use on-line upgrade service.
Upgrade to the latest version of the C Compiler Package for M32C Series
You can use on-line upgrade service.
Upgrade to the latest version of the Simulator Debugger
You can use separate on-line upgrade service.
Upgrade to the latest version of the High-performance Embedded Workshop
You can use separate on-line upgrade service.

Support

Support Communities

  1. problem in project compilation in newer (6.00.00) version of HEW

    I made a project in HEW version 5.43 using R8c 25 group, it compiles successfully withour errors and warnings.Now the same project, i am compiling in HEW version 6.00.00, it gives me 1 error as follows: ERROR:L2310 (E) Undefined external symbol "__init" referenced in "C ...

    Jun 20, 2012
  2. Getting started R8C

    I have to learn R8C mcu basically R5F212L4SNFP & R5F21258SNFP. 1. Where to download the IDE for it. I didnt find link for HEW. Is HEW only IDE or any other renesas IDE also?2. Where to find code examples in C?

    Aug 7, 2016
  3. Simulator not working R5F212L4SNFP

    I am using HEW Version 4.09.01.007 for R5F212L4SNFP. I have written some code for it. It builds successfully. But when I run simulator, output window shows error: " ConnectedCan't read/write, because there are no memory at that area. (16653) " Also control runs to disassembly code ...

    Aug 17, 2016
View All Results from Support Communities (5)

Knowledge Base

  1. New project I made can't be debugged w/ C/C++ Compiler Package

    ... cannot be performed because the "-nodebug" option is set in the initial state for the configurations created by using the C/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA] V.6.00 Release 00.In the High-performance Embedded Workshop, click the [Build] menu -> [Renesas M16C ...

    Jun 20, 2013
  2. Makefile is not generated and can't be terminated in HEW

    ... custom build phase name. Example:   Custom build phase name: RenRenesas Command: $(PROJDIR)\_Sample\Renesas\test.bat Default directory: $(PROJDIR)\_Sample Difference in command and  default directory names: Renesas The difference between the command directory name "$(PROJDIR)\_Sample\Renesas" and the default directory name "$(PROJDIR)\_Sample" is ...

    Jun 20, 2012
  3. [HEW V.4, V.3] Are there methods for accomplishing the standard I/O?

    ... accomplish the standard I/O matches to the user system. For detail, refer to the “9.2 Creation of Initial Setting Programs” on the C/C++ Compiler Assembler Optimizing Linkage Editor User’s Manual. When using C compiler package for R8C, M16C familyThe output destination of the printf ...

    Jul 27, 2010
View All Results from Knowledge Base (29)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?