Overview
Description
M3S-TFAT-Tiny (TFAT) is a FAT file system that only requires a small amount of memory. TFAT supports FAT16 and FAT32. This is based on open source FatFs open_in_new. In addition, this is also Firmware Integration Technology (FIT) and can be combined with other FIT modules.
Use TFAT in any device incorporating a target microcontroller for functions such as accumulating measured or archived data, or rewriting a stored program via memory card. Although TFAT is a FAT file system, and PC data exchange capability enable analysis and management of data by a PC application.
TFAT supports various types of memory devices: SD memory card, USB memory, eMMC, and Serial Flash memory. The supplied sample programs include sample software for reading/writing files to SD Memory card and USB Flash drive on the CPU board which comes with the Renesas Starter Kit.
Components
- File system software
- Sample program that supports Renesas integrated development environment.
- API function user's manual and other documents in a complete set
Memory Devices Supported by the FIT Module
- SD Card (SD Mode/SPI Mode)
- USB memory
- MMC/eMMC
- Serial Flash memory

TFAT FIT:
RX Family Open Source FAT File System M3S-TFAT-Tiny Module Firmware Integration Technology
TFAT driver FIT:
M3S-TFAT-Tiny Memory Driver Interface Module Firmware Integration Technology
Features
- Compact design tailored for embedded systems
Realizable using the internal memory of the microcontroller
Approx. 8.9KB ROM and approx. 900B RAM (for the RX Family) - Supported CC-RX, IAR and GCC compilers
- Supported both of non RTOS and RTOS (FreeRTOS and RI600V4) Learn More
Target Devices
Design & Development
Additional Details
System Configuration
TFAT is used in the configuration shown below. Use TFAT in combination with other required drivers (FIT modules) which suit the memory devices (SD card, USB memory, etc.) you will be using.
Functions
| Function Name | Description |
|---|---|
| f_mount | Mounts a volume |
| f_open | Opens a file |
| f_close | Closes a file |
| f_read | Reads from a file |
| f_write | Writes to a file |
| f_lseek | Moves the read/write pointer |
| f_truncate | Truncates a file |
| f_sync | Flushes the cache |
| f_opendir | Opens a directory |
| f_readdir | Reads a directory |
| f_getfree | Gets free area |
| f_stat | Gets file status |
| f_mkdir | Makes a directory |
| f_unlink | Deletes a file or a directory |
| f_rename | Renames or moves a file or a directory |
| f_tell | Get current read/write pointer |
| f_eof | Test for end-of-file |
| f_size | Get file size |
| f_error | Test for an error |
| f_mkfs | Format a volume as FAT file system |
| disk_initialize | Initializes a drive Note |
| disk_read | Reads from a drive Note |
| disk_write | Writes to a drive Note |
| disk_ioctl | Controls drive I/O Note |
| disk_status | Gets drive status Note |
| get_fattime | Gets date and time Note |
Note: The TFAT module is not designed for use with a specific piece of hardware and therefore does not include these functions (drivers). In fact, the M3S-TFAT-Tiny memory driver interface module Firmware Integration Technology (TFAT driver FIT) includes these functions.
Operating Environment
| Target Device | RX Family |
|---|---|
| Integrated Development Environment | |
| Supporting compiler |
|
| Occupied ROM Size | Approx. 8.9KB |
| Occupied RAM Size | Approx. 0.9KB *including the stack |
Purpose
Examples of application field:
- Data preservation and data logging in various types of equipment
- Preservation of number of revolutions, temperature and other data in industrial equipment
- Preservation of a history of operations and settings alteration for remote equipment failure diagnostic
- Preservation of personal information in health equipment and similar other equipment used individually
- Preservation of heart rate and blood pressure data in health equipment
- Preservation of physical exercise data in training equipment
- Updating of programs and data in various types of equipment
- Flash memory rewriting with programs or data stored in a memory card in places where equipment is installed

How to Obtain
The RX Driver Package provides the set of FIT modules. Obtain the package, and you can then download the set of FIT modules you require. Furthermore, FIT modules work in combination with the Smart Configurator, which eases both downloading of the FIT modules and embedding them in user applications.
TFAT
| Target Device | Application Note Title |
|---|---|
| RX-family MCUs that support FIT modules | RX Family Open Source FAT File System M3S-TFAT-Tiny Module Using Firmware Integration Technology Rev.4.16 - Sample Code (ZIP) |
Memory Driver Interface
| Target Device | Application Note Title |
|---|---|
| RX-family MCUs that support FIT modules | RX Family M3S-TFAT-Tiny Memory Driver Interface Module Using Firmware Integration Technology Rev.2.63 - Sample Code (ZIP) |
Device Driver
| Target Device | Application Note Title |
|---|---|
| RX-family MCUs that support FIT modules | RX Family CMT Module Using Firmware Integration Technology Rev.5.81 - Sample Code (ZIP) |
| RX Family System Timer Module Firmware Integration Technology Rev.1.03 - Sample Code (ZIP) |
For details on other device driver software, see the following Web pages.
Support
Support Communities
- FAT32 library for RH850
Hello, Currently now I'm working with SD card, so I would like to have FAT32 library for RH850 I already tried to find it on the internet but it is not available. How can I get this library ? And who should I contact for support ? Thank you
May 11, 2022
Knowledge Base
- Tasks (such as initialization) required before the M3S-TFAT-Tiny module can be used for serial flash memory
... initialization) are required prior to using the M3S-TFAT-Tiny module for serial flash memory. Answer: First, see the following webpage, which outlines information about M3S-TFAT-Tiny: https://www.renesas.com/software-tool/fat-file-system-m3s-tfat-tiny-rx-familyFrom the above webpage ...
Apr 23, 2025