Skip to main content
Renesas Electronics Corporation

Overview

Description

FAT file system for RZ/A series
FAT file system software library for RZ/A series.
FAT file system [M3S-TFAT-Tiny] for RL78 Family
Memory-saving type FAT file system software for the RL78 Family.
FAT file system [M3S-TFAT-Tiny] for RX Family
Memory-saving type FAT file system software for the RX Family.

Target Devices

Documentation

Support

Support Communities

  1. Error on Sample program that uses Open Source FAT File System

    Hello,I import from HEW a sample program of the aplication note "Sample program that uses Open Source FAT File System [M3S-TFAT-Tiny] Module Firmware Integration Technology". I use the e2 studio IDE, version: 3.1.0.24 and the RX Compiler version 2.02.00 for the RX62N ...

    Oct 15, 2014
  2. Fat File System supporting V850, SH and RX

    Has anyone used this open source file system? I'm curious to see if there is example code written for the YRDKRX62N board?http://elm-chan.org/fsw/ff/00index_e.html

    Mar 30, 2011
  3. File system on flash memory [RX71M Revelation Kit]

    Hello, I'm new to MCU generally and I've recently started using the RX71M Revelation kit and would like to write files on the flash memory on the board. I found this library for a FAT file system but seems not to have support for flash. https:// ...

    Nov 28, 2019
View All Results from Support Communities (203)

Knowledge Base

  1. Tasks (such as initialization) required before the M3S-TFAT-Tiny module can be used for serial flash memory

    ... /www.renesas.com/software-tool/fat-file-system-m3s-tfat-tiny-rx-family From the above webpage, you can access “Open Source FAT File System M3S-TFAT-Tiny Module Firmware Integration Technology Rev.4.02”, where you can obtain the ZIP file that contains the FITDemos folder ...

    Apr 23, 2025
  2. There are no errors that appeared when using NC30 V.5 or earlier. Why?"

    ... this method.It has been confirmed that this method can be used to avoid this problem in the following middleware and driver products.Confirmed products: "FAT File System Supporting Long Filenames for M16C/60 Series, M16C/50 Series, M16C/30 Series, M16C/Tiny Series, and M16C ...

    Oct 5, 2012
  3. RA Family: Cases Where ff_fopen() Processing Time Becomes Long When Using USB Mass Storage

    ... the characteristics of the FAT file system. In particular, the allocation unit size and the state of free space are dominant factors. Questions When performing file write operations using USB mass storage,the file open operation (ff_fopen()) may take longer than expected. Is this behavior caused by an issue ...

    Jan 5, 2026
View All Results from Knowledge Base (6)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?