メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation) - 6月はプライド月間として、LGBTQ+の権利や文化、コミュニティについて啓発する世界的な活動月間です

説明

RZ Multi-OS Packageは、マルチOSソリューション開発のためのソフトウェアパッケージで、Arm® Cortex®-MまたはCortex-Rコアを搭載したルネサスMPU向けソフトウェアパッケージであるFlexible Software Package(FSP)と、プロセッサ間通信フレームワークの標準化APIであるOpenAMPで構成されています。

特長

  • OpenAMPによるRTOSベースのコアとLinuxベースのコア間のコア間通信。

リリース情報

  • 2026年3月31日: RZ Multi-OS Package v4.0.0
  • RZ/Gシリーズ
    • 2026年2月6日: Multi-OS Package v3.2.0
  • RZ/Vシリーズ
    • 2026年1月13日: Multi-OS Package v3.3.0
  • RZ/Tシリーズ
    • 2025年12月26日: Multi-OS Package v3.0.0
  • RZ/Nシリーズ
    • 2026年1月30日: Multi-OS Package v3.0.0

ターゲットデバイス

分類 タイトル 日時
ソフトウェア/ツール-ソフトウェア
ログインしてダウンロード ZIP 582.22 MB
ソフトウェア/ツール-ソフトウェア ZIP 40.93 MB
ソフトウェア/ツール-評価版ソフトウェア
ログインしてダウンロード ZIP 214.73 MB
The Multi-OS package provides sample programs for operation across multiple OS environments. It supports various combinations of Linux, bare metal, and FreeRTOS, enabling developers to evaluate and develop with different core configurations. The package includes sample code for each combination, project files for each core setup, related libraries and configuration files, example folder structures, and documentation or guides for development and debugging.
ソフトウェア/ツール-ソフトウェア ZIP 17.39 MB Compiler: GNU ARM Embedded Function: Communication Interface IDE: e2 studio
ソフトウェア/ツール-評価版ソフトウェア
[Software=RZ/T2 FSP|v3.0.0],[Toolchains=GNU ARM Embedded Toolchain|13.3.1.arm-13-24;IAR Embedded Workbench for ARM v9.60.3]
ログインしてダウンロード ZIP 273.60 MB Compiler: GNU ARM Embedded, ICCARM IDE: e2 studio, IAR EWARM
The Multi-OS package provides sample programs for operation across multiple OS environments. It supports various combinations of Linux, bare metal, and FreeRTOS, enabling developers to evaluate and develop with different core configurations. The package includes sample code for each combination, project files for each core setup, related libraries and configuration files, example folder structures, and documentation or guides for development and debugging.
5件
分類 タイトル 日時
アプリケーションノート PDF 10.34 MB
Learn how to use the Renesas RZ Flexible Software Package (FSP) for developing applications for the RZ microprocessor series. This document explains the usage of the RZ FSP running on the Cortex-A55 (CA55) core incorporated in the RZ/A3UL and RZ/A3M devices, including the development environment, software configuration, and application development workflow.
アプリケーションノート PDF 9.95 MB
Learn how to develop applications for the RZ microprocessor series using the Renesas Flexible Software Package (FSP). This application note explains how to use the FSP on the Cortex®-M33 (CM33) core integrated into RZ/G2L, RZ/G2LC, RZ/G2UL, RZ/G3S, and RZ/G3E devices, providing guidance for software development and application implementation on supported RZ MPUs.
アプリケーションノート PDF 17.85 MB
Learn how to develop applications on the Renesas RZ MPU series using the Flexible Software Package (FSP). This application note covers FSP usage on Arm Cortex‑R52 and Arm Cortex‑A55 cores in RZ/T2 and RZ/N2 MPUs, outlining software architecture, development flow, and application implementation considerations.
アプリケーションノート PDF 9.54 MB
Learn how to use the Renesas Flexible Software Package (FSP) running on the Cortex-M33 (CM33) and Cortex-R8 (CR8) cores integrated in the RZ/V2L, RZ/V2H, and RZ/V2N devices. This document explains the development environment, software configuration, and usage of the FSP for these RZ/V series devices. Support for the CR8 core is available on the RZ/V2H only.
アプリケーションノート PDF 356 KB
Introduces practical example projects for the RZG2L-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZG2L-EVK kit.
アプリケーションノート PDF 356 KB
Introduces practical example projects for the RZV2H-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZV2H-EVK kit.
アプリケーションノート PDF 356 KB
Introduces practical example projects for the RZV2N-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZV2N-EVK kit.
アプリケーションノート PDF 356 KB
Introduces practical example projects for the RZG2LC-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZG2LC-EVK kit.
アプリケーションノート PDF 356 KB
Introduces practical example projects for the RZG2UL-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZG2UL-EVK kit.
アプリケーションノート PDF 359 KB
Introduces practical example projects for the RZG3E-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZG3E-EVK kit.
アプリケーションノート PDF 356 KB
Introduces practical example projects for the RZG3S-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZG3S-EVK kit.
アプリケーションノート PDF 453 KB
Introduces practical example projects for the RZN2H-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZN2H-EVK kit.
アプリケーションノート PDF 453 KB
Introduces practical example projects for the RZT2H-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZT2H-EVK kit.
アプリケーションノート PDF 356 KB
Introduces practical example projects for the RZV2L-EVK kit. The example projects contained within the bundle show how to write code for the various Renesas Flexible Software Package (FSP) modules supported by the RZV2L-EVK kit.
アプリケーションノート PDF 1.07 MB
The AWO example project that is included in the RZ/G Multi-OS package demonstrates the behavior of waiting in low-power mode with only Cortex-M33 running after a Linux shutdown and restarting Linux from Cortex-M33.
アプリケーションノート PDF 1.17 MB
The AWO example project that is included in the RZ/G Multi-OS package demonstrates the behavior of waiting in low-power mode with only Cortex-M33 running after a Linux shutdown and restarting Linux from Cortex-M33.
アプリケーションノート PDF 1.05 MB
The Always On (AWO) example project that is included in the RZ/V Multi-OS Package demonstrates the behavior of waiting in low-power mode with only Cortex-M33 running after a Linux shutdown and restarting Linux from Cortex-M33.
クイックスタートガイド PDF 1.03 MB
Learn the procedure for integrating the RZ/G Multi-OS Package into the RZ/G Verified Linux Package (referred to as VLP) for the RZ/G2L, G2LC, G2UL. By integrating the Multi-OS Package, users can efficiently establish a multi-OS environment wherein Linux operates on the Cortex-A55 and FreeRTOS/bare metal runs on the Cortex-M33, with support for inter-processor communication between these CPU cores.
クイックスタートガイド PDF 1.97 MB
Learn the procedure for integrating the RZ/G Multi-OS Package into the RZ/G Verified Linux Package (referred to as VLP) for the G3E. By integrating the Multi-OS Package, users can efficiently establish a multi-OS environment wherein Linux operates on the Cortex-A55 and FreeRTOS/bare metal runs on the Cortex-M33, with support for inter-processor communication between these CPU cores.
クイックスタートガイド PDF 1.97 MB
Learn the procedure for integrating the RZ/G Multi-OS Package into the RZ/G Verified Linux Package (referred to as VLP) for the RZ/G3S. By integrating the Multi-OS Package, users can efficiently establish a multi-OS environment wherein Linux operates on the Cortex-A55 and FreeRTOS/bare metal runs on the Cortex-M33, with support for inter-processor communication between these CPU cores.
クイックスタートガイド PDF 3.39 MB
Learn sample program setup procedures for multiple-core (bare-metal/FreeRTOS/Linux running on Cortex-A55 and bare-metal/FreeRTOS running on Cortex-R52) environments and sample programs. This package consists of the RZ/N2H Cortex-R52 Flexible Software Package (RZ/N2H CR52/CA55 FSP), the inter-processor communication feature via OpenAMP for the RZ/N2H Board Support Package (RZ/N2H BSP), and the Linux BSP software package.
クイックスタートガイド PDF 3.64 MB
Learn sample program setup procedures for multiple-core (bare-metal/FreeRTOS/Linux running on Cortex-A55 and bare-metal/FreeRTOS running on Cortex-R52) environments and sample programs. This package consists of the RZ/T2H Cortex-R52 Flexible Software Package (RZ/T2H CR52/CA55 FSP), the inter-processor communication feature via OpenAMP for the RZ/T2H Board Support Package (RZ/T2H BSP), and the Linux BSP software package.
クイックスタートガイド PDF 2.15 MB
Learn the procedure for integrating the RZ/V Multi-OS Package into the RZ/V2H AI SDK. By integrating the Multi-OS Package, users can efficiently establish a multi-OS environment wherein Linux operates on the Cortex-A55 and FreeRTOS/bare metal runs on the Cortex-M33 and/or Cortex-R8 with support for inter-processor communication between these CPU cores.
クイックスタートガイド PDF 1.27 MB
Learn the procedure for integrating the RZ/V Multi-OS Package into the RZ/V Verified Linux Package (referred to as VLP) for the RZ/V2L. By integrating the Multi-OS Package, users can efficiently establish a multi-OS environment wherein Linux operates on the Cortex-A55 and FreeRTOS/bare metal runs on the Cortex-M33, with support for inter-processor communication between these CPU cores.
クイックスタートガイド PDF 2.14 MB
Learn the procedure for integrating the RZ/V Multi-OS Package into the RZ/V2N AI SDK. By integrating the Multi-OS Package, users can efficiently establish a multi-OS environment wherein Linux operates on the Cortex-A55 and FreeRTOS/bare metal runs on the Cortex-M33 with support for inter-processor communication between these CPU cores.
リリースノート PDF 207 KB
See what’s additionally supported, improvements, and bug fixes for the RZ Multi-OS Package V4.0.0.
リリースノート PDF 236 KB
アプリケーションノート PDF 2.55 MB
Learn the easy way to establish a multi-OS (i.e. CIP Linux running on Cortex-A55 and bare-metal/FreeRTOS running on Cortex-R52/A55) environment and sample program showing how to implement inter-processor communication between those CPU cores. This package consists of the RZ/N2H Cortex-R52/A55 Flexible Software Package (RZ/N2H FSP) and the inter-processor communication feature package for the RZ/N2H Board Support Package (RZ/N2H BSP).
リリースノート PDF 240 KB
The Multi-OS package provides sample programs for operation across multiple OS environments. It supports various combinations of Linux, bare metal, and FreeRTOS, enabling developers to evaluate and develop with different core configurations. This is the release note for the multi-OS package running on the RZ/N2H.
リリースノート PDF 151 KB
See what’s additionally supported, improvements, and bug fixes for the RZ/V Multi-OS Package.
リリースノート PDF 241 KB
The Multi-OS package provides sample programs for operation across multiple OS environments. It supports various combinations of Linux, bare metal, and FreeRTOS, enabling developers to evaluate and develop with different core configurations. This is the release note for the multi-OS package running on the RZ/T2H.
アプリケーションノート PDF 3.14 MB
Learn the easy way to establish a multi-OS (i.e. CIP Linux running on Cortex-A55 and bare-metal/FreeRTOS running on Cortex-R52/A55) environment and sample program showing how to implement inter-processor communication between those CPU cores. This package consists of the RZ/T2H Cortex-R52/A55 Flexible Software Package (RZ/T2H FSP) and the inter-processor communication feature package for the RZ/T2H Board Support Package (RZ/T2H BSP).
アプリケーションノート PDF 259 KB
AI生成コンテンツ: The RZ/G FSP Example Project Bundle provides sample code demonstrating how to use various Renesas Flexible Software Package (FSP) modules for embedded system design. It supports multiple RZ/G evaluation boards and FSP version 3.1.0, offering lightweight, efficient drivers with uniform APIs and detailed documentation. The bundle includes examples for peripherals like ADC, CANFD, SPI, UART, FreeRTOS, and watchdog timers, with recent updates adding support for the RZ/G3E board and new examples. The license is BSD-3-Clause, enabling flexible use in open-source projects. Users should refer to the Example Project Usage Guide and Getting Started documents for setup and debugging.
アプリケーションノート PDF 9.69 MB
AI生成コンテンツ: The guide explains how to operate example projects using the RZ/G Flexible Software Package (FSP) on supported RZ/G series devices and evaluation kits. It details prerequisites such as tool experience and embedded system knowledge. It lists hardware and software requirements, including Windows 10, RZ/G FSP v3.1.0, e2 studio 2025-07, and SEGGER J-Link RTT Viewer v7.96j. Installation instructions for FSP and J-Link RTT Viewer are provided. The document outlines project import, running procedures, and numerous example projects covering various peripherals like CANFD, RIIC, RSPI, SCIF, GPT, FreeRTOS, and others, including hardware settings and operation steps.
アプリケーションノート PDF 242 KB
AI生成コンテンツ: The RZ/V FSP Example Project Bundle offers practical example projects demonstrating how to use various Renesas Flexible Software Package (FSP) modules for embedded system design. It supports RZ/V2L and RZ/V2H evaluation boards and FSP version 2.0.1, providing lightweight, efficient drivers with uniform APIs and detailed documentation. The bundle includes examples for ADC, CANFD, RIIC, SPI, UART, FreeRTOS, and more, with recent additions supporting RZ/V2H kits and enhanced DMAC transfer. The package ensures high-quality code through peer reviews and automated testing. Users can access related resources and support via Renesas websites.
アプリケーションノート PDF 7.09 MB
36件

サンプルコード

サンプルコード

フィルター
分類 タイトル 日時 日時
サンプルコード
ログインしてダウンロード ZIP 1.94 MB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZV2H-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード
ログインしてダウンロード ZIP 1.15 MB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZV2N-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード
ログインしてダウンロード ZIP 955 KB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZG2LC-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード
ログインしてダウンロード ZIP 872 KB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZG2UL-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード
ログインしてダウンロード ZIP 1.76 MB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZG3E-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード
ログインしてダウンロード ZIP 1.20 MB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZG3S-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード
ログインしてダウンロード ZIP 10.86 MB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZN2H-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード
ログインしてダウンロード ZIP 10.00 MB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZT2H-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード
ログインしてダウンロード ZIP 1.06 MB
Demonstrates how to write code using various unified Renesas RZ Flexible Software Package (FSP) v4.x.x modules supported by the RZV2L-EVK. The unified RZ FSP consolidates all previous family‑specific FSPs into a single package and provides an optimized, easy‑to‑use, scalable, high‑quality software solution for embedded system design.
サンプルコード ZIP 3.62 MB Function: Application Example
サンプルコード
[Software=RZ Flexible Software Package|v2.0.1],[Toolchains=GNU Arm Embedded|???]
ログインしてダウンロード ZIP 4.33 MB Compiler: GNU ARM Embedded Function: Driver or Library IDE: e2 studio
11件

関連ボード&キット

ニュース&ブログ

各デバイス向けのマルチOSパッケージの使用方法については、以下の情報とドキュメントをご参照ください。

RZ/Gシリーズ

RZ/Vシリーズ

項目RZ/V2NRZ/V2HRZ/V2L
マルチOSパッケージ V4.0.0コア間通信(OpenAMP: Linux - FSP)クイックスタートガイド(PDF)クイックスタートガイド(PDF)クイックスタートガイド(PDF)
電力管理 AWO (Always-On)AWOサンプルプロジェクト スタートアップガイド(PDF)AWOサンプルプロジェクト スタートアップガイド(PDF)-
RZ Flexible Software PackageV4.0.0V4.0.0V4.0.0
Linuxソフトウェアパッケージ--VLP V3.0.7
AI Software Development Kit (SDK)RZ/V2N AI-SDK V6.3.0RZ/V2H AI-SDK V6.00-

RZ/Nシリーズ

項目RZ/N2H
マルチOSパッケージ V4.0.0コア間通信(OpenAMP: Linux - FSP)アプリケーションノート(PDF)
コア間通信(OpenAMP: FSP - FSP)クイックスタートガイド(PDF)
RZ Flexible Software PackageV4.0.0
Verified Linux PackageVLP V5.0.0

RZ/Tシリーズ

項目RZ/T2H
マルチOSパッケージ V4.0.0コア間通信(OpenAMP: Linux - FSP)アプリケーションノート(PDF)
コア間通信(OpenAMP: FSP - FSP)クイックスタートガイド(PDF)
RZ Flexible Software PackageV4.0.0
Verified Linux PackageVLP V5.0.0

RZ FSPに関する詳細情報は、RZ Flexible Software Package (FSP)のソフトウェアページをご参照ください。

動作環境

統合開発環境e2 studio統合開発環境、デフォルトのツールチェーンはGCC Arm Embeddedです。
エミュレータSEGGER(J-Linkシリーズ)

サポートコミュニティ

  1. Amazon FreeRTOSだそうです。ルネサスさんのRXは参加しないのかな?

    こんにちは。NoMaYです。ライセンスはMIT Licenseでした。TLSとしてmbed TLSが使用されていました。サポートされているボードの写真 ...

    2017年12月2日
  2. やっちゃうんですね(やっちゃったんですね、かな)

    ... ティ、周辺機能の最適解を追求~フレキシブル・ソフトウェア・パッケージとArmエコシステムが、開発スピードを加速~www.renesas ...

    2019年10月8日
  3. RenesasさんからStrategy Updateが発表されましたね

    ... www.renesas.com/jp/ja/about/ir/event/pdf/fy2020/automotive-strategy.pdfInfra industrial and iot strategy ( ↓ RZの新シリーズ? )www.renesas.com/jp/ja/about/ir/event/pdf/fy2020/ ...

    2020年2月18日
サポートコミュニティからの全ての結果を参照 (17件)
サポートコミュニティ

サポートコミュニティ

ルネサスエンジニアリングコミュニティの技術スタッフから迅速なオンライン技術サポートを受けることができます。
記事を参照する

ナレッジベース

ナレッジベースを参照して、役立つ記事、FAQ、その他の役立つリソースを入手してください。
サポートチケット

サポートチケット

技術的に深い内容や公開したくない内容のご質問はこちらです。