Overview
Description
The SSC Communication Board is included in Renesas' modular SSC Evaluation Kits for select sensor signal conditioner (SSC) ICs. It is also part of the modular SSC Mass Calibration System for SSC ICs. It provides communication between the user's computer and the SSC IC mounted on the SSC Evaluation Board, the user's module, or a mass calibration reference board connected to the mass calibration board. It can be ordered separately.
Features
- SSC Communication Board
- USB cable
Applications
Design & Development
Support
Support Communities
- Evaluation Kit for ZSC31150: Problem with communication (SSC_Board not found)
Hello, Currently I am trying to use a newly purchased ZSC31150KIT with a ZSC31150 connected to it via OWI. Unfortunately, I always get the error message “SSC_Board not found” when I try to establish communication via OWI. I am also unable to switch on the “KS5V” sensor supply on ...
Apr 16, 2025 - Can I get ZSSC3241Kit schematic?
Can I get ZSSC3241Kit schematic? Thank you!
Apr 29, 2025 - ZSSC3241-Writing Commands
Hi all- I am hoping for some assistance in writing commands to my ZSSC3241 (e.g. CHECK_DIAG) using the Renesas interface. So far I have tried writing them using the terminal: Thanks in advance!
Feb 25, 2025