Skip to main content
Renesas Electronics Corporation

Overview

Description

Topics
RA Smart Configurator supports the new device RA0E3.
Supports FSP 6.4.0.

The Renesas RA Smart Configurator (RA SC) is a desktop application that helps you in configuring software systems (including a Board Support Package (BSP), drivers, RTOS, and middleware) for RA-Family MCUs when you are using a third-party IDE and toolchain.

You need to download the platform installer included FSP (Flexible Software Package) to use RA Smart Configurator .
For details, see Release Information.

Release Information

MCUSupported IDEs and user guidesLatest Ver.
e² studioIARArm Keil
RAe² studio plug-in
(Note1)
download
RA SC User Guide for MDK and IAR
V2025-12

Note

  1. The package of the e² studio includes this plug-in.

Target Devices

Downloads

Documentation

Videos & Training

Additional Details

Functions

Creating Projects for the IDEs from Renesas Partners

You can create projects for EWARM from IAR Systems or the Keil MDK from Arm.

Image
Create EWARM and Keil MDK project
When creating a new project, you can select whether to create it for EWARM from IAR Systems or the Keil MDK from Arm.

Creating a Project that Supports TrustZone®

You can create a project that supports TrustZone® or a flat project that does not support TrustZone®

Image
Secure project
Secure Project
Image
Non secure project
Non-secure Project
Image
Flat project
Flat Project

Reading and Changing the State of a Device that Supports TrustZone®

You can read and change the state of a device that supports TrustZone®

Image
Read and modify device status

For a device that supports TrustZone®, you can use the Renesas Device Partition Manager (RDPM) to check and change the state of the device lifecycle management (DLM), make the memory partition settings, and restore the state of the device to that at the time of shipment.

Setting Pins

You can set pins via a GUI and verify and resolve cases where conflicting functions are assigned to the same pins.

Image
Pin settings
[Pins] page (showing each peripheral function)
You can set the pins to be used for each peripheral function on the [Pins] page.
Image
FSP Visualization view
[FSP Visualization view]
The [FSP Visualization] view shows used pins, unused pins, and pins to which conflicting functions are assigned in different colors to allow easy confirmation of the overall state.

Adding and Deleting Threads and Objects

You can add and delete threads, FSP module instances, and kernel objects on the [Stacks] page and change each of the properties in the [Properties] view.

Image
FSP Smart Configuration

Support

Support Communities

  1. In RA smart Configurator, uart stack option cannot be generated, and uart stack can be added manually, only starting from uart0, uart1 cannot be configured as needed

    In RA smart Configurator, why I completed the settings of SCI1 and ports in the pins option, but the uart configuration item does not appear in the stack option. [locked by: Herald at 13:34 (GMT 0) on 14 Sep 2021]

    Sep 2, 2021
  2. How to add defines like _RENESAS_RA_ using RA Smart configurator

    ... RA Smart configurator to move my e2 studio project to IAR IDE but i need to add some customs defines to the following three general defines :  -D_RA_ORDINAL=1-D_RA_CORE=CM33-D_RENESAS_RA_I'm using a R7FA6M5 This thread was automatically locked due to age.

    May 17, 2024
  3. In RA smart Configurator, uart stack option cannot be generated, and uart stack can be added manually, only starting from uart0, uart1 cannot be configured as needed

    In RA smart Configurator, why I completed the settings of SCI1 and ports in the pins option, but the uart configuration item does not appear in the stack option. [locked by: Herald at 13:34 (GMT 0) on 14 Sep 2021]

    Sep 2, 2021
View All Results from Support Communities (301)

Knowledge Base

  1. RA Family: Using ELC to Output WDT Underflow Event to GPIO Pin

    ... to directly link a WDT underflow event to a port output and set the target pin to High level. Configure the following settings in the RA Smart Configurator: Pin AssignmentIn the [Pins] tab, set the target pin to "Output mode (Initial Low)".Note that not all ports support ELC event ...

    Sep 15, 2026
  2. RA Family: Implementing CTSU Driver and Touch Middleware APIs from Developer Assistance

    ... Answer The CTSU driver and Touch middleware instances are generated by QE for Capacitive Touch (hereafter referred to as the QE tool), not by the RA Smart Configurator.Developer Assistance cannot reference the instance names defined by the QE tool.As a result, APIs inserted by Developer Assistance use placeholder ...

    Apr 8, 2026
  3. How to convert an e² studio FSP project into an RA or RZ Smart Configurator project that can be built in a partner IDE

    Install RA or RZ SC v2022-07 or higher, open Quick Start Guide from the Help menu, and then see the chapter "From Existing e² studio Projects."

    Jul 30, 2024
View All Results from Knowledge Base (25)