Skip to main content
Renesas Electronics Corporation

Overview

Description

Topics 
・A new DSPASM Structured Assembler V1.06.00 for the FAA or GREEN_DSP (for Linux and macOS) has been added.
・A new SMS Assembler V1.01.00 (for Linux and macOS) has been added.

In development of embedded systems, C Compilers for RL78 Family offers the powerful optimizations for enhancing execution speed and code efficiency, and the utilities to increase productivity. Products differ depending on each integrated development environment.

 

Features

  • https://www.renesas.com/en/document/rln/rl78-compiler-cc-rl-v11201-release-noteANSI-compliant
    • Support C89, C99 of ANSI
      Note: The variable length array type, complex type, and some standard library functions of the C99 standard are not supported.
  • Superior optimization
    • The compiler applies our latest optimization techniques to generate code that has excellent performance in execution (up to a three-fold (Measured for programs held by Renesas) improvement in execution performance over code compiled by the CA78K0R compiler, our previous product)
    • The compiler applies our latest optimization techniques to the generation of compact code (up to a 10-percent (Measured for programs held by Renesas) improvement over the CA78K0R).
    • Easy optimization settings and many optimization features
    • Linker-level optimization is now included in addition to optimization at the compiler level.
  • Cooperated with RL78 MCU architecture
    • Interrupt processing routines can be written in the C language (up to a six-fold (Measured for programs held by Renesas) improvement in interrupt response performance over code compiled by the CA78K0R compiler)
    • Provides intrinsic functions
  • An MISRA C rule checker supports the description of high-quality program [Professional edition only]
    • Supports automatic checking of C source code based on the MISRA-C: 2004/2012 rules as compiler options
    • About MISRA C, refer to here. [Learn More]
  • Assistance in Porting Files to the CC-RL from the CA78K0R. [Learn More]
  • Learn More

Release Information

Product NameCompiler Name / Release Date of the Latest VersionDownload
RL78 Family C Compiler PackageCompiler: CC-RL V1.16.00 for Windows
Released: Jan 20, 2026 Details of upgrade (See Release Note)
CC-RL for CS+
Note1
CC-RL for e² studio
Note2
License Manager for Windows
Compiler: CC-RL V1.16.00 for Linux
Released: Jan 20, 2026 Details of upgrade (See Release Note)
CC-RL for Linux
Note3
License Manager for Linux
Note4
Compiler: CC-RL V1.16.01 for macOS
Released: Jan 20, 2026 Details of upgrade (See Release Note)
CC-RL for macOS
Note3
License Manager for macOS
Note4

Note

  1. Update CS+ if you are not already using the latest version.
  2. Separately install the e² studio.
  3. Equivalent to CC-RL V1.16.00 for Windows. A license manager is required for each operating system.
  4. The license manager for Linux does not have a GUI and is operated using a command line interface (CLI).

FAQ

Title
MCUs which can be used with the free evaluation edition (CC-RL)
Is the RL78 C compiler license bought with CS+ valid for e² studio, too?
How to shorten time until interrupt function processing starts(CC-RL)

See all related FAQs

Target Devices

Downloads

Documentation

Explore

Videos & Training

Order

When purchasing a compiler package, contact your nearest distributor.
Alternatively, Web sites for online sales are accessible by clicking on a [Buy/Quote] button in the table below.

  • We offer various licenses to suit a range of needs. Refer to Compiler Licenses for details.
  • The license keys of the compiler included in the packages for each of the products are usable with either CS+ or the e² studio.
    In the Americas and Europe, use the e² studio instead of the CS+.
  • The C Compiler Package no longer includes the installation medium (CD/DVD).
    Please obtain the installer from each product page.
  • 1.01.00 or later versions of CC-RL support both floating licenses and annual licenses.

 

Licenses for Newly Purchasing the Latest CC-RL

Give the part number from the list below to the distributor. Web sites for online sales are also accessible by clicking on a [Buy/Quote] button in the table below.

Important
Each of the compiler packages listed below comes with a license which allows you to use the latest version of CC-RL.

Period Form of usage Edition Part Number

RL78 Family C Compiler PackageOnline Sales 
MouserAvnetDigikey    
annualNode-LockedstandardLow price
RTCRL7800CB01WNR
Buy/QuoteBuy/QuoteBuy/Quote
  professionalRTCRL7800CA01WNRBuy/QuoteBuy/QuoteBuy/Quote
 FloatingstandardRTCRL7800CB01WNRN1Buy/QuoteBuy/QuoteBuy/Quote
  professionalRTCRL7800CA01WNRN1Buy/QuoteBuy/QuoteBuy/Quote
permanentNode-LockedstandardRTCRL7800CS01WNRBuy/QuoteBuy/QuoteBuy/Quote
  professionalPopular item
RTCRL7800CL01WNR
Buy/QuoteBuy/QuoteBuy/Quote
 FloatingstandardRTCRL7800CS01WNRN1Buy/QuoteBuy/QuoteBuy/Quote
  professionalRTCRL7800CL01WNRN1Buy/QuoteBuy/QuoteBuy/Quote

For multiple licenses, the end of the part number depends on the number of licenses.

  • For Node-Locked licenses, L5, LA, or LT is added at the end of the part number depending on the number of licenses (5, 10, or 20).
    (For example, when the number of licenses is 5, the part number is RTCRL7800CL01WNRL5)
  • For Floating licenses, the last numeric character “1” at the end of the part number is replaced by 5, A, or T depending on the number of licenses (5, 10, or 20).
    (For example, when the number of licenses is 5, the part number is RTCRL7800CL01WNRN5)

 

License for Upgrading from the CC-RL Standard Edition to the Professional Edition

Give the part number from the list below to the distributor. Web sites for online sales are also accessible by clicking on a [Buy/Quote] button in the table below.

C Compiler Package for RL78 Family V1 Upgrade (Edition)Online Sales 
PeriodForm of usagePart NumberMouserAvnetDigikey
permanentNode-LockedRTCRL7800CU01WNRBuy/QuoteBuy/QuoteBuy/Quote

Note:

  1. Node-Locked license for CC-RL standard version (permanent) is required.
  2. This form of upgrade (of the edition) is only for node-locked licenses; it will not apply to floating licenses and annual licenses.

For multiple licenses, the end of the Part Number changes depending on the number of licenses.

  • For Node-Locked licenses, L5, LA, or LT is added at the end of the part number depending on the number of licenses (5, 10, or 20).
    (For example, when the number of licenses is 5, the part number is RTCRL7800CU01WNRL5)

 

License Requirements

Regardless of whether you have a license or not, all versions of CC-RL can be used for commercial purposes such as development and production. If you will be using the CC-RL beyond the restrictions on the linkage size or optimization or would prefer to use the professional edition, consider purchasing a license for CC-RL.

For more information on the trial period and types of license, see Compiler Licenses.

 

Related Services

Compiler Qualification (Service to Support Functional Safety)

For customers who are using a compiler for Renesas devices, we offer a support service for the qualification of confidence that development tools meet the requirements of ISO 26262, Road Vehicles Functional Safety. This service incurs a charge.
Compiler Qualification

Assistance with Compiler Migration

The IDEs from Renesas (such as the e² studio and CS+) allow for the porting of projects between IDEs to facilitate the reuse of existing resources. Refer to the guidance page of migration when changing your compiler after changing your development environment. The guidance page describes precautions that must be taken when changing compilers, such as differences in options and in extended language specifications.
Migrating between Integrated Development Environments

Image
Import other IDE Project

Support

Support Communities

  1. migrate IAR embedded to CUBESUITE +

    Hi , how to migrate IAR embedded workbench project  to CUBESUITE + Thanks.

    May 31, 2022
  2. Using I2C / IIC API code from AP4 / Applilet / Code Generator for RL78... only getting first clock

    Overall I've been loving the AP4 Code Generator from Renesas for the RL78 (except for the billion possible names for the tool, not to mention I2C versus IIC, makes internet searches hard), but I'm having a problem getting I2C to work on my RL78 project and I've ...

    Apr 1, 2016
  3. How to enable Autocomplete feature in CS+ IDE?

    Hello all hope you all are doing well, can anybody tell me is there any auto-completion feature is available in CS+ if yes then how can I enable and use it. My project is huge so want to enable this feature so that CS+ suggests to me the possible ...

    Jul 13, 2021
View All Results from Support Communities (419)

Knowledge Base

  1. Downloading Commercial Edition of C Compiler Package (CC-RL/CC-RX/CC-RH)

    ... license key. If  you have purchased a node lock licenseBy registering the license key in the License Manager, you can use the commercial edition of C compiler package.  If you have purchased a floating licenseOnce you have registered a license key in the floating license management software, you can use ...

    Mar 27, 2026
  2. Use of CS+ Integrated Development Environment on C Complier Package License (Without IDE) (CC-RL/CC-RX/CC-RH)

    You can use CS+ or e² studio on a license for a "without IDE" C compiler package. The license is for the compiler. The integrated development environment itself is not license-based.

    Apr 12, 2019
  3. Storing the CRC result from multiple RL78 memory blocks (RL78 CC-RL)

    Since CC-RL V1.12.00 or later, it is possible to specify multiple -CRC options to perform CRC operations at the same time. For more information, see [FAQ] Configure multiple CRC operations. If you use the versions before CC-RL V1.12.00, you can store the CRC operation ...

    Feb 9, 2026
View All Results from Knowledge Base (127)