Skip to main content

Renesas Blog

Smart Asset Tracking Label Blog Image

Smart Asset Tracking Label: The Future of Package Tracking

Our smart asset tracking label solution is a Bluetooth Low Energy, multi-sensor solution supporting data logging, real-time inventory and environmental data monitoring to prevent record and time-stamp inventory loss and damage.

Realize OTA update using RX MCU with Bluetooth Low Energy (Bluetooth LE) wireless communication

Realize OTA Updates Using an RX MCU with Bluetooth Low Energy (Bluetooth LE) Wireless Communication

This blog introduces Renesas’ Over-the-Air (OTA) solution that uses Bluetooth Low Energy (LE) wireless technology to update the RX23W firmware from your smartphone.
CPX3 – The First Powerline Solution with a PRIME 1.4 Certification Supporting Security Profiles and Backward Compatibility Blog

CPX3 – The First Powerline Solution with a PRIME 1.4 Certification Supporting Security Profiles and Backward Compatibility

The R9A06G037 Cool Phoenix 3 Powerline Modem (CPX3) has been re-certified to the PRIME Powerline standard Version 1.4 covering all security profiles as well as backward compatibility features.  

Introducing the Wireless Evaluation Board from "Silex" that Can Easily be Used for Wireless and Total Power Evaluation of the BT5 Device Using the Renesas IDE Blog

Wireless and Total Power Evaluation of a BT5 Device Using Silex Evaluation Board and Renesas IDE

Easily get actual wireless and power evaluation even at a very early stage of the development using the Silex wireless evaluation board and Renesas’ IDE.

Certified for G3-Hybrid on CPX3 - Optimal Coverage with PLC or RF

CPX3 Goes “G3-PLC Hybrid”

The R9A06G037 Cool Phoenix 3 Power Line Modem (CPX3) in combination with the RAA604S00 TsuRuGi sub-GHz transceiver has received the certification for the G3-PLC Hybrid specification.

Introducing the RX Family Firmware Update Middleware that can easily realize FOTA (Firmware Update Over-The-Air) implementation

Introducing the RX Family Firmware Update Middleware that Can Easily Realize FOTA (Firmware Update Over-The-Air) Implementation

With the increase in IoT device deployment, the number of inquiries for Over-the-Air firmware updates has been increasing. This blog introduces Firmware Update Over-the-Air middleware for the RX MCU Family.

DSP Experience with RX Family MCU! Visualizing DSP Behavior with Free Sample Program! Blog

DSP Experience with RX Family MCU! Visualizing DSP Behavior with Free Sample Program!

Introducing a low cost and easy way to realize Digital Signal Processing (DSP), which is often thought to be expensive and difficult, with the RX Family of MCUs.

Triac-Based Motor Controller Blog

Cool Off and Reduce Time-to-Market with the Triac-Based Motor Control Solution

Renesas’ triac-based motor controller is a compact air conditioning system solution that offers optimized triac control for a simplified compressor motor control system design.

Model-Based Development Product of Renesas RH850/C1M-Ax Specializing in HEV/EV Motor Control Blog

Model-Based Development Product of Renesas RH850/C1M-Ax Specializing in HEV/EV Motor Control

The model-based development software for Renesas’ RH850/C1M-Ax in-vehicle microcontroller specializes in HEV/EV motor control and is available as in a paid or free version.

Do You Want to Develop a Touchless Button? Introducing a Solution with a General-Purpose MCU Blog

Do You Want to Develop a Touchless Button? Introducing a Solution Using a General-Purpose MCU

To meet the increasing demands for touchless control, Renesas offers a cost-efficient Touchless Button Demo Solution using Renesas microcontrollers with a built-in capacitive touch sensor unit (CTSU).