Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Topics
・e² studio simulator supports the new device RL78/F22.

This simulator enables source-level debugging of applications on our integrated development environment e² studio even before the target system becomes available, thus achieving efficient debugging of the programs developed for the RL78 family.

It comes with diverse break and coverage measurement functions and allows you to evaluate software modules almost as if they were running on the actual system board. Furthermore, its intuitive GUI (Graphical User Interface) operability makes your debugging environment highly user-friendly.

Features

  • Comes with diverse break and coverage measurement functions.
  • Allows you to evaluate software modules almost as if they were running on the actual system board.
  • Intuitive GUI* operability makes your debugging environment highly user-friendly.
    *Graphical User Interface
  • Simulation of the following items is available as well as CPU instruction simulation (only some MCU groups).
    • The simulation of MCU peripheral functions such as timers and serial ports
    • Virtual target board simulation via the [I/O panel] window
    • MCU pin signal waveform generation in the [Timing chart] window
    • Simulation of current drawn by MCUs

Release Information

Operating Environment

This product is included in e² studio and will be added to the integrated development environment automatically upon installing e² studio.

For RL78/G10, RL78/G11, RL78/G12, RL78/G13, RL78/G13A, RL78/G14, RL78/G15, RL78/G16, RL78/G1F, RL78/G22, RL78/G23, RL78/G24, RL78/L12, RL78/L23, 78K0/Kx2, 78K0R/Ix3, 78K0R/Kx3, and 78K0R/Lx3 devices, simulation of the following items is available as well as CPU instruction simulation.

  • The simulation of MCU peripheral functions such as timers and serial ports
  • Virtual target board simulation via the [I/O panel] window
  • MCU pin signal waveform generation in the [Timing chart] window
  • Simulation of current drawn by MCUs*
    *Simulation of current drawn is available for a simulated MCU of the RL78/G10, RL78/G11, RL78/G12, RL78/G13, RL78/G13A, RL78/G14, RL78/G23, RL78/L12, or RL78/L23 group.

Target Devices

Type Title Date
Release Note PDF 283 KB 日本語
This document describes support features and important notes for using the RL78/G22 Simulator, which can simulate not only CPU instructions but also RL78/G22 peripheral functions. It lists supported RL78/G22 microcontrollers, changes, and precautions. Please read it before using the tool.
Release Note PDF 275 KB 日本語
This document describes support features and important notes for using the RL78/G23 Simulator, which can simulate not only CPU instructions but also RL78/G23 peripheral functions. It lists supported RL78/G23 microcontrollers, changes, and precautions. Please read it before using the tool.
Release Note PDF 294 KB 日本語
This document describes support features and important notes for using the RL78/L23 Simulator, which can simulate not only CPU instructions but also RL78/L23 peripheral functions. It lists supported RL78/L23 microcontrollers, changes, limitations, and precautions. Please read it before using the tool.
Release Note PDF 296 KB 日本語
This document describes support features and important notes for using the RL78/G24 Simulator, which can simulate not only CPU instructions but also RL78/G24 peripheral functions. It lists supported RL78/G24 microcontrollers, changes, and precautions. Please read it before using the tool.
Release Note PDF 183 KB 日本語
Release Note PDF 191 KB 日本語
Release Note PDF 187 KB 日本語
Release Note PDF 189 KB 日本語
Release Note PDF 192 KB 日本語
Release Note PDF 160 KB 日本語
Release Note PDF 204 KB 日本語
Release Note PDF 201 KB 日本語
Release Note PDF 190 KB 日本語
Tool News - Note PDF 84 KB 日本語
14 items

Support Communities

  1. Simulator GUI not starting

    ... says it connected to the simulator, but the Simulator GUI never starts (as the instructional video says it should).Could it be because I'm running in a VirtualBox VM (I'm on a Mac, so running E2Studio in a Windows VM)?  Is there a way to start it manually?

    Apr 1, 2022
  2. Unit testing for RL78 E2 Studio

    ... or missed?  Or anything do I need to do more to run that 'elf' file? The document I referred is 'How to use CUnit in e² studio'. It guides us to use CUnit for RX610. But implemented it for RL78. Is there problem while usinf CUnit for RL78? Thanks & ...

    Feb 9, 2022
  3. Getting Started with R5F212CCSNFP with e2 Studio.

    Hi!!   I am very new to Renesas microcontrollers - only familiar with AVR and PIC microcontrollers. I have just downloaded e2 studio with all options for all families ticked. But I am still not able to get started. I cannot find my controller R5F212CCSNFP in the target. Nor I am able ...

    Nov 19, 2019
View All Results from Support Communities (6)

Knowledge Base

  1. How to check connected debug tool(CS+)

    ... When you create a new project, a simulator is set for the debug tool by default. [Example 1] Display when the debug tool is a simulator in the RL78 familyRL78 Simulator[Example 2] Display when the debug tool is E2 emulator Lite in the RX familyRX E2 Lite[Example 3 ...

    Jun 28, 2017
  2. How can I measure an execution time for the specified interval? (e² studio; Cortex core devices, e.g. RA, RZ)

    Note: The following description covers Arm Cortex core-based device families (RA/RZ/RE/Synergy). For RX and RL78 families, please refer to FAQ 1011210. When the debugger is active, Run-Break time is shown at the bottom of the window in the status bar. Run-Break ...

    May 15, 2024
  3. Using the E1 or E20 emulator, is it possible to use the AZ78V4 performance analyzer to obtain a trace display for an application which is using the RI78V4 operating system? (E2, E2 Lite, E1, E20)

    No, it is not possible. This is because the AZ78V4 uses a record of data access to obtain a trace display. To use the AZ78V4 in tracing, you need to•    use IECUBE, or•    use a simulator.

    Mar 8, 2021
View All Results from Knowledge Base (5)