Skip to main content
Renesas Electronics Corporation

Overview

Description

The RZ Multi-OS Package is a software package for developing multi-OS solutions, consisting of the Flexible Software Package (FSP) as a software package for Renesas MPUs with Arm® Cortex®-M or Cortex-R core, and OpenAMP as a standardized API for framework for interprocessor communication.

Features

  • Inter-core communication between an RTOS-based core and a Linux-based core by OpenAMP.

Release Information

  • Mar 31, 2026: RZ Multi-OS Package v4.0.0
  • RZ/G series
    • Feb 6, 2026: Multi-OS Package v3.2.0
  • RZ/V series
    • Jan 13, 2026: Multi-OS Package v3.3.0
  • RZ/T series
    • Dec 26, 2025: Multi-OS Package v3.0.0
  • RZ/N series
    • Jan 30, 2026: Multi-OS Package v3.0.0

Target Devices

Downloads

Documentation

Design & Development

Sample Code

Related Boards & Kits

Videos & Training

News & Blog Posts

Additional Details

Please refer to the following information and documents to learn how to use the multi-OS package for each device.

RZ/G series

ItemRZ/G3ERZ/G3SRZ/G2L, G2LC, G2UL
Multi-OS Package V4.0.0Interprocessor communication (OpenAMP : Linux - FSP)Quick Start Guide (PDF)Quick Start Guide (PDF)Quick Start Guide (PDF)
Power Management AWO (Always On)AWO Example Project Start-up Guide (PDF)AWO Example Project Start-up Guide (PDF)-
RZ Flexible Software PackageV4.0.0V4.0.0V4.0.0
Linux Software PackageRZ/G3E Linux BSP v1.0.0VLP V3.0.7VLP V3.0.7
VLP V4.0.1

RZ/V series

ItemRZ/V2NRZ/V2HRZ/V2L
Multi-OS Package V4.0.0Interprocessor communication (OpenAMP : Linux-FSP)Quick Start Guide (PDF)Quick Start Guide (PDF)Quick Start Guide (PDF)
Power Management AWO (Always On)AWO Example Project Start-up Guide (PDF)AWO Example Project Start-up Guide (PDF)-
RZ Flexible Software PackageV4.0.0V4.0.0V4.0.0
Linux Software Package--VLP V3.0.7
AI Software Development Kit (SDK)RZ/V2N AI-SDK V6.3.0RZ/V2H AI-SDK V6.00-

RZ/N series

ItemRZ/N2H
Multi-OS Package V4.0.0Interprocessor communication (OpenAMP : Linux - FSP)Application Note (PDF)
Interprocessor communication (OpenAMP : FSP - FSP)Quick Start Guide (PDF)
RZ Flexible Software PackageV4.0.0
Verified Linux PackageVLP V5.0.0

RZ/T series

ItemRZ/T2H
Multi-OS Package V4.0.0Interprocessor communication (OpenAMP : Linux - FSP)Application Note (PDF)
Interprocessor communication (OpenAMP : FSP - FSP)Quick Start Guide (PDF)
RZ Flexible Software PackageV4.0.0
Verified Linux PackageVLP V5.0.0

For more information about the RZ FSP, please refer to the RZ Flexible Software Package (FSP) software page.

Operating Environment

Integrated Development Environmente2 studio Integrated Development Environment, default toolchain is GCC Arm Embedded
EmulatorSEGGER (J-Link Series)

Support

Support Communities

  1. RTOS sample related to RZG Multi OS package

    Hi all The sample codes of RZ/G Multi-OS Package V2.3.0 are in FSP 2.1.0. Currently, RZG's latest FSP is 3.0.0, and there are many additional features, so I would like to evaluate it as FSP 3.0.0, but it ...

    May 29, 2025
  2. RZG2UL: Running M33 core application from Uboot

    We are testing M33 core on RZG2UL evk board.We tested rpmsg demo application given along with vlp3.0.1 BSP and it is working.After compiling blinky application in e2studio for G2UL evk blinky.elf binary is generated.Should we use JTAG only for testing applications on M33 core ...

    Apr 19, 2023
  3. Data sharing between M-33 cortex and A-53 Processor

    Hi , We are planning to use Rz/v2l for our requirement. How M-33 Microcontroller unit can communicate with A-53 cores. We will be running Linux on the MPU and would like to do data exchange between Linux user-space applications and M-33 cores.  What are the ...

    Jun 8, 2023
View All Results from Support Communities (17)

Knowledge Base

  1. RZ/G2L, LC: Communication between OS

    We provide RZ/G2L CM33 Multi-OS Package that can use OpenAMP which is an API with a standardized framework for communication between processors. https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rz-arm-based-high-end-32-64-bit-mpus ...

    Oct 27, 2021
  2. RZ/G3S: Communication between OS

    We provide RZ/G3S Multi-OS Package that can use OpenAMP which is an API with a standardized framework for communication between processors.  By using this package, you can use Free RTOS with Cortex-M33 and create an application that links Linux and RTOS using OpenAMP. Please also refer ...

    Jan 16, 2024
  3. RZ Family: Using power saving mode and wakeup by CAN signal on RZ/V2H

    ... the CAN signal and reboot Linux on core CA55. For this solution, a multi-OS package is required. The implementation instructions can be found here: RZ/V Multi-OS Package. Important Notice:  When this article is written (September, 2025), RZ/V2H does not support "Suspend to RAM" on ...

    Nov 14, 2025
View All Results from Knowledge Base (5)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?