Overview
Description
Topics
The RX Driver Package V1.49 released. Various existing FIT modules have also been updated.
Learn More (Application Note: RX Family RX Driver Package Ver.1.49 (PDF | English, 日本語))
RX Driver Package Software Platform Helps Speed Up Time to Market
The RX Driver Package is a software package for using such basic functions as initializing MCUs, programming flash memory by self-programming, timer control, UART communications, and A/D conversion, and application functions such as USB and Ethernet transfer and control. The software are provided as the Firmware Integration Technology (FIT) modules.
Components
- FIT middleware module
- FIT peripheral function module
- Board support package (BSP) module
Features
- This package allows you to start using the peripheral functions of RX MCUs at once, and can shorten times taken in considering prototypes.
- Applications which utilize Firmware Integration Technology (FIT) can be used for all RX-series products, and can reduce the cost of developing software as you expand your product development.
Release Information
Latest Ver.: V1.49
Released: Mar. 31, 26
Details of upgrade (See Application Note: RX Family RX Driver Package Ver.1.49 (PDF | English, 日本語))
Operating Environment
Other downloads
List of FIT Modules: This is a list of FIT modules and devices they support. You can download the list as an .xlsx or .pdf file.
List of FIT Modules (XLSX) List of FIT Modules (PDF)
Previous Versions : Download the previous versions of RX Driver Package
FAQ
| 内容 |
|---|
| FAQ 2000571 : Flash Self-Programming |
| FAQ 2000510 : RX Family SCI Troubleshooting |
| FAQ 2001203 : About using FIT module and RTOS in combination |
Target Devices
Videos & Training
Learn how to run the demo program with the CAN API module on RX microcontrollers using the Starter Kit+ for RX671. The CAN API makes it simple to work with the built-in CAN bus interface, and the demo highlights the different modes it supports, including internal loopback, external loopback, and listen-only.
News & Blog Posts
Blog Post Jan 23, 2023 |
Blog Post Sep 1, 2022 |
Blog Post Feb 1, 2022 |
Additional Details
Operating Environment
| Type | Product Name |
|---|---|
| IDE | e² studio CS+ IAR Embedded Workbench for Renesas RX |
| Cross tool | C/C++ Compiler Package for RX Family IAR C/C++ Compiler for Renesas RX GCC for Renesas RX |
How to Obtain
Please download the RX Driver Package from the link below.
- You can confirm the device support status of each Firmware Integration Technology module included in the latest version of the RX Driver Package by viewing the List of FIT Modules ( XLSX version or PDF version ).
- The list of version information for Firmware Integration Technology modules included in the RX Driver Package can be confirmed by consulting RX Family List of Firmware Integration Technology modules included with RX Driver Package (PDF | English, 日本語) (R01AN5976).
| Product Name | Doc Number (Program Name) | Download | Released | Target Device |
|---|---|---|---|---|
| RX Family RX Driver Package Ver.1.49 | R01AN8228 | RX Family RX Driver Package Ver.1.49 - Sample Code (ZIP) | Mar. 31, 26 | RX110, RX111, RX113, RX130, RX13T, RX140, RX14T, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX260, RX261, RX64M, RX65N, RX651, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
Previous Versions
| Product Name | Doc Number (Program Name) | Download | Released | Target Device |
|---|---|---|---|---|
| RX Family RX Driver Package Ver.1.48 | R01AN8121 | RX Family RX Driver Package Ver.1.48 - Sample Code (ZIP) | Nov. 20, 25 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX260, RX261, RX64M, RX65N, RX651, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.47 | R01AN7754 | RX Family RX Driver Package Ver.1.47 - Sample Code (ZIP) | Apr. 21, 25 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX260, RX261, RX64M, RX65N, RX651, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.46 | R01AN7577 | RX Family RX Driver Package Ver.1.46 - Sample Code (ZIP) | Jan. 20, 25 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX260, RX261, RX64M, RX65N, RX651, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.45 | R01AN7470 | RX Family RX Driver Package Ver.1.45 - Sample Code (ZIP) | Oct. 15, 24 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX260, RX261, RX64M, RX65N, RX651, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.44 | R01AN7446 | RX Family RX Driver Package Ver.1.44 - Sample Code (ZIP) | Aug. 9, 24 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX64M, RX65N, RX651, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.42 | R01AN7163 | RX Family RX Driver Package Ver.1.42 - Sample Code (ZIP) | Jan. 23, 24 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX64M, RX65N, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.41 | R01AN6907 | RX Family RX Driver Package Ver.1.41 - Sample Code (ZIP) | Aug. 25, 23 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX64M, RX65N, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.40 | R01AN6906 | RX Family RX Driver Package Ver.1.40 - Sample Code (ZIP) | Aug. 25, 23 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23E-B, RX23T, RX23W, RX24T, RX24U, RX26T, RX64M, RX65N, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.39 | R01AN6905 | RX Family RX Driver Package Ver.1.39 - Sample Code (ZIP) | May 24, 23 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX26T, RX64M, RX65N, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.37 | R01AN6721 | RX Family RX Driver Package Ver.1.37 - Sample Code (ZIP) | Jan. 20, 23 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX64M, RX65N, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.36 | R01AN6515 | RX Family RX Driver Package Ver.1.36 - Sample Code (ZIP) | Aug. 1, 22 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX64M, RX65N, RX660, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.34 | R01AN6323 | RX Family RX Driver Package Ver.1.34 - Sample Code (ZIP) | Apr. 20, 22 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.33 | R01AN6073 | RX Family RX Driver Package Ver.1.33 - Sample Code (ZIP) | Jan. 20, 22 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.32 | R01AN6013 | RX Family RX Driver Package Ver.1.32 - Sample Code (ZIP) | Sep. 22, 21 | RX110, RX111, RX113, RX130, RX13T, RX140, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.31 | R01AN5975 | RX Family RX Driver Package Ver.1.31 - Sample Code (ZIP) | Sep. 1, 21 | RX110, RX111, RX113, RX130, RX13T, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX671, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.30 | R01AN5882 | RX Family RX Driver Package Ver.1.30 - Sample Code (ZIP) | Jun. 30, 21 | RX110, RX111, RX113, RX130, RX13T, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.29 | R01AN5826 | RX Family RX Driver Package Ver.1.29 - Sample Code (ZIP) | Apr. 16, 21 | RX110, RX111, RX113, RX130, RX13T, RX230, RX231, RX23E-A, RX23T, RX23W, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.27 | R01AN5600 | RX Family RX Driver Package Ver.1.27 - Sample Code (ZIP) | Nov. 28, 20 | RX110, RX111, RX113, RX130, RX13T, RX23W, RX230, RX231, RX23E-A, RX23T, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.26 | R01AN5401 | RX Family RX Driver Package Ver.1.26 - Sample Code (ZIP) | May 29, 20 | RX110, RX111, RX113, RX130, RX13T, RX23W, RX230, RX231, RX23E-A, RX23T, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.25 | R01AN5371 | RX Family RX Driver Package Ver.1.25 - Sample Code (ZIP) | Apr. 7, 20 | RX110, RX111, RX113, RX130, RX13T, RX23W, RX230, RX231, RX23E-A, RX23T, RX24T, RX24U, RX64M, RX65N, RX66N, RX66T, RX71M, RX72M, RX72N, RX72T |
| RX Family RX Driver Package Ver.1.24 | R01AN5267 | RX Family RX Driver Package Ver.1.24 - Sample Code (ZIP) | Mar. 31, 20 | RX110, RX111, RX113, RX130, RX13T, RX23W, RX230, RX231, RX23E-A, RX23T, RX24T, RX24U, RX64M, RX65N, RX66T, RX71M, RX72M, RX72T |
| RX Family RX Driver Package Ver.1.23 | R01AN4976 | RX Family RX Driver Package Ver.1.23 - Sample Code (ZIP) | Dec. 16, 19 | RX110, RX111, RX113, RX130, RX23W, RX230, RX231, RX23E-A, RX23T, RX24T, RX24U, RX64M, RX65N, RX66T, RX72M, RX71M, RX72T |
| RX Family RX Driver Package Ver.1.22 | R01AN4873 | RX Family RX Driver Package Ver.1.22 - Sample Code (ZIP) | Sep. 13, 19 | RX110, RX111, RX113, RX130, RX23W, RX230, RX231, RX23T, RX24T, RX24U, RX64M, RX65N, RX66T, RX72M, RX71M, RX72T |
| RX Family RX Driver Package Ver.1.20 | R01AN4794 | RX Family RX Driver Package Ver.1.20 - Sample Code (ZIP | English, 日本語) | Jul. 22, 19 | RX110, RX111, RX113, RX130, RX230, RX231, RX23T, RX24T, RX24U, RX64M, RX65N, RX66T, RX71M, RX72T |
| RX Family RX Driver Package Ver.1.19 | R01AN4677 | RX Family RX Driver Package Ver.1.19 - Sample Code (ZIP | English, 日本語) | May 13, 19 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX24U, RX63N, RX64M, RX65N, RX66T, RX71M, RX72T |
| RX Family RX Driver Package Ver.1.18 | R01AN4659 | RX Family RX Driver Package Ver.1.18 - Sample Code (ZIP | English, 日本語) | Feb. 28, 19 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX24U, RX63N, RX64M, RX65N, RX66T, RX71M |
| RX Family RX Driver Package Ver.1.16 | R01AN4471 | RX Family RX Driver Package Ver.1.16 - Sample Code (ZIP | English, 日本語) | Nov. 27, 18 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX24U, RX63N, RX64M, RX65N, RX66T, RX71M |
| RX Family RX Driver Package Ver.1.15 | R01AN4372 | RX Family RX Driver Package Ver.1.15 - Sample Code (ZIP | English, 日本語) | Jul. 27, 17 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX24U, RX63N, RX64M, RX65N, RX71M |
| RX Family RX Driver Package Ver.1.14 | R01AN4191 | RX Family RX Driver Package Ver.1.14 - Sample Code (ZIP | English, 日本語) | Mar. 31, 17 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX24U, RX63N, RX64M, RX65N, RX71M |
| RX Family RX Driver Package Ver.1.13 | R01AN3859 | RX Family RX Driver Package Ver.1.13 - Sample Code (ZIP | English, 日本語) | Oct. 20, 17 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX24U, RX63N, RX64M, RX65N, RX71M |
| RX Family RX Driver Package Ver.1.12 | R01AN3651 | RX Family RX Driver Package Ver.1.12 - Sample Code (ZIP | English, 日本語) | Apr. 5, 17 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX24U, RX63N, RX64M, RX65N, RX71M |
| RX Family RX Driver Package Ver.1.11 | R01AN3467 | RX Family RX Driver Package Ver.1.11 - Sample Code (ZIP | English, 日本語) | Oct. 13, 16 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX63N, RX64M, RX65N, RX71M |
| RX Family RX Driver Package Ver.1.10 | R01AN3345 | RX Family RX Driver Package Ver.1.10 - Sample Code (ZIP | English, 日本語) | Jul. 15, 16 | RX110, RX111, RX113, RX130, RX210, RX230, RX231, RX23T, RX24T, RX63N, RX64M, RX71M |
| RX64M, RX71M Group RX Driver Package Ver.1.02 | R01AN2606 | RX64M, RX71M Group RX Driver Package Ver.1.02 - Sample Code (ZIP | English, 日本語) | May 16, 16 | RX64M, RX71M |
| RX110, RX111, RX113, RX130, RX230, RX231, RX23T, RX24T Group RX Driver Package Ver.1.03 | R01AN3233 | RX110, RX111, RX113, RX130, RX230, RX231, RX23T, RX24T Group RX Driver Package Ver.1.03 - Sample Code (ZIP | English, 日本語) | Apr. 15, 16 | RX110, RX111, RX113, RX130, RX230, RX231, RX23T, RX24T |
| RX110, RX111, RX113, RX130, RX231, RX23T Group RX Driver Package Ver.1.02 | R01AN3159 | RX110, RX111, RX113, RX130, RX231, RX23T Group RX Driver Package Ver.1.02 - Sample Code (ZIP | English, 日本語) | Feb. 29, 16 | RX110, RX111, RX113, RX130, RX231, RX23T |
| RX110, RX111, RX113, RX231 Group RX Driver Package Ver.1.01 | R01AN2670 | RX110, RX111, RX113, RX231 Group RX Driver Package Ver.1.01 - Sample Code (ZIP | English, 日本語) | Oct. 31, 15 | RX110, RX111, RX113, RX231 |
Support
Support Communities
- RX Family RX Driver Package
Hello everybody.Why is the R63N not listed in the driver package?www.renesas.com/.../D4800289.htmlI can only find the following chips:Applicable ProductsRX110RX111RX113RX130RX13TRX231, RX230RX23E-ARX23TRX23WRX24TRX24URX64MRX65N, RX651RX66NRX66TRX71MRX72MRX72NRX72TGreetings Simon
Oct 28, 2020 - Getting Error while downloading RX Family RX Driver Package Ver 1.44
Hi, When I am trying to download RX Family RX Driver Package Ver 1.44, I am getting error as shown below, HTTP Status Error (404 not found) 1.when I Opened the project created with RX 111 Group on e2 studio,2.I am seeing the pop up, FIT ...
Sep 23, 2024 - PWM Driver in FIT RX Driver Package v1.20
Hello, Is there a PWM driver available in the FIT RX Driver Package v1.20? I am unable to find any. I see that MTU is listed under the Package diagram in the application note however an MTU driver is not available as such. If not available, what are the ...
Sep 30, 2019
Knowledge Base
- About using FIT module and RTOS in combination
... use R_BSP_InterruptsDisable() and R_BSP_InterruptsEnable().These APIs execution section should interrupt disabled or enabled. Please refer to the URL below for details.RX Driver Package:https://www.renesas.com/en/software-tool/rx-driver-packageSupplement: Have you verified operations of FIT modules ...
Dec 24, 2024 - Adding FIT Module for QE for Capacitive Touch on Smart Configurator
... then click ‘Download more software components’. b. Select the region, and log in to your account using My Renesas ID. c. Uncheck the filter ‘Show RX Driver Package only’, then select the FIT modules for QE for Capacitive Touch for download. (2) Download the FIT modules for installation from Renesas ...
Jul 18, 2019 - How to add a FIT module to an RI600V4 or RI600PX sample project using FIT (CS+ version)
1. Add the folder of FIT module source files to the project. Copy the folder of required FIT module source files from software modules, such as RX Driver Package, to the project root.In Windows Explorer, drag and drop the copied folder to the “File” folder of the CS+ Project ...
May 17, 2017