Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Topics
QE for USB V2.0.0 Release Note (PDF | English, 日本語)
- Supports RA2L2 of the RA Family
  Supports USB Type-C debugging function for RA2L2 Type-C
- Supports Workflow view

QE for USB is a tool for embedded software development currently supports system development involving the USB modules. It eases the debugging of USB systems, shortening development periods and lowering costs. USB peripheral functionality is supported.

By expanding the existing integrated development environment (IDE), it will help in resolving problems in development for systems which use the USB such as :
"How do I actually include the USB in my embedded application?"
"It seems the USB is not connecting even though I've included the code."

This product is a plug-in which extends the Renesas IDE "e² studio". You can download and utilize it free of charge.

Features

  • View transitions of the USB state at a glance: [USB State Chart (QE)] view
  • The registers to be set are listed, and pop-up messages indicate errors in settings: [USB Setting Registers (QE)] view
  • Check the settings for USB descriptors in a dedicated list: [USB Descriptors (QE)] view
  • Learn More

Release Information

Product NameLatest Ver.ReleasedTarget Device (Note1)Details of upgradeDownloadOperating Environment
QE for USBV2.0.0Jun 10, 2025RA Family
RL78 Family
RX Family
See Release NoteDownloade² studio plug-in(Note2) 
Operating Environment

Notes

  1. For details on supported MCUs, refer to the section Target Devices.
  2. We recommend using the e² studio installer provided for the RA Family for customers using RA Family. For details, see the GitHub page on the Flexible Software Package (FSP).

Target Devices

Type Title Date
Software & Tools - Software
Log in to Download ZIP 5.31 MB 日本語
Software & Tools - Other
Log in to Download ZIP 2.18 MB 日本語
2 items
Type Title Date
Release Note PDF 405 KB 日本語
Flyer PDF 752 KB 日本語 , 简体中文
Tool News - Release PDF 261 KB 日本語
Application Note PDF 1.58 MB 日本語
AI-generated Summary: The document provides detailed instructions for installing QE for USB using the e2 studio environment. It guides users through accessing the software via Renesas' website or the e2 studio smart browser, adding the repository by selecting the downloaded zip file, and completing installation by accepting license agreements and security certificates. The process includes restarting e2 studio to finalize the setup.
Release Note PDF 222 KB 日本語
Tool News - Release PDF 161 KB 日本語
Tool News - Release PDF 272 KB
7 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 2.51 MB 日本語
1 item

Related Boards & Kits

Functions

View transitions of the USB state at a glance: [USB State Chart (QE)] view

A state chart of the USB connection (enumeration) process is displayed in real-time. As well as confirming the success of connection, the user can visually check the state and timing where processing stopped when connection has failed, which enables a problem to be quickly solved.

Image
[USB State Chart (QE)] view

The registers to be set are listed, and pop-up messages indicate errors in settings: [USB Setting Registers (QE)] view

The register values and descriptions related to the settings for USB connection are indicated. If a register is not set to a correct value needed for connection, it is marked "NG" (no good) and the user can find problems simply by opening this view. For some MCUs, the tool also supports another feature where placing the mouse cursor over a register value in the view pops up a message with the meaning of the value so the user can see how to correct the setting.

Image
[USB Setting Registers (QE)] view

Check the settings for USB descriptors in a dedicated list: [USB Descriptors (QE)] view

This is a list of the descriptor values and states which are set in the process of USB connection (enumeration). If the value of a descriptor is incorrect, it is marked "NG". A single-click on an "NG" location will cause a jump to the corresponding source code so the user can immediately edit it.

Image
[USB Descriptors (QE)] view