Skip to main content
Renesas Electronics Corporation

Description

The Renesas Starter Kit for RX231 (B Mask: built-in Trusted Secure IP) is the perfect starter kit for developers who are new to the RX231. The kit includes an LCD display module, on-chip debugging emulator, and integrated development environment so you can start evaluating the RX231 immediately after opening the box. Please use this product to experience the performance and functions of the RX231.

About the bundled emulator

We have already discontinued production of the E1 emulator due to components of the product having reached their EOL (end of life, i.e. end of production). Please click on the following link to confirm the details and our successor products.
[Notification] End of Life (EOL) Notice for E1 Emulator (PDF | English, 日本語)

The Renesas Starter Kit which includes the E1 emulator is for sale as long as stocks last. There are no changes to the included emulator.
After stock of the Kit with E1 emulator ends, the kit will not include the E1 emulator.
[Notification] End of Life (EOL): Renesas Starter Kits with E1 Emulator (PDF | English, 日本語)
The IDE and flash programmer of the DVD-ROM do not support the E2 emulator and E2 emulator Lite. When you use either of the emulators, download the latest tool from the Renesas website.

Touch Demonstration Project
The RSKRX231B includes a simple demonstration project to showcase the touch functionality of the RX231 device.
As a customer touch project is dependent not only on the embedded code, but also on a PC tuning application that is specific to the selected compiler and IDE.
Capacitive Touch Sensor System (Second-Generation Capacitive Touch Technology)

Features

  • RX231 builds in Trusted Secure IP. AES encryption function and robust key management can be evaluated.
  • Supports SDHI. If an optional Wireless LAN expansion board package for RSK (RTK0ZZZZZZP00000BR#WS) is used, Wireless LAN can evaluated.
  • Touch feature (self-capacitive type) can be evaluated.
  • 1 channel USB Function and 1 channel USB Host can be evaluated.
  • In addition, CAN, IIC, etc. can be evaluated.
  • Required IBM-PC compatible PC (need USB interface, Processor 1GHz over), OS: Windows 8/7/Vista (other than the listed OS is not supported)

Applications

  • Washing Machine, Refrigerator, IH Cooking Heater, Touch Sensor System, FA Equipment, Office Equipment, Washing Toilet Seat, Security System, Access Control, Alarm Control, Detector, HMI, Building Management System, IoT, Smart Meter
Type Title Date
Tool News - Release PDF 261 KB 日本語
Tool News - Release PDF 210 KB 日本語
Tool News - Release PDF 236 KB 日本語
Tool News - Notification PDF 153 KB 日本語
Application Note PDF 497 KB
AI-generated Summary: The document guides users through importing sample projects for the RX231 Group Renesas Starter Kit into the e2 studio IDE using CC-RX. It details selecting the 'Go to e2 studio workbench' on the welcome screen, choosing 'Import' from the menu, and navigating the import wizard to load existing projects from an archive file. The sample code includes multiple projects such as Application, Async_Serial, Low_Power_Mode, RTC, System_BootLoader, Timer_PWM, Touch, and Tutorial. Users locate the project ZIP file and import these projects into their workspace for development and testing.
Tool News - Note PDF 237 KB 日本語
Application Note PDF 536 KB
AI-generated Summary: The RX231 Group Renesas Starter Kit sample code includes multiple projects demonstrating peripheral initialization and functionality using CS+ for CC-RX. Users open the tutorial project file to access source code and dependent files organized by type. Each project contains sample code for specific peripherals and a Description.txt explaining its function. The code supports debugging and plug-ins such as Pin Configurator and Program Analyzer. The sample code updates include improvements to system bootloader projects and development environment upgrades, including IDE and compiler versions.
Tool News - Note PDF 149 KB 日本語
Tool News - Note PDF 148 KB 日本語
Manual - Development Tools PDF 2.07 MB 日本語
Manual - Development Tools PDF 2.75 MB 日本語
Manual - Development Tools PDF 215 KB 日本語
Manual - Development Tools PDF 1.53 MB 日本語
Manual - Development Tools PDF 248 KB
Manual - Development Tools PDF 1.17 MB
Quick Start Guide PDF 2.70 MB
Manual - Development Tools PDF 111 KB
17 items

Software & Tools

Software Downloads

Type Title Date
Board Description File ZIP 1 KB
Software & Tools - Other
Log in to Download ZIP 554 KB
2 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 10.72 MB Compiler: CC-RX IDE: e2 studio
Sample Code
Log in to Download ZIP 13.02 MB 日本語 Compiler: CC-RX IDE: CS+
2 items
Part NumberStatusStockBudgetary Price (USD)DescriptionDebugger supplied
R0K505231S920BEActiveOut of Stock1u | $258.82Renesas Starter Kit for RX231 (B Mask: Built-in Trusted Secure IP)None