Overview
The Renesas Starter Kit for RL78/G1C is intended as a user-friendly introductory and evaluation tool for the RL78/G1C microcontroller. The board provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging using CubeSuite+.
The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run, only minutes after opening the box. It can also prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.
Note: CubeSuite+ is not generally promoted to the U.S. and European customers. Customers in the U.S. and Europe ,who are interested in CubeSuite+, are requested to contact our regional marketing departments for details.
Features
- Renesas microcontroller programming
- User code debugging
- User circuitry such as switches, LEDs, and a potentiometer
- Sample application
- Sample peripheral device initialization code
Sample & Buy
Renesas Starter Kit for RL78/G1C (Kit with CubeSuite+)
| Description: | Renesas Starter Kit for RL78/G1C (Kit with CubeSuite+) |
| Debugger supplied: | None |