Overview
Build Smart Sensor Products with Real-Time Bluetooth Connectivity
Accelerate the development of connected sensor products with a ready-to-evaluate project that acquires live 3-axis motion data and transmits it to a Bluetooth Low Energy (LE) client. The solution combines the Renesas RA6E2 MCU, a DA14531 Bluetooth LE module, and an ICM42670 motion sensor in a modular prototype designed for rapid evaluation and reuse.
The reference application uses interrupt-driven sensing, configurable data filtering, and (GATT Generic Attribute Profile) notifications to deliver responsive sensor telemetry without a fixed polling loop. A connected client can also adjust the sensor output data rate at runtime, helping developers explore the balance between responsiveness, data volume, and power-oriented system behavior.