Skip to main content

Overview

Description

Topics
QE for USB V2.0.0 Release Note (PDF | English, 日本語)
- Supports RA2L2 of the RA Family
  Supports USB Type-C debugging function for RA2L2 Type-C
- Supports Workflow view

QE for USB is a tool for embedded software development currently supports system development involving the USB modules of RX family and RL78 family devices. It eases the debugging of USB systems, shortening development periods and lowering costs.

By expanding the existing integrated development environment (IDE), it will help in resolving problems in development for systems which use the USB such as :
"How do I actually include the USB in my embedded application?"
"It seems the USB is not connecting even though I've included the code."

This product is a plug-in which extends the Renesas IDE "e² studio". You can download and utilize it free of charge.

Features

  • View transitions of the USB state at a glance: [USB State Chart (QE)] view
  • The registers to be set are listed, and pop-up messages indicate errors in settings: [USB Setting Registers (QE)] view
  • Check the settings for USB descriptors in a dedicated list: [USB Descriptors (QE)] view
  • Learn More

Release Information

Product NameLatest Ver.ReleasedTarget Device (Note1)Details of upgradeDownloadOperating Environment
QE for USBV2.0.0Jun 10, 2025RA Family
RL78 Family
RX Family
See Release NoteDownloade² studio plug-in(Note2) 
Operating Environment

Notes

  1. For details on supported MCUs, refer to the section Target Devices.
  2. We recommend using the e² studio installer provided for the RA Family for customers using RA Family. For details, see the GitHub page on the Flexible Software Package (FSP).

Target Devices

Downloads

Documentation

Design & Development

Sample Code

Related Boards & Kits

Support

Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?

Videos & Training

Additional Details

Functions

View transitions of the USB state at a glance: [USB State Chart (QE)] view

A state chart of the USB connection (enumeration) process is displayed in real-time. As well as confirming the success of connection, the user can visually check the state and timing where processing stopped when connection has failed, which enables a problem to be quickly solved.

Image
[USB State Chart (QE)] view

The registers to be set are listed, and pop-up messages indicate errors in settings: [USB Setting Registers (QE)] view

The register values and descriptions related to the settings for USB connection are indicated. If a register is not set to a correct value needed for connection, it is marked "NG" (no good) and the user can find problems simply by opening this view. For some MCUs, the tool also supports another feature where placing the mouse cursor over a register value in the view pops up a message with the meaning of the value so the user can see how to correct the setting.

Image
[USB Setting Registers (QE)] view

Check the settings for USB descriptors in a dedicated list: [USB Descriptors (QE)] view

This is a list of the descriptor values and states which are set in the process of USB connection (enumeration). If the value of a descriptor is incorrect, it is marked "NG". A single-click on an "NG" location will cause a jump to the corresponding source code so the user can immediately edit it.

Image
[USB Descriptors (QE)] view