DALI Communication

DALI is an international communication standard for lighting specified in IEC 62386. Communication takes place between a master (control device) and slaves (control gear). The DALI standard supports a single control device, which can control up to 64 items of control gear.

 

DALI Standard Listing

Source: Digital Illumination Interface Alliance

 

DALI Standard Listing

One feature of DALI is that the entire setup is standardized systematically. Data transfer route basics are covered by 101, control gear by 102, control devices by 103, and so on. Control devices include routers, switches, and motion or light sensors. Control gear includes lighting fixtures. There are also upper-level standard numbers (2xx and 3xx) that cover characteristics

Advancing to DALI-2

A new DALI standard, DALI-2, is currently coming into use. DALI-2 defines new applications, adds new functions, and improves compatibility to better meet the lighting requirements of customers. Also, a device must pass an official test to receive certification of compliance with the standard. Renesas was the first semiconductor device manufacturer to join the DALI standardization organization. This enables us to deliver solutions that track the latest trends in the standard and include a tested protocol stack by official DALI tester.

Implementing Task/Ambient Lighting with DALI

“Task/ambient lighting” means that different types of lighting are used for “tasks” such as desks and for “ambient” areas such as floors and corridors. Some features of task/ambient lighting are that it can boost work efficiency by allowing adjustment of the brightness and hue to match individual preferences, and that it can boost energy efficiency by providing only the amount of night needed in each location.
Further energy savings can be achieved by, for example, using motion sensors to detect when people are around, allowing the lights to be extinguished automatically when not needed, or using light sensors to detect light from outside, which can be taken into account when controlling brightness. Figure 3 shows an example of task/ambient lighting using DALI.

 

Example of Task/Ambient Lighting Using DALI

Example of Task/Ambient Lighting Using DALI

This task/ambient lighting configuration allows individual control of the lighting of task areas such as desks and of ambient areas such as floors and corridors. The lighting fixtures, sensors, and switches are all connected via DALI, and alternatively a unit such as a lighting controller can be used to provide centralized management. In this way DALI can be used to link and control all essential devices, making it easy to implement task/ambient lighting.

Solutions

The Evaluation Systems for LED Solutions

The hardware listed below is available for LED lighting evaluation, enabling customers to create a development environment that matches their products.

Software Development Environment (DALI Protocol Stack)

The Renesas LED lighting solution supports the DALI ed. 2.0 international lighting communication standard.