Skip to main content
Renesas Electronics Corporation
Alternative(s) Available
CK-RX65N - Cloud Kit Based on RX65N MCU Group
  • Notes:For developing IoT devices with the RX65N, it is recommended to use the latest evaluation kit CK-RX65N. CK-RX65N v1 supports LTE CAT-M1 and Ethernet, while CK-RX65N v2 supports Wi-Fi and Ethernet for cloud connectivity.

Overview

Description

The Renesas RX65N Cloud Kit is an RX65N microcontroller-based cloud communications evaluation kit which is an ideal evaluation environment for IoT device developers. You can easily provide Wi-Fi connectivity to Amazon Web Services (AWS) and Microsoft Azure (Azure) to help start developing IoT devices.

The kit includes a Wi-Fi communication module, a temperature and humidity sensor, an optical sensor, a 3-axis acceleration sensor, a USB port for serial communication, and a USB port for debugging. The sensor data that is uploaded to AWS and Azure from this kit can be observed on cloud services. In addition, the e2 studio integrated development environment has been enhanced for this kit. The network stack for FreeRTOS and Azure RTOS, the configuration of component libraries, and the generation of source code can be done within e2 studio.

The RX65N microcontroller included in this kit is a next-generation general-purpose MCU with a human machine interface (HMI) and security features that are ideal for IoT edge devices. The built-in dual-bank capability and trusted secure IP features make secure cloud communications and firmware updates both easy and robust.

*The "Renesas web dashboard" has been discontinued in 2022 because it can be replaced by AWS or Azure services.

Cloud Connectivity Sample Program

AWS Certified Program

Microsoft Certified Programs

Features

  • Securely and reliably connect to cloud services
    • The Renesas RX65N Cloud Kit, combined with a real-time OS from cloud services has the following certifications:
      • AWS FreeRTOS certification
      • Microsoft Azure RTOS certification
  • Assists in IoT device prototyping
    • Free editing and debugging sample programs for AWS and Azure communications.
    • Comprehend the behavior of the sample programs from the application notes.
  • Reduction in actual product development manhours
    • The sample programs are based on the real-time OS provided by cloud service. You can leverage the large ecosystem of existing tools that have been developed for FreeRTOS and Azure RTOS kernels.
    • You can easily program commonly needed IoT features to devices using the software library embedded in the real-time OS by cloud service.

Evaluate cloud communications using a variety of programs

  • Basic AWS communications program
    • Sends a "Hello World" text message to the AWS cloud at regular intervals
    • FreeRTOS certified
    • Communicates wirelessly using Wi-Fi
  • Program for uploading sensor and other data to the AWS cloud, and for observing the information in the dashboard
    • Sends data from its three on-board sensors to the AWS cloud at regular intervals
    • Allows for observation of the sensor data in the dashboard
  • Azure IoT plug and play certified programs
    • Connects to Azure Central without coding, and monitors sensor data in a dashboard
  • A program that uploads sensor data to Microsoft Azure, and then monitors it on Azure IoT Explorer's Telemetry
    • Send MCU temperature data to Azure Cloud at regular intervals
    • Monitor sensor data with Telemetry in Azure IoT Explorer
  • A variety of sample programs that can be utilized to develop IoT devices

Applications

Documentation

Design & Development

Software & Tools

Software Downloads

Sample Code

Related Boards & Kits

Product Options

Applied Filters:

Videos & Training

Support

Support Communities

  1. Rx65N Cloud Connectivity Kit - Firmware Download Issue

    Hi  I'm trying to download the freeRTOS firmware for aws cloud connectivity to the RX65N cloud kit and encountering the error.  I have plugged in all three USB cable(thru an external USB adaptor), since the laptop has only one USB port. Please advise how to get this working ...

    Apr 28, 2020
  2. LWIP porting on RX64M starter kit

    Hi All, Is there any LWIP example code for RX64M starter kit?? Regards, Mayur

    Jun 6, 2022
  3. CK-RX65N Quick Start

    Quick Start Guide for CK-RX65N mentions Example Project Bundle: There are no example projects following the link, where I could find them?

    Apr 25, 2024
View All Results from Support Communities (7)

Knowledge Base

  1. If I use Renesas RX65N Cloud Kit to connect to AWS Cloud, do I need to create an AWS account?

    Yes, Renesas does not provide it. Please prepare your own AWS account for yourself.   [Tags]   FAQNo:2000623,   JFAQNo:2000623,   CFAQNo:2000623

    Aug 20, 2019
  2. Is it possible to incorporate the Renesas RX65N Cloud Kit into products?

    No, the Renesas RX65N Cloud Kit is intended for development and evaluation. It is not intended to be incorporated into products.   [Tags]   FAQNo:2000622,   JFAQNo:2000622,   CFAQNo:2000622

    Aug 20, 2019
  3. Getting Started with the RL78/G24 DALI 102+207+209 Reference Solution

    ... Boards Control Gear: RL78/G24 DC/DC LED Control Evaluation Board Control Device (Application Controller): RL78/G23 Lighting Communication Master Evaluation BoardRX65N Cloud Kit+DALI-2 Option Board (support board no longer available) Control Device (Input Device): RL78/G23 Lighting Communication Master Evaluation Board The ...

    Sep 24, 2026