Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The SmartBond™ devices are supported by a comprehensive set of software tools, such as:

  • SmartSnippets™ Studio
  • SmartSnippets™ Toolbox
  • SmartBond™ Flash Programmer
  • Production Line Tool Kit

SmartSnippets™ Studio is a royalty-free software development platform for SmartBond™ devices. It fully supports the DA14531, DA14531-01, DA14580/581/583, DA1585/586, DA1468x, DA1469x, and DA1470x families of devices.

Note: Some of the tools (such as KEIL, GCC, etc.) might need to get installed separately since they are not included by default.

SmartSnippets™ Studio is a framework of tools that comes with the popular open-source IDE Eclipse CDT and contains as well:

  • SmartSnippets™ Toolbox which covers all software development requirements, including:
    • Programming and loading of firmware into SRAM, OTP, and Flash
    • Power profiling
  • SmartSnippets™ documentation

The SmartSnippets™ IDE is enabled by an on-board J-Link debugger from SEGGER. This offers standard debug capabilities such as single stepping, setting breakpoints, software download, and many more. For more details on the debugger capabilities, visit https://www.segger.com.

All components, tools, and plugins are taken from the internet without changes and modifications. A subset of useful tools/plugins is selected by Renesas, and these are bundled with Eclipse CDT. Users can interact with all different tools from within the Studio environment. The availability of tools and features is directly dependent on the selected Device Family.

The SmartBond™ Flash Programmer is a Programming GUI that supports flash memory programming. 

The Connectivity Production Line Tool (PLT) is used mainly during production to reduce cost and has many benefits:

  • PLT is optimized to do the production testing and programming memory
  • High level of parallelization will reduce the testing and memory programming time
  • On Board XTAL trimming is supported

Release Information

Target Devices

Type Title Date
Software & Tools - Software MSI 775.37 MB
Software & Tools - Software ZIP 560.04 MB
Software & Tools - Software RUN 498.45 MB
Software & Tools - Software RUN 218.20 MB
Software & Tools - Software MSI 162.83 MB
5 items

Support Communities

  1. Problem in Da14580

    Dear Dialog I have a problem with a DA 14580. I took the IC for ON and Off a LED. I read your site and I found that I need to define two commands for the work. First, determining output for the pin and second high or low being the ...

    Feb 24, 2019
  2. Connect betwen DA14580 and STM32F4 via UART

    Hello, STM32F4 <-----UART-----> DA14580 <-----BLE(DSPS)----> Android I want to connect between DA14580 and STM32F4 via UART. Let DA14580 read data from STM32F4 Then, from STM32F4 can send data to the phone. How to transmit data from DA and STM32F4 by UART? Help me.

    Apr 24, 2019

Knowledge Base

  1. How to do 1-Wire UART Programming on the DA14531MOD?

    We are going to show how you can do 1-Wire UART Programming on the DA14531MOD with the Development Kit Pro.You will have to use the SmartSnippets Toolbox which can be downloaded from: SmartBond™ Development Tools | Renesas Hardware Configurations:Please refer on UM-B-141, on section 5 ...

    Jul 4, 2024