Overview
Description
Renesas offers a production test and programming unit that enables you to reduce the time to ramp up at a lower cost. The Connectivity Production Line Tool (PLT) is a flexible platform that helps to increase throughput in volume test and programming of units centered around Renesas Connectivity ICs.
The Connectivity PLT is designed to test, calibrate, and perform memory operations for multiple devices under test (DUTs) in parallel. Up to four PLT boards, each with eight test sites, can be daisy-chained to support 32 simultaneous test sites.
Features
- Up to 32 parallel programming and testing
- Flexibility in programming OTP/Flash/eFlash
- Ease of integration: CLI tool included
- Modular approach: Bluetooth® Low Energy (LE), Wi-Fi, DECT
- Included tests:
- Xtal trimming
- Sensor test
- GPIO test
- RSSI test
- Current measurement
- Many more
- Customizable test steps
Target Devices
Design & Development
Videos & Training
Discover how the Renesas Connectivity Production Line Tool (PLT) streamlines wireless device production. It enables automated testing, high-speed programming, and reliable RF validation to support efficient and high-quality manufacturing.
News & Blog Posts
Blog Post Aug 28, 2025 |
Support
Support Communities
- Production on RA6W1
Hi Renesas,When I get to the production stage for the RA6W1 will I have to use the Renesas Flash Programmer (Programming GUI) | Renesas ?Can I modify it to support the UART interface for programming?Do you have any adapters for production lines with this tool?Thank you
Dec 24, 2025 - DA14535MOD Codeless without a Dev Kit
I have previously used the DA14535MOD module with the DA1453x Devkit, running several examples as per your documentation.But now I have to use the DA14535MOD without the Devkit, connected to an RA6M3 microcontroller. Some questions: I understand that SmartBoot is loaded as a secondary bootloader automatically at power on ...
Nov 29, 2025 - Programming OTP through Debug Access Port
I am seeing times when the OTP programming is not successful, looks like it misses an entire FIFO. Details: Accessing memory via DAP (Debug Access Port). 1) CPU Halted 2) OTP Access * CLK_AMBA_REG = OTP_ENABLE * SPOTP_TEST_REG = LDO_OTP_WRITE 3) OTP Write * OTPC_MODE_REG = 0 ...
Sep 25, 2018