Skip to main content
View
View
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

RX IoT Cloud Over-the-Air (OTA) Solution

Depending on your system, you can select the optimal environment from on-premises environments using TCP/IP communication to integration with the Amazon Web Services (AWS) cloud environment. For the AWS cloud environment, we support easy and secure system development of IoT products via Ethernet or Wi-Fi using SSL/TLS, OTA, MQTT, TCP/IP, and Fleet Provisioning.

Getting Started Guide: iot-reference-rx (GitHub)

 

Image
RX IoT Cloud Over-the-Air (OTA) Solution

Hardware

CK-RX65N v2

Image
Chart
  • ROM/RAM: 2MB/640KB 144-pin, temperature, humidity sensor, indoor/outdoor air quality sensor, etc.
  • Connectivity: Wi-Fi*, Ethernet
    *Wi-Fi module included
  • Acquired AWS Partner Device certification
  • For more information and to purchase: CK-RX65N v2

Software

Step 1: Trial for CK-RX65N v2

Easily try visualizing sensor data on Renesas dashboard

Image
Visualizing sensor data on Renesas dashboard

Step 2: IoT Product Development

Demo projects with the following features essential for IoT devices are available. Please refer to the Getting Started Guide on GitHub for usage instructions.

Image
PubSub / MQTT, OTA, Fleet Provisioning: Assisted provisioning for mass production

Development Support

IDE & Tools

  • Various Free RTOS samples can be generated as new projects in the free IDE e² studio
  • Development support tool QE for OTA enables easy implementation of OTA firmware updates

Solutions

Security

Image
Steps to Start Development
Image
Get Evaluation Board

The latest evaluation kit, CK-RX65N, supports the following communication controls and examples.
For supported RTOS versions, please check GitHub ( AWS / Azure ).
Click Here to purchase CK-RX65N v2.

Please refer to the GitHub Wiki for the differences between CK-RX65N v1 and v2.

Board AppearanceBoard NameCommunication ControlDashboardMQTTOTAQE for OTA (*1)Fleet Provisioning (*2)
Image
CK-RX65N Overview
CK-RX65N v2Wi-FiAWSAWSAWSAWSAWS
Ethernet (*3)-AWSAWSAWSAWS

*1: A free development support tool that allows you to easily try OTA. The e² studio GUI supports various settings required for OTA and OTA execution.
*2: One of the provisioning methods provided by AWS. Automate the provisioning of multiple devices, which is a challenge during mass production.
*3: For the steps to perform Ethernet communication with CK-RX65N v2, please refer to the Getting Started Guide on GitHub.
*4: Use of cellular modules other than RYZ014A is described in the Porting Guide.

Image
Prepare IDE

Install the integrated development environment and compiler

 RENESASIAR Systems
*Supports Azure RTOS only
Integrated development environmente2 studio (free)IAR Embedded Workbench for Renesas RX (commercial version)
CompilerRenesas CC-RX complier (paid)
or
GNU GCC compiler (free) *
*This can be installed at the same time as e² studio
IAR RX compiler (commercial version)
Development Assistance ToolQE for OTA (free)
Easily test OTA (Over the Air) firmware updated using AWS
-
Image
Project Execution

Various sample projects(MQTT Pub/Sub, OTA, Fleet Provisioning) are supported by the Project Generation feature of e² studio.

RTOSHow to Get SamplesHow to Use SamplesHow to Use VideoOther Sample, etc.
AWS Free RTOSGithubRefer to Getting Started Guide.md included with sampleLinkFor more information on AWS-related solutions, click here.
Microsoft Azure RTOSAPNAPNLinkFor more information on Azure-related solutions, click here.

Recommended Microcontrollers

We have selected the best products for cloud connectivity from our extensive line of RX microcontrollers.
As a basis for this selection, Renesas has ported the RTOS and as a result, believes that the memory resources required are at least 96KB RAM and at least 512KB ROM (or at least 1.5MB for OTA feature implementation).
Taking into account the communications, security and OTA capabilities required for cloud connectivity, we have selected the following products:

 Part NumberCPUFrequencyROMRAMTrusted
Secure IP
BGO,
Dual Bank
FreeRTOS
Kernel OnlyFreeRTOS-Plus-TCPNote 
(TCP/IP Communication)
AWS LibrariesNote
(Connect to AWS IoT Core)
MCURX72M  /  RX72NRXv3240MHz4MB1MBcheckcheckcheckNo (Porting available)No
RX66NRXv3120MHz4MB1MBcheckcheckcheckNo (Porting available)No
RX671RXv3120MHz2MB384KBcheckcheckcheckNo (Porting available)No
RX65N  /  RX651RXv2120MHz2MB640KBcheckcheckcheckcheck
(RX65N Only) 
check
(RX65N Only) 

Note: For sample projects, refer to iot-reference-rx (GitHub).

The RX Family offers programs that port real-time OSs provided by major cloud vendors for the RX Family. The FreeRTOS and Azure RTOS compatible programs have been certified as AWS and Azure devices, respectively, and can be used with confidence.

 Amazon FreeRTOSMicrosoft Azure RTOSNote
Usage feeFree
(MIT Open Source License)
Free
(MIT Open Source License)
Cloud IT Vendor CertificationAWS Partner Device certification for various kitsAzure Certified Device certification for various kits
Sample programs
for OTA/FW Update
check
(AWS FreeRTOS OTA)
check
(Microsoft ADU)
RTOS-LTS support
for IT vendors
check
(FreeRTOS - LTS Libraries)
check
(Azure RTOS - LTS Components)
Development environmentfree IDE (e² studio) provided by Renesasfree IDE (e² studio) provided by Renesas
IAR Embedded Workbench for RX

Note: Microsoft has announced the open sourcing of Azure RTOS. Azure RTOS will now be provided by the Eclipse Foundation as Eclipse ThreadX. With this change, the Azure Certified Device program and our sample projects support have also been terminated. Please check the Microsoft website for details.

Image
aws logo

AWS Certified Programs

The following sample projects are available for the AWS Device Certified Kit CK-RX65N.
Please check GitHub for information on how to obtain and use sample projects.

  • PubSub/MQTT sample project
  • PubSub/MQTT with Fleet Provisioning sample project
  • PubSub/MQTT with Over-the-air(OTA) update sample project
  • PubSub/MQTT with Over-the-air(OTA) update sample project (TLS with TSIP *)
  • Minimal sample project (FreeRTOS-Plus-TCP library)

*: Trusted Secure IP

Extended Programs

FreeRTOS Extended Programs

We provide sample programs with extended functions useful for IoT device development based on the AWS certification program.

Programacquisitionboardcommunicationoperation overview
Sensor data uploadLinkRenesas CK-RX65NEthernet
Cellular
This explains the series of steps from activation of the SIM card included with the CK-RX65N to displaying the sensor data on the Dashboard. You can start developing IoT devices right away by using the SIM card included with the CK-RX65N and an AWS trial account.
LinkRenesas CK-RX65N v2Wi-FiThis is a sample project to connect to AWS via Wi-Fi to visualize sensor data values on a dashboard. 10USD worth of service is available free of charge by using the AWS trial account that comes with the CK-RX65N. This sample is recommended for beginners in AWS cloud development.
MbedTLS for Trusted Secure IPLinkRenesas CK-RX65NEthernet
Cellular
This application note describes how to manage keys safely and speed up the encryption/description processing in TLS communication by using the Trusted Secure IP (TSIP) module, which is security hardware built into RX Family MCUs. This application note also provides concrete implementation examples and sample code.
OTA firmware update of secondary devicesLinkRenesas CK-RX65N v2 Ethernet

This is sample code for an OTA firmware update (2nd OTA) for a secondary device. The OTA FW update is performed to the RX microcontroller for the secondary device using a gateway device (RX65N) that communicates with AWS. The OTA can be performed on devices that are not directly connected to the cloud, allowing for flexible service updates and response to vulnerabilities in secondary devices.
Introduction video: Secondary Device OTA Update using FreeRTOS and Amazon Web Services 

Image
FreeRTOS-secondary-device-OTA
Low power operationLinkRenesas CK-RX65NCellularThis is a sample program for low power consumption (intermittent operation) using the LTE Cat-M1 module (RYZ014A) and FreeRTOS. Many IoT devices are designed to be battery-powered, so it is necessary to devise ways to reduce power consumption. Low power consumption can be achieved by intermittent operation of communication control with this sample program.
Introduction video: RX MCU Low Power Consumption Operation with FreeRTOS by Amazon Web Service
Image
Azure-logo
 

Azure Certified Programs

Sample projects using Azure RTOS 6.4.0 and earlier versions are available*. Please refer to the Application Note for information on how to obtain and use the samples for Azure RTOS 6.4.0.
Note: Azure RTOS was open-sourced in April 2024 and is currently released as Eclipse ThreadX. With this change, the Azure Certified Device program and our sample projects support have also been terminated.

  • IoT Embedded SDK sample project
  • IoT Embedded SDK PnP sample project
  • Azure Device Update (ADU) sample project... etc.

Azure RTOS Extended Programs

We provide sample programs with extended functions useful for IoT device development based on the Azure Certified program.

ProgramAcquisitionBoardCommunicationOperation Overview
OTA firmware update of secondary devicesLinkRenesas CK-RX65NEthernet

This is sample code for an OTA firmware update (2nd OTA) for a secondary device. The OTA FW update is performed to the RX microcontroller for the secondary device using a gateway device (RX65N) that communicates with Azure. The OTA can be performed on devices that are not directly connected to the cloud, allowing for flexible service updates and response to vulnerabilities in secondary devices.
Introduction video: Leaf Device OTA Update using Microsoft Azure ADU

Image
Azure rtos expand secondary device OTA update
NetXDuo with TSIP for TLSLinkRenesas CK-RX65N This APN presents an example of adding the TSIP driver to Azure RTOS, which includes NetX Duo, and explains how to confirm its operation. No keying information is handled as plaintext during TLS protocol processing, thereby reducing the risk that customer keying information stored on the device may leak. In addition, hardware acceleration speeds up encryption processing.

Amazon Web Services is a trademark of Amazon.com, Inc. or its affiliates in the United States and/or other countries.
https://aws.amazon.com/jp/trademark-guidelines/

FreeRTOS™ is a trademark of Amazon Web Services, Inc.
http://www.openrtos.net/copyright.html

GitHub® is a trademark of GitHub, Inc.
https://github.com/logos

Azure is a registered trademark or trademark of Microsoft Corporation in the United States and/or other countries.
https://azure.microsoft.com

Type Title Date
Application Note PDF 1.64 MB 日本語
The Firmware Updating Communications Module provides communication control functionality between microcontrollers in a primary MCU-secondary MCU system configuration. By using this module, firmware updates for the secondary MCU can be easily performed via the primary MCU. The communication protocol supports UART or 3-wire SPI.
Application Note PDF 4.16 MB 日本語
This application note explains the overview of the provisioning methods that AWS provides, along with the implementation of fleet provisioning using FreeRTOS on the CK‑RX65N and the procedures for verifying its operation.
Application Note PDF 5.73 MB 日本語
This application note explains the procedures for using an OTA demo application on the RX65N under FreeRTOS with IoT Libraries.
Application Note PDF 12.71 MB 日本語
By using the FIT module, users can easily incorporate firmware update functionality and secure boot functionality into their applications. The firmware update module provides middleware that functions as a component when adding firmware update functionality to the user's system.
Flyer PDF 452 KB 日本語
Application Note PDF 6.16 MB 日本語
AI-generated Summary: This document explains how to implement FreeRTOS Over-The-Air (OTA) firmware updates on RX65N microcontrollers using Amazon Web Services (AWS). It covers the use of the dual bank memory function to enable seamless firmware updates without interrupting device operation. The guide details hardware and software setup, including the CK-RX65N board, cellular modules, and necessary software tools like e2 studio, FreeRTOS, Python, and OpenSSL. It also provides step-by-step instructions for AWS configuration, device registration, firmware creation, and update procedures. The document supports versions v202210.01-LTS-rx-1.1.3 and later, with notes on hardware module replacements due to product discontinuation.
Application Note PDF 1.15 MB 日本語
AI-generated Summary: The document explains how to extend and control cellular communication modules using firmware integration technology, focusing on adding new AT commands and managing modules beyond the RYZ014A cellular module. It details hardware and software requirements, including MCU functions and dependencies on specific firmware modules and FreeRTOS. The guide covers API functions for communication control, command processing, timeout, and lock handling, along with examples for adding various types of AT commands. It also provides reusable processing functions for other cellular modules and outlines necessary modifications in related software components.
Application Note PDF 6.73 MB 日本語
AI-generated Summary: The document explains DALI-2 lighting communication using the RX65N Cloud Kit as a Control Device/Application Controller. It covers the DALI protocol, including receiver and transmitter functions, frame types, and communication between bus units. It details hardware and software configurations, system operation modes, and development environment setup. The document also addresses error handling and provides references for further study. It supports multi-master and single-master application controllers with specific frame transmission requirements.
Flyer PDF 931 KB 日本語
Application Note PDF 1.01 MB
AI-generated Summary: e2 studio integrates a Partner OS Debugging Plug-in to enable RTOS-aware debugging for Renesas RX devices using FreeRTOS with IoT libraries. It allows developers to create FreeRTOS projects, view and manage RTOS resources such as tasks, queues, timers, and stacks during debugging sessions. The environment supports Renesas RX family devices with specific toolchains and debuggers, enhancing real-time OS resource visibility and control within the development workflow.
White Paper PDF 812 KB 日本語 , 简体中文
The Renesas RX65N Cloud Kit enables Wi-Fi connection to Amazon Web Services (AWS) using the RX65N MCU, providing an optimal evaluation environment for IoT developers integrating applications with the cloud. This paper offers a step-by-step guide to key considerations for connecting applications to AWS quickly and securely.
Application Note PDF 2.71 MB 日本語
AI-generated Summary: The document explains how to download and run Amazon FreeRTOS on the Renesas RX family using e2 studio. It guides users through preparing and configuring the demo project, selecting the demo, setting up AWS and hardware, configuring the debug serial port, and building and running the demo. It also details downloading the source code from Renesas GitHub, highlighting that e2 studio version 7.5 and above supports importing Amazon FreeRTOS projects directly within the IDE, simplifying the process.
12 items
Type Title Date
Sample Code
[Software=RX Driver Package|V1.48],[Toolchains=CC-RX|V3.07.00;GNURX|14.2.0.202505;IAR Compiler for RX|v.5.20.1]
Log in to Download ZIP 156.61 MB
Application: Consumer Electronics
Compiler: CC-RX, ICCRX Function: Driver or Library IDE: e2 studio, GCC EWRX, IAR EWRX
By using the FIT module, users can easily incorporate firmware update functionality and secure boot functionality into their applications. The firmware update module provides middleware that functions as a component when adding firmware update functionality to the user's system.
Sample Code
[Software=RX-Driver-Package|V122],[Toolchains=GNURX|V8.3.0.2019.4]
Log in to Download ZIP 442.25 MB 日本語
Application: Industrial
Compiler: GNURX Function: Application Example, Communication Interface, Driver or Library, Other peripherals IDE: e2 studio
Board Description File ZIP 1 KB
Upgrade - IDE
Log in to Download ZIP 570.25 MB 日本語
Upgrade - IDE
Log in to Download ZIP 1,616.95 MB 日本語
Upgrade - IDE
Log in to Download ZIP 1,264.29 MB 日本語
Upgrade - Compiler
Log in to Download ZIP 22.40 MB 日本語
7 items