Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Renesas offers a production test and programming unit that enables you to reduce the time to ramp up at a lower cost. The Connectivity Production Line Tool (PLT) is a flexible platform that helps to increase throughput in volume test and programming of units centered around Renesas Connectivity ICs.

The Connectivity PLT is designed to test, calibrate, and perform memory operations for multiple devices under test (DUTs) in parallel. Up to four PLT boards, each with eight test sites, can be daisy-chained to support 32 simultaneous test sites.

Features

  • Up to 32 parallel programming and testing
  • Flexibility in programming OTP/Flash/eFlash
  • Ease of integration: CLI tool included
  • Modular approach: Bluetooth® Low Energy (LE), Wi-Fi, DECT
  • Included tests:
    • Xtal trimming
    • Sensor test
    • GPIO test
    • RSSI test
    • Current measurement
    • Many more
  • Customizable test steps

Target Devices

Type Title Date
Software & Tools - Software
Log in to Download ZIP 42.02 MB
1 item
Type Title Date
Manual - Software PDF 9.11 MB
The Connectivity Production Line Tool Manual provides comprehensive guidance on the setup, configuration, and operation of the Renesas Connectivity Production Line Tool (PLT). These manuals detail both the hardware and software components of the PLT system, offering step-by-step instructions for installation, initialization, and troubleshooting. It covers Core and Database Services, communication error fixes, and demo mode for visual setup without execution. Designed for production use, it ensures reliable, efficient deployment of connectivity testing workflows.
Release Note PDF 585 KB
The Connectivity Production Line Tool (PLT) Release Note summarizes the release of the Connectivity PLT, detailing new features, known issues, and limitations introduced in the current version. It supports production testing and programming for Renesas devices and includes updates to hardware support, software functionality, and integration capabilities. The release notes also outline versioning rules and compliance information.
Quick Start Guide
The Connectivity Production Line Tool (PLT) User Guides provide technical documentation for deploying and operating Renesas' production test tools across Bluetooth Low Energy SoC platforms, such as the DA1453x. They detail the command-line interface (CLI) used on Windows for UART communication with devices running test firmware supporting Bluetooth SIG HCI commands and proprietary extensions. The guides also cover binary integration, setup, and hardware configuration to streamline testing and accelerate Bluetooth LE product delivery.
3 items

Related Boards & Kits

Models

Models

Type Title Date
Model - Other
Log in to Download ZIP 1.29 MB
1 item

News & Blog Posts

Support Communities

  1. Production on RA6W1

    Hi Renesas,When I get to the production stage for the RA6W1 will I have to use the Renesas Flash Programmer (Programming GUI) | Renesas ?Can I modify it to support the UART interface for programming?Do you have any adapters for production lines with this tool?Thank you

    Dec 24, 2025
  2. DA14535MOD Codeless without a Dev Kit

    I have previously used the DA14535MOD module with the DA1453x Devkit, running several examples as per your documentation.But now I have to use the DA14535MOD without the Devkit, connected to an RA6M3 microcontroller.  Some questions: I understand that SmartBoot is loaded as a secondary bootloader automatically at power on ...

    Nov 29, 2025
  3. Which is best method JTAG or UART

    Hi , I have used DA14583 chip set for custom application. which is best method to flash the device using jtag or Uart ? Is there any difference in programming ? For production programming also which is best method ? why dialog gives two options ? Is there any specific reason ..?

    Oct 4, 2018
View All Results from Support Communities (212)