Skip to main content
Renesas Electronics Corporation

Overview

This Connectivity Production Line Tool (PLT) with companion board provides the necessary components to get started with production testing of Renesas Bluetooth ® Low Energy (LE) devices such as the DA1453x family. The kit includes the PLT main board,  the PLT self tester "companion board", and a DA14695 USB development kit which is preconfigured as a RF Testing Unit (RFTU).

The combination of the Connectivity PLT software is designed to reduce ramp-up time and lower production costs. By validating your hardware before volume testing begins, the companion board helps increase throughput and maintain confidence throughout the testing process.

Features

  • Up to 32 parallel programming and testing
  • Flexibility in programming OTP/Flash/eFlash
  • Ease of integration: CLI tool included
  • Modular approach: Bluetooth® Low Energy (LE), Wi-Fi, DECT
  • Included tests:
    • Xtal trimming
    • Sensor test
    • GPIO test
    • RSSI test
    • Current measurement
    • Many more
  • Customizable test steps

Products in the Design

Sample & Buy

Connectivity Production Line Tool Starter Kit

RTKRQ00101S00000BJ

Active
1u | $1,500.00Budgetary Price

Add-on Hardware

Additional boards that work with this platform. Some may be required for full functionality or to evaluate specific features.

Connectivity Production Line Tool 8-Site Main Board

Enable high‑throughput production testing of connectivity devices using a scalable multi‑site production line platform.

Connectivity Production Line Tool Companion Board for Debugging

Validate and debug production test setups using a companion board designed to ensure reliable PLT operation.

Connectivity Production Line Tool Bluetooth Low Energy RF Test Unit

Accelerate volume production testing of Bluetooth Low Energy devices using a dedicated RF test unit for the PLT system.