Skip to main content
Renesas Electronics Corporation

Description

The CK-RA6M5 Cloud Kit enables users to securely connect to the cloud and explore the features of the Cortex®-M33 based RA6M5 group of MCUs and cloud services. With multiple network connectivity options, the kit provides a seamless cloud connectivity experience to most of the global cloud service providers. The kit is equipped with an on-board ethernet PHY for ethernet connectivity and includes the DA16600MOD  for wireless connectivity. With the Renesas Flexible Software Package (FSP), the kit has complete software stack support using FreeRTOS, Azure RTOS, and other middleware stacks, thereby making it an ideal platform for efficiently developing cloud solutions and greatly reducing the time-to-market.

Visit Renesas Cloud Solutions for a complete cloud solution package.

Features

  • CK-RA6M5 v2 baseboard
  • Wi-Fi with US159-DA16600EVZ Pmod
  • Ethernet
  • USB Full-Speed host and device
  • Sensors:
    • Humidity and temperature
    • Indoor air quality index
    • Outdoor air quality index
    • Heart rate, blood oxygen saturation (SpO2), respiration rate
    • Barometric pressure
    • 6 axis motion tracking
  • 2 MEMS microphones
  • Battery connector for portability
  • Arduino™ (Uno R3) connector
  • USB Type-C power connector
  • On-board MCU:
    • RF7A6M5BH3CFC microcontroller
    • 200MHz, Arm® Cortex®-M33 core
    • 2MB Code Flash, 512KB SRAM
    • 176 pins, LQFP package
  • Ecosystem:
    • MCU and Pmod current measurement points
    • 5V input through USB or external power supply
    • USB serial converter
    • Debug onboard (SEGGER J-Link)
    • 4 user LEDs
    • One user button
    • 2 Digilent Pmod (SPI/UART/I2C: Type-6A and Type-2A) connectors

Applications

Type Title Date
Quick Start Guide PDF 2.92 MB
Quick Start Guide PDF 2.70 MB
Provides the fundamental knowledge needed to port example projects from one RA kit to another. It then demonstrates these principles by explaining how to port three example projects of varying levels of complexity from the MCK-RA4T1 to the FPB-RA4T1.
Tool News - Release PDF 182 KB 日本語
Application Note PDF 402 KB
AI-generated Summary: The document explains the two operational modes, highlighting their advantages and disadvantages, and provides practical guidance for selecting and using each mode. It also includes reference links to Renesas RA Family Application Projects that demonstrate these modes with detailed examples of the related FSP module usage.
Tool News - Notification PDF 170 KB 日本語
Application Note PDF 2.35 MB
AI-generated Summary: This guide details the implementation of AWS IoT Core connectivity and OTA firmware updates on Renesas RA MCUs using the CK-RA6M5 v2 kit with Ethernet. It covers bootloader creation with MCUboot, MQTT/TLS setup, integration of AWS IoT Device SDK components, and secure authentication with X.509 certificates leveraging RA MCU hardware security. It also includes prerequisites, tools, and step-by-step instructions for building secure, cloud-connected applications with OTA updates.
Application Note PDF 8.33 MB
This guide details the objectives, architecture, and scope of OTA updates using AWS IoT OTA, and provides step-by-step instructions for preparing, executing, and validating firmware updates on the CK-RA6M5 v2 board. The project integrates three core components: a secure bootloader, a cloud connectivity application with downloader functionality, and AWS OTA cloud-side configurations for image storage and update initiation.
Application Note PDF 1.25 MB
Learn how to effectively use the FSP MQTT/TLS modules in end-product design. By following this guide, developers can add the “AWS Core MQTT,” “Mbed TLS,” and “AWS DA16xxx Wi-Fi sockets wrapper” using the Wi-Fi interface, configure them for the target application, and write code using the included example as a reference for a quick and efficient start.
Quick Start Guide PDF 4.27 MB
Learn to run the AWS cloud connectivity application project on CK-RA6M5 v2 via the Wi-Fi DA16600 interface, and develop MQTT/TLS applications using Wi-Fi DA16600 modules on the Renesas RA6 MCU Series.
Application Note PDF 3.78 MB
Learn how to run the AWS Cloud Connectivity Application Project on the CK-RA6M5 v2 using an Ethernet interface. This guide is intended for users developing applications with MQTT/TLS modules over Ethernet on the Renesas RA6 MCU Series.
Application Note PDF 1.20 MB
Learn how to effectively use the FSP MQTT/TLS modules for end-product design. By completing this guide, developers will add the “AWS Core MQTT,” “Mbed TLS,” and “AWS TCP Sockets Wrapper” using the Ethernet interface, configure them for the target application, and write code based on the included application example code as a reference, providing an efficient starting point.
Application Note PDF 2.55 MB
Users can follow the provided steps in this application note to recreate the bootloader and link the application projects to work with the bootloader by using the FSP Solution. This application note also includes procedures for mastering an application to work with the bootloader, and for downloading and updating a new application.
Tool News - Release PDF 284 KB 日本語
Application Note PDF 4.36 MB
Learn how to use the RA FSP modules in your own design with the FSP-integrated Azure IoT SDK. Upon completing this guide, you will be able to add the FSP modules to your own design, configure them correctly with the Azure IoT SDK for the target application, and write code using the included application example code as a reference and efficient starting point.
Quick Start Guide PDF 4.35 MB
Learn to run the AWS cloud connectivity application project on CK-RA6M5 v2 via the cellular interface and develop MQTT/TLS applications using cellular modules on the Renesas RA6 MCU Series.
Application Note
Log in to Download PDF 1.88 MB
Learn how to effectively use the FSP MQTT/TLS modules for end-product design. By completing this guide, developers will add the “AWS Core MQTT,” “Mbed TLS,” and “AWS Cellular Sockets Wrapper” using the cellular interface, configure them for the target application, and write code based on the included application example, providing an efficient starting point.
Tool News - Release PDF 170 KB 日本語
Application Note PDF 1.19 MB 日本語
AI-generated Summary: The document explains how to connect Renesas RA MCUs to AWS IoT Core using MQTT over TLS via cellular networks. It covers configuring AWS IoT Core, using MQTT/TLS modules, and integrating AWS Core MQTT, Mbed TLS, and cellular socket wrappers. The guide includes hardware and software requirements, cloud dashboard monitoring, device management, and security features like X.509 certificates and encryption. It targets developers building secure IoT applications with cellular connectivity on RA6M5 MCUs.
Application Note PDF 4.03 MB
AI-generated Summary: The document explains how to connect Renesas RA family MCUs to Microsoft Azure IoT services using MQTT over TLS with cellular connectivity. It covers the integration of RA Flexible Software Package (FSP) MQTT/TLS modules and Azure IoT SDK for Embedded C, enabling secure device provisioning, registration, and data exchange via Azure IoT Hub and Device Provisioning Service. The guide details hardware and software requirements, including development tools, cellular modules, and cloud setup. It provides step-by-step instructions for creating, building, and running a sample application on the CK-RA6M5v2 kit, focusing on secure communication and device management in IoT cloud environments.
Tool News - Notification PDF 158 KB 日本語
PCB Design Files ZIP 77.80 MB
Flyer PDF 412 KB
Application Note PDF 5.76 MB
AI-generated Summary: Instructions guide users to run an AWS cloud connectivity project on the CK-RA6M5 board using a Cellular interface. It covers importing, building, and loading the MQTT/TLS application with the Renesas e2 studio IDE and Flexible Software Package v5.0.0. Detailed steps include hardware setup, SIM activation, serial console connection, and AWS IoT configuration. The document emphasizes prerequisites like familiarity with MQTT/TLS, cellular modems, and Renesas development tools. It also explains programming methods, connection settings, and debugging tips to enable seamless cloud communication via LTE Cat-M1 cellular modules.
Flyer PDF 614 KB 日本語
Quick Start Guide PDF 2.90 MB
Manual - Development Tools PDF 4.59 MB
Quick Start Guide PDF 2.55 MB
Manual - Development Tools PDF 1.86 MB
Release Note PDF 189 KB
Application Note PDF 536 KB
AI-generated Summary: The AWS dashboard for Renesas CK-RA6M5 and CK-RX65N cloud kits enables visualization and management of sensor data via AWS IoT Core. Users register their cloud kits by creating an account, verifying email, and entering the device UUID. After accepting an AWS Single Sign-On invitation and downloading security certificates, users access the dashboard with initial credentials and then change their password. Each cloud kit receives $10 AWS credits valid for one year; accounts enter quarantine status upon credit expiration, requiring credit card activation. Additional resources and application projects are available for download on Renesas’ website.
PCB Design Files ZIP 60.57 MB
31 items

Software & Tools

Software & Tools

Software title
Software type
Company
RA Flexible Software Package (FSP)
FSP is an enhanced software package designed to provide easy-to-use, scalable, high-quality software for embedded system designs using Renesas RA Family of Arm Microcontrollers. Note: FSP with e² studio Installer (Platform Installer) will install the e² studio tool, FSP packs, GCC toolchain, and Segger J-Link drivers required to use this software. No additional installations are required.
Software Package Renesas
QuickConnect Platform
QuickConnect platform enables fast prototyping by providing compatible hardware and software building blocks.
Software and Hardware Development Tools Renesas
Reality AI Utilities
Round-trip workflow for AI development and performance validation allowing to collect data, optimize models, and deploy directly to Renesas hardware
Solution Toolkit Renesas
3 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 4.82 MB
Provides the fundamental knowledge needed to port example projects from one RA kit to another. It then demonstrates these principles by explaining how to port three example projects of varying levels of complexity from the MCK-RA4T1 to the FPB-RA4T1.
Sample Code
Log in to Download ZIP 10.38 MB
Sample Code
Log in to Download ZIP 5.77 MB
Use this application example to add and configure the “AWS Core MQTT,” “Mbed TLS,” and “AWS DA16xxx Wi-Fi sockets wrapper” using the Wi-Fi interface in the target application.
Sample Code
[Software=RA FSP|v5.0.0]
Log in to Download ZIP 4.96 MB Compiler: GNUARM-None IDE: e2 studio
Learn how to effectively use the FSP MQTT/TLS modules in end-product design. This sample code allows developers to add and configure the “AWS Core MQTT”, “Mbed TLS”, and “AWS TCP Sockets Wrapper” using the Ethernet interface for the target application.
Sample Code
Log in to Download ZIP 2.54 MB
Learn how to create an application project using the MCUboot Module in Protected Mode on the Renesas EK-RA6M4 board with FSP v6.1.0. The intended audience includes product developers, product manufacturers, product support, and end users who are involved in designing application systems involving the use of a secure bootloader.
Sample Code
[Software=FSP | v4.2.0],[Toolchain: GCC ARM Embedded Toolchain version 10.3.1.20210824]
Log in to Download ZIP 4.65 MB Compiler: GNUARM-None IDE: e2 studio
Learn how to use the RA FSP modules in your own design with the FSP-integrated Azure IoT SDK. This sample code demonstrates how to correctly add and configure the FSP modules for your target application using the Azure IoT SDK.
Sample Code
Log in to Download ZIP 5.95 MB
Use this application example to add and configure the “AWS Core MQTT,” “Mbed TLS,” and “AWS Cellular Sockets Wrapper” using the cellular interface in the target application.
Sample Code
Log in to Download ZIP 4.64 MB
Sample Code
[Software=RA FSP|v4.2.0]
Log in to Download ZIP 7.74 MB Compiler: GNUARM-None IDE: e2 studio
Sample Code
[Software=FSP | v4.2.0],[Toolchain: GCC ARM Embedded Toolchain version 10.3.1.20210824]
Log in to Download ZIP 12.71 MB Compiler: GNUARM-None IDE: e2 studio
Sample Code
Log in to Download ZIP 4.11 MB
11 items

Related Boards & Kits

Boards & Kits

Part NumberStatusStockBudgetary Price (USD)Remarks
RTK7CKA6M5S08002BEActiveIn Stock1u | $60CK-RA6M5 v2 (Wi-Fi, Ethernet)
RTK7CKA6M5S04001BEObsoleteIn StockCK-RA6M5 v1 (Cellular LTE CAT-M1, Ethernet)

Support Communities

  1. ck-ra6m5 v2 quick start example project issue

    ... /../../arm-none-eabi/bin/ld.exe: ./src/net_thread_entry.o: in function `net_thread_entry': C:\r20qs0059eg0100-ck-ra6m5-v2- exampleprojects\ck_ra6m5-v2\_quickstart\quickstart_ck_ra6m5_v2_ep\e2studio\Debug/../src/net_thread_entry.c:317: undefined ...

    Jul 3, 2024
  2. sci_uart is not working on CK-RA6M5

    Hi All, Board : CK-RA6M5FSP : 4.1.0 Example : ra-fsp-examples-master\example_projects\ck_ra6m5\sci_uart I'm running an example "sci_uart" on e2 studio. I changed two codes because of miss-matched FSP version. 1. configuration.xml 2. APP version APP_PRINT(BANNER_4 ...

    Dec 9, 2022
  3. CK_RA6M5 SCI-SPI

    Hi, everyone. I am working with kit CK-RA6M5 with ADS1299. I have used to configure via SPI "sci_spi_ek_ra6m5". Try to send ID commnad to ADS1299. It has used  "R_SCI_SPI_Write", "R_SCI_SPI_Read" or "R_SCI_SPI_WriteRead". When I were reading data ...

    Jun 19, 2023
View All Results from Support Communities (33)

Knowledge Base

  1. RX Family: CK-RA6M5/CK-RX65N is used. I can only read 00h data from the outdoor sensor (ZMOD4510) installed in the same kit. Is it malfunctioning?

    The ZMOD4510 (outdoor sensor) in the CK-RA6M5 and CK-RX65N requires a warm-up time. This time varies depending on the operating mode of the sensor.It is 60 minutes when operated in Gen1 mode and 42 hours in Gen2 mode.Also, since this warm-up time is required ...

    Jun 9, 2022
  2. RA Family: CK-RA6M5/CK-RX65N is used. I can only read 00h data from the outdoor sensor (ZMOD4510) installed in the same kit. Is it malfunctioning?

    The ZMOD4510 (outdoor sensor) in the CK-RA6M5 and CK-RX65N requires a warm-up time. This time varies depending on the operating mode of the sensor.It is 60 minutes when operated in Gen1 mode and 42 hours in Gen2 mode.Also, since this warm-up time is required ...

    Jun 9, 2022