Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Solution Suite Concept: Software-Based Refrigerator

Image
Omar Shrit
Omar Shrit
AI Core Tech, Solution Marketing
Published: December 8, 2025

Imagine a world without cold storage—medicines would spoil, food would perish, and supply chains would collapse. Refrigeration systems are vital to modern life, from pharmaceutical coolers to large-scale warehouses. These systems form the backbone of the cold chain, ensuring products meet strict storage requirements.

To achieve durability and sustainability in these operations, embracing AI is essential for maximum performance optimization. Renesas has been continuously innovating in this space, delivering a range of AI-driven solutions tailored for the refrigeration industry—helping businesses enhance efficiency, reliability, and energy savings.

Renesas Enablement for AI-powered Refrigeration Solutions

Renesas' solution concept introduces a suite of AI-driven applications designed to tackle everyday challenges in refrigeration systems. These proposals focus on enhancing operational efficiency and reliability in key areas such as predictive maintenance, energy optimization, and asset management, among others.

Image
Refrigerant Gas Leak Detection
Refrigerant Gas Leak Detection

Refrigerant gas is crucial for maintaining stable cold temperatures in cooling systems. Over time, however, leaks can develop due to wear and tear in pipes or refrigerant circuits. To address this challenge, Renesas AI leverages advanced AI algorithms to detect anomalies by analyzing changes in electrical current and compressor vibrations. This proactive approach enables timely maintenance, prevents costly breakdowns, and ensures optimal cooling efficiency.

Compressor Overheat Detection

Compressor overheating can result from issues such as low refrigerant levels or clogged filters, leading to potential system damage. Renesas AI HVAC solutions go beyond leak detection by continuously monitoring filter conditions and measuring intake airflow in real time. By analyzing this data, the system predicts risks before they escalate, ensuring the cooling system operates efficiently and reliably.

Cooling Capacity Monitoring

Renesas HVAC solutions integrate advanced AI features to predict fan imbalances that directly impact cooling efficiency. Using AI models trained with electrical current data, these anomalies can be detected, enabling seamless and sensorless monitoring. This proactive approach enhances system reliability and ensures optimal cooling performance.

Assets Monitoring: Availability and Expiry Tracking

AI-powered object detection and classification enable real-time monitoring of stock levels and refrigerated assets. The system can automatically suggest restocking needs and estimate lead times for each item. By reducing the need for manual inventory checks and minimizing the frequency of opening cooling units, it reduces energy consumption and improves operational efficiency.

Person Identification

AI-powered person identification enhances security and user experience in refrigeration systems. Authorized access can be ensured through two approaches:

  • Vision-based authentication using an object detection model combined with on-device learning for custom face recognition.
  • Voice-based authentication using a speaker identification model with a microphone sensor.

These methods can be combined for two-step authentication, which is especially critical in medical or industrial refrigeration environments. For home appliances, person identification enables context-aware interactions, such as personalized dietary recommendations or recipe suggestions, creating a smarter and more intuitive user experience.

Renesas HVAC solutions leverage advanced AI technologies to transform cooling system management. By integrating real-time monitoring, predictive maintenance, and intelligent object detection, these systems deliver optimal performance, energy efficiency, and operational reliability. From detecting refrigerant leaks and airflow issues to predicting fan imbalances and automating inventory management, the Renesas solution concept offers a comprehensive, end-to-end approach to cooling system optimization.

This seamless and sensorless monitoring capability not only extends system longevity but also drives significant energy savings. As demand for smarter, more efficient refrigeration systems grows, Renesas is leading the way, pioneering the next generation of intelligent cooling solutions.

Explore more about Renesas' AI-powered HVAC innovations: