Skip to main content
Renesas Electronics Corporation

Overview

Description

This product is a real-time operating system (real-time OS) that is an implementation of the μITRON4.0 specification. μITRON is the predominant real-time OS for embedded systems in Japan. Its low resource requirements, outstanding real-time performance, and broad range of service calls make it very suitable for embedded systems requiring true real-time and multi-tasking capabilities.

In addition, its high degree of compatibility with the CS+ IDE and the configurator which automatically generates startup files will help you greatly reduce development times and get your products to market more quickly.

Important:This product is a separate product from RI850V4 V2.00.xx.

 

Features

  • Conformance with the µITRON4.0 Specification
    The design conforms with the µITRON4.0 Specification, which prescribes a representative OS architecture for embedded control.
  • Excellent portability
    To support its execution in various environments, the RI850V4 is separated into the target-dependent section for hardware-dependent processing and the parts for use in the user’s own code. Sample files of source code are provided. This enhances portability to various execution environments and facilitates customization.
  • ROM-based implementation
    Since the system is a real-time and multi-tasking OS designed on the assumption of usage in embedded execution environments, it was designed to be compact and ready for ROM-based implementation. A system can be configured with only those service calls that are actually used in the user’s application being linked (rather than all service calls provided by the RI850V4), so a real-time/multi-tasking OS which is optimally compact in terms of the user's needs can be configured.
  • Realization of memory savings
    The ability to disable preemption provided by the RI850V4 can reduce a system's memory requirements.
  • Interlinking with the CS+ Integrated Development Environment from Renesas Electronics[Learn More]
    • Automatic settings for options required in building the OS
    • Displaying the states of OS control objects such as tasks, semaphores, etc. (Resource Information)
    • Generates service calls to start up tasks from debugger, set up event flags, etc.
    • Graphical display of the history of task operations and of issuing service calls (system performance analyzer)
  • Interlinking with Green Hills Software, MULTI IDE from LLC[Learn More]
  • Supported compiler: CC-RH, GHS
  • Learn More

Release Information

Details of upgrade (See Tool News)
Operating Environment
Agreement Details

OS

Latest Ver.: V1.01.00
Released: Oct 1, 2014

CS+ interface plug-ins (RTOS Common plug-in)

Latest Ver.: V3.00.00
Released: Oct 1, 2014

CS+ interface plug-ins (Plug-in for RI850V4 V1)

Latest Ver.: V3.00.00
Released: Oct 1, 2014

Target Devices

Documentation

Design & Development

Sample Code

Additional Details

Functions

The RI850V4 kernel consists of the following modules. Each module is provided by functions (service calls) .

  • Task management functions
    Provided by the RI850V4 include a function to reference task statuses such as priorities and detailed task information, in addition to a function to manipulate task statuses such as generation, activation and termination of tasks.
  • Task dependent synchronization functions
    Changes task status from other task, and synchronizes tasks.
  • Task exception handling functions
    The task exception handling functions of the RI850V4 include a function related to the task exception handling routine that is activated when a task exception handling request is issued (function for manipulating or referencing the task exception handling routine status).
  • Synchronization and communication functions
    The synchronization and communication functions of the RI850V4 consist of Semaphores, Eventflags, Data Queues, and Mailboxes that are provided as means for realizing exclusive control, queuing, and communication among tasks.
    • Semaphores: In the RI850V4, non-negative number counting semaphores are provided as a means (exclusive control function) for preventing contention for limited resources (hardware devices, library function, etc.) arising from the required conditions of simultaneously running tasks.
    • Eventflags: Provides 32-bit eventflags as a queuing function for tasks.
    • Data Queues: Provides the data queues that have the data queue area in which data read/write is enabled for transferring the prescribed size of data.
    • Mailboxes: Provides a mailbox, as a communication function between tasks, that hands over the execution result of a given processing program to another processing program.
  • Extended synchronization and Communication functions
    Provides Mutexes as the extended synchronization and communication function for implementing exclusive control between tasks.
    • Mutexes: Provides a mutex, as a function to prevent contentions on using the resources.
  • Fixed-Sized Memory Pools
    When a dynamic memory manipulation request is issued from a processing program in the RI850V4, the fixed-sized memory pool is provided as a usable memory area.
  • Variable-Sized Memory Pools
    When a dynamic memory manipulation request is issued from a processing program in the RI850V4, the variable-sized memory pool is provided as a usable memory area.
  • Time management functions
    Provides methods to implement time-related processing (Timer Operations: Delayed task wakeup, Timeout, Cyclic handlers) by using base clock timer interrupts that occur at constant intervals, as well as a function to manipulate and reference the system time.
  • System state management functions
    Provides functions for referencing the system status such as the context type and CPU lock status, as well as functions for manipulating the system status such as ready queue rotation, scheduler activation, or the like.
  • Interrupt management functions
    The RI850V4 provides as interrupt management functions related to the interrupt handlers activated when an interrupt (maskable interrupt, software interrupt, reset interrupt) is occurred.
  • Service call management functions
    Provides the function for manipulating the extended service call routine status, such as registering and calling of extended service call routines.
  • Scheduler
    The scheduling functions provided by the RI850V4 consist of functions manage/decide the order in which tasks are executed by monitoring the transition states of dynamically changing tasks, so that the CPU use right is given to the optimum task.

Specifications

Target deviceV850
Maximum number of tasks255
Number of priority levels32
Service call number132
Performance
(Time takes for a target task
to be executed after the wup_tas is issued.)
16 microseconds
(V850E/MA1, 25MHz. embedded memory)
Kernel code sizeFrom 6K bytes to 20K bytes
Kernel RAM usage per taskdata : 32 bytes
stack : 128 bytes

Components

Provided itemsExplanationNote
Kernel source programKernel source programProvided only with mass- production licenses which include source code.
Kernel libraryKernel library for system building
Standard header filesITRON specification common definition files
Kernel specification definition files
Other definition files
Header files are provided both in C languages
Command line configuratorOutputs all types of definition files from the cfg file that describes the structure parameters in text.
Sample programA simple program using ITRON.
CS+ interface plug-ins
- RTOS Common plug-in
- Plug-in for RI850V4
Function for easy kernel embedding
Function for referencing the OS state during debug
System performance analyzerA tool that displays a transition diagram of the OS operation history and analyzes performance, such as CPU usage rate.Interfaces with CS+ and MULTI
Task debuggerA tool for referencing the OS state during debugInterfaces with MULTI
ManualUser's manual 

Processing Flow

Image
 ri850v4-flow-e

Support

Knowledge Base

  1. Service calls for release sometimes return which are not contain in UM

    Breaking of a task stack or a task stack breaking the OS management table are the possible reasons. Check the behavior after increasing the sizes of task stacks. Unintended incrementation of a stack before or after the task concerned might also cause this, rather than the actual stack for the ...

    Jul 14, 2015
  2. What will happen if a service call dedicated is issued from a non-task?

    Some operating systems can issue calls in this way, while others cannot. The RI600V4 and RI600PX distinguish between service calls with “i” and service calls without “i”, however the RI78V4, RI850V4, RI850MP, RX850, RX850 Pro, and HI7700/4 do not. As an extended specification of uITRON, service calls without ...

    Jul 14, 2015
  3. Error occurred when defining an interrupt function in dly_tsk

    ... periods of cyclic handlers are not exact. For example, when the time tick is 1 ms, dly_tsk(3) means a delay of at least 3 ms plus less than a full time tick, not a delay of exactly 3 ms. Refer to the following graph and descriptions for details.

    Jun 12, 2015
View All Results from Knowledge Base (8)