Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

Renesas offers a production test and programming unit that enables you to reduce the time to ramp up at a lower cost. The SmartBond™ Production Line Tool (PLT) helps to increase throughput in volume test and programming of units centered around the Renesas Bluetooth® ICs.

Features

  • Ease of integration with DLL-based commands
  • Flexibility in programming OTP, Flash, and EEPROM
  • Low overall cost of tester equipment
  • High level of parallelization and short testing time
  • Up to 16 times parallel programming and testing

Release Information

 

DA1470x

DA1453x

DA1458x

DA1459x

DA1468x

DA1469x

PLT v4.3

 

 

 

 

PLT v4.6

 

 

 

 

PLT v5.x

 

 

 

 

 

PLT v6.x

 

 

 

 

 

Target Devices

Type Title Date
Software & Tools - Software
Log in to Download ZIP 65.72 MB
Software & Tools - Software
Log in to Download ZIP 75.92 MB
Software & Tools - Software ZIP 73.45 MB
Software & Tools - Software
Log in to Download ZIP 77.00 MB
Software & Tools - Software
Log in to Download ZIP 77.92 MB
5 items
Type Title Date
Manual - Development Tools
Log in to Download PDF 7.05 MB
Release Note
Log in to Download PDF 779 KB
Manual - Development Tools PDF 4.99 MB
Manual - Development Tools PDF 6.58 MB
Release Note PDF 883 KB
Release Note
Log in to Download PDF 658 KB
Manual - Development Tools PDF 10.15 MB
Presentation
Log in to Download PDF 2.51 MB
Manual - Development Tools PDF 237 KB
Release Note PDF 196 KB
10 items

Support Communities

  1. Current measurement with Production Line Tool using Rigol supply

    Hi, I am trying to do current measurements on my DA14585 by using a Rigol DP832 as power supply. I have followed the guide in the manual but I get this error when I try to do the test with these settings: https://imgur.com/a/ ...

    May 11, 2021
  2. Dialog Production Line Tool SPI Image

    ... tought we can program spi flash with multi command. But we couldn't find image headers bin file. How can we write img file to spi flash?Smartbond Production Line Tool version v4.4.2 SDK Version: 6.0.14.1114 SmartSnippets Toolbox Version : v5.0.16.3720 Best Regards...

    Nov 7, 2023
  3. PLT Production Tool Power supply

    The PLT documentation suggests that I may need to up to 4 separate power supplies to make this work.  In my case I am using the PLT to program DA14530 modules. I believe VPP is not required to program the OTP on the 14530 - can this be left disconnected? The ...

    Sep 2, 2021
View All Results from Support Communities (53)

Knowledge Base

  1. How to program and test DA1459x in a production environment?

    The SmartBond Production Line Tool (PLT) is Renesas cost-effective solution for testing and programming DA14xxx devices. Find out more about the PLT on the product page.

    Dec 9, 2024
  2. How is firmware programmed during DA14592/DA14594 production?

    Renesas has developed the SmartBond Production Line Tool to assist with production testing and programming of the DA1459x family devices. This is a low cost solution for high throughput programming of application boards, ideal for use on a production floor. Please refer to this web page for the details.

    Apr 11, 2025