Overview
Description
Renesas offers a production test and programming unit that enables you to reduce the time to ramp up at a lower cost. The SmartBond™ Production Line Tool (PLT) helps to increase throughput in volume test and programming of units centered around the Renesas Bluetooth® ICs.
Features
- Ease of integration with DLL-based commands
- Flexibility in programming OTP, Flash, and EEPROM
- Low overall cost of tester equipment
- High level of parallelization and short testing time
- Up to 16 times parallel programming and testing
Release Information
DA1470x | DA1453x | DA1458x | DA1459x | DA1468x | DA1469x | |
|---|---|---|---|---|---|---|
| PLT v4.3 |
|
|
|
| ||
| PLT v4.6 |
|
|
|
| ||
| PLT v5.x |
|
|
|
|
| |
| PLT v6.x |
|
|
|
|
|
Target Devices
Support
Support Communities
- Current measurement with Production Line Tool using Rigol supply
Hi, I am trying to do current measurements on my DA14585 by using a Rigol DP832 as power supply. I have followed the guide in the manual but I get this error when I try to do the test with these settings: https://imgur.com/a/ ...
May 11, 2021 - Dialog Production Line Tool SPI Image
... tought we can program spi flash with multi command. But we couldn't find image headers bin file. How can we write img file to spi flash?Smartbond Production Line Tool version v4.4.2 SDK Version: 6.0.14.1114 SmartSnippets Toolbox Version : v5.0.16.3720 Best Regards...
Nov 7, 2023 - Alternative to J-Link for DA14531 SWD Programming in Production Line
... GND We are now preparing the firmware flashing process for the production line, and we would like to avoid using the Segger J-Link in production, looking for a more cost-effective, scalable, and automatable solution. We would like to ask: What is the recommended tool or setup from Renesas ...
Jul 9, 2025
Knowledge Base
- How is firmware programmed during DA14592/DA14594 production?
Renesas has developed the SmartBond Production Line Tool to assist with production testing and programming of the DA1459x family devices. This is a low cost solution for high throughput programming of application boards, ideal for use on a production floor. Please refer to this web page for the details.
Apr 11, 2025 - How to program and test DA1459x in a production environment?
The SmartBond Production Line Tool (PLT) is Renesas cost-effective solution for testing and programming DA14xxx devices. Find out more about the PLT on the product page.
Dec 9, 2024