Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Empower the Future: Build Smaller Smart Sensors with CSP MCUs

Image
Graeme Clark
Graeme Clark
Principal Engineer, Product Marketing
Published: May 12, 2026

Shrinking Sensors, Growing Constraints

Smart, connected IoT sensors used in medical devices, wearables, and industrial systems are expected to deliver high performance, and low power consumption—all within an ever-shrinking form factor. Designers are no longer constrained only by the printed circuit board (PCB) area; package height, total system weight, and mechanical envelope are now equally critical. As sensor functionality expands, traditional microcontroller (MCU) packaging technologies can become a bottleneck. Even when the silicon itself is small, the package often dominates the footprint, making it difficult to meet compact size and thickness targets. Engineers need packaging solutions to reduce package dimensions without sacrificing electrical, thermal, or manufacturing reliability.

Why Traditional MCU Packages Fall Short?

Conventional MCU packages—such as the low-profile quad flat package (LQFP), quad flat no lead (QFN), and standard ball grid array (BGA)—are widely used because they are proven, robust, and easy to assemble. However, these packages introduce significant overhead in size and thickness compared to the actual die. In space-constrained sensor designs, this extra packaging material limits further miniaturization. When every square millimeter of PCB area matters, a different packaging approach is required, one that brings the package size much closer to the silicon itself.

Wafer Level Chip Scale Packaging (WLCSP) Solution

Chip scale packaging (CSP) addresses these challenges. Renesas uses a specific version of CSP called wafer level chip scale packaging (WLCSP), where the device is directly packaged at the wafer level, rather than after the die is singulated. This approach results in a final package that is typically less than 1.2× the die size, with an ultra-thin profile and minimal added material.

In a WLCSP device, the MCU die is connected to a redistribution layer (RDL), sometimes referred to as an interposer. The RDL reroutes the die's bond pads into a solder ball pattern suitable for surface‑mount assembly. Lead‑free solder balls are then formed, allowing the device to be assembled using standard BGA‑style processes. Refer to the following figure for the internal structure of a WLCSP.

Image
Diagram showing the simplified internal structure of the WLCSP package.
Figure 1. Simplified Internal Structure of the WLCSP Package

The die is typically thinned to reduce overall thickness, and protective passivation layers are applied to provide mechanical protection, ultraviolet light shielding, and compatibility with standard pick and place equipment.

How the WLCSP Solves Key Sensor Design Challenges

By minimizing package overhead, the WLCSP enables several important benefits for compact sensor and embedded designs.

  • Minimal footprint and ultra-thin profile, making it ideal for space and height-constrained applications
  • Lower package weight due to reduced packaging materials
  • High I/O density within a very small footprint
  • Improved electrical performance, with lower parasitic inductance and resistance from shorter interconnections
  • Lower thermal resistance, enabling efficient heat dissipation from the device through the solder balls into the PCB
  • Easier handling and testing compared to bare die, while retaining near-die-size dimensions
Table 1. Package Specification Comparison
PackageLQFPBGAWLCSP
SizeLargeMediumSmall
PitchMediumMedium - SmallSmall
Electrical CharacteristicsOKGoodExcellent
Thermal CharacteristicsOKGoodExcellent
CostLowHighMedium

Design and Manufacturing Considerations

While the WLCSP offers clear advantages, it also introduces new design considerations. The ultra-fine pitch, typically 0.5mm or less, requires tighter PCB layout rules than many traditional packages. Trace width, spacing, via structures, and PCB material selection must all be carefully planned. Assembly processes must also support fine pitch placement and inspection. With early planning and close collaboration with PCB and manufacturing partners, these challenges can be effectively managed, allowing designers to fully benefit from WLCSP technology.

WLCSP Package Available in the RA4L1 Low-Power MCU

One example of the WLCSP in practice is the RA4L1 low-power MCU, featuring the Arm® Cortex®-M33, and designed for energy-efficient embedded and sensor applications. The RA4L1 is available in a compact 72-ball WLCSP measuring just 3.64mm × 4.28mm with a thickness of 0.5mm, making it well-suited for highly space-constrained designs. The RA4L1 is equipped with an 80MHz CPU, 512KB dual-bank Flash memory, and a rich set of peripherals optimized for sensor systems, including on-chip SPI, I²C, and I3C interfaces, low-power analog functions, multiple low-power UARTs, and a USB Full-Speed interface. By combining low power consumption, high performance, and a near-die-size WLCSP footprint, the RA4L1 enables advanced sensing and connectivity features in applications where PCB area and package height are critical constraints.

Image
Image showing the WLCSP package.
Figure 2. RA4L1 WLCSP Package

When to Choose a WLCSP

WLCSP technology is your choice when sensor designs face aggressive size, weight, and height limitations. With the near die size packaging, excellent electrical and thermal performance, and compatibility with standard surface mount assembly, the WLCSP enables a new class of compact, highly integrated sensor systems. With MCUs such as the RA4L1 having WLCSP options, designers can build powerful and reliable solutions for wearables, hearables, optical modules, smart sensors, audio products, and digital imaging systems.

Learn more about the RA4L1 microcontroller and its available package options