1. Home
    2. Tecnologia Chave

Motor Control Overview

Renesas offers solutions for motor control in a broad range of fields, from factory automation to consumer electronics.

Renesas Motor Control Solutions

Due to rising concerns about global warming issues and demands to reduce power costs, power consumption reduction requirements (energy-saving requirements) for electronic equipment and devices are becoming more severe. It is said that power consumption by motors in home appliances makes up over half of the total power consumption of a common household. Thus, it can be said that reducing motor power consumption is the key to saving energy.

There are various methods of controlling a motor. Among them, the best control method for reducing power consumption is inverter control. Although inverter control demonstrates a tremendous ability to achieve energy savings, there are more than a few challenges associated with its implementation. The difficulty of carrying out the inverter control itself, the complicated hardware, and high cost are the typical challenges. Renesas has developed and provides solutions that help overcome such challenges.

Where Renesas Devices Are Used

PartsConsumerIndustrialAutomotive
Permanent Magnet Synchronous Motor (Brushless DC Motor)Electric Fan, Washing Machine, Electric Screwdriver, Air Conditioner, Refrigerator, Vacuum Cleaner, Sewing Machine, Copier, Power Assisted BicycleSequencer, Robot Arm, Actuator, Industrial EquipmentCar
Single-Phase Induction Motor (Universal Motor)Electric Fan, Washing Machine, Refrigerator, Vacuum Cleaner, Sewing Machine--
Stepper MotorAir Conditioner, CopierActuator-
Three-Phase Induction Motor-Industrial Equipment-
Brushed DC MotorElectric Screwdriver-Car

*There are exceptions in terms of the type of motors found in these products.

Contact