Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The PMBus™ Communication Interface (CI) provides the interface between the Evaluation Board and the user's computer for the ZSPM2000 Evaluation Kit and select ZSPM8xxx Evaluation Kits. It is included in the kits and can also be ordered separately.

Features

  • PMBus™ Communication Interface (CI)

Applications

Related Boards & Kits

Boards & Kits

Part NumberStatusStockBudgetary Price (USD)Sampleable
PMBUSCOMMINTERFACEActiveOut of Stock1u | $86.59Available