Overview
Description
RL78/G1D Bluetooth LE Wireless Solution
Bluetooth Low Energy (LE) is a low energy mode of Bluetooth wireless technology that has an effect on power consumption especially for battery-operated applications. The attractive point of Bluetooth Low Energy lies in that it can operate while being connected to applications for smartphones and tablets. Renesas RL78/G1D Bluetooth LE Solutions provide smart connections with the lowest level of power consumption in the industry and can be used in applications such as healthcare and fitness devices, home electric appliances and RFID tags that use beacons to connect them with smartphones at low power consumption without wires.

Bluetooth LE Solution & Resource Quick Start Guide
This guide summarizes the Bluetooth LE MCU RL78/G1D Solution and related resources for each product development phase. Please download and use it.
Download: RL78/G1D Bluetooth LE Solution & Resource Quick Start Guide (PDF | English, 日本語)
Devices
RL78 16-bit Bluetooth LE MCU: R5F11Axxxxx
Renesas' RL78/G1D low power 16-bit microcontrollers (MCUs) support Bluetooth Low Energy and enable reliable connections with current consumption levels among the lowest in the industry. The chip incorporates a balun element and a filter. It is only required to connect the chip to an antenna. Reduction in the number of external components leads to reduction in labor required for design and quality control. It also supports the long-term product supply program.

RL78/G1D Module: RY7011A0000DZ00
The RL78/G1D module contains the RL78/G1D 16-bit MCU, a 32MHz crystal resonator for the RF chip and an antenna, all in a compact 8.95mm x 13.35mm x 1.7mm module. The module inherits the functional pins of the RL78/G1D, so not only can it be used for modem configuration, but the strengths of the microcontroller can also be leverage for embedded configuration. This Bluetooth Low Energy module offers a good balance between size and the number of functional pins.

H/W & Kits
RL78/G1D Evaluation Board: RTK0EN0001D01001BZ
The RL78/G1D evaluation board can be used to evaluate and develop applications for Renesas' RL78/G1D Bluetooth Low Energy solution. The board consists of an RL78/G1D module which can be plugged on to the development board and connected to an IDE for development and debugging. The development board can also work with a PC GUI tool for application level evaluation.
This evaluation board is best suited for the following purposes.
- For evaluation of the Renesas' RL78/G1D microcontroller device
- For operation evaluation of Bluetooth Low Energy
- For use as a principle prototype
The Renesas RY7011 module can be evaluated with the following configuration.

RL78/G1D BLE Module Expansion Board: RTKYRLG1D0B00000BJ
The RL78/G1D BLE Module Expansion Board (RTKYRLG1D0B00000BJ) is an evaluation board with a Pmod™ interface that incorporates the RL78/G1D module (RY7011A0000DZ00).
Build IoT Devices Such as Sensors with the RL78/G1D Module and a Host MCU

It can connect to the RL78/G14 Fast Prototyping Board (RTK5RLG140C00000BJ) and can be used to evaluate Bluetooth LE functions. Additionally, customers can use the RL78/G1D evaluation board to develop new Bluetooth LE applications with a Bluetooth LE system employing the RL78/G1D 16-bit microcontroller (MCU). Use the expansion board together with sensor devices to easily evaluate and develop IoT applications.
*Each board can be purchased from distributors.
S/W & Tools
Bluetooth Low Energy Protocol Stack for RL78 Family
The Bluetooth Low Energy protocol stack is software required to operate the RL78/G1D IC. It supports modem configuration and embedded configuration. It can also adapt to custom profiles created by customers.
Renesas has prepared a dedicated "Beacon Stack" that reduces current consumption by 40% in beacon operation that constantly transmits radio waves. Renesas also provides sample programs as a reference for customers' program development.
Bluetooth Low Energy Protocol Stack Sample Program:
- Virtual UART (custom Profile) application
This is a sample program that realizes serial communication and wireless communication between embedded devices. It has a simple AT command execution function to control and set Bluetooth LE communication, thereby realizing virtual UART communication where characters are transmitted/received via Bluetooth LE communication.

- Embedded Configuration sample program
- Host sample for (RL78/G14, RX113) sample program
- Sensor application
Beacon Stack Sample Program:
A transmitter that transmits a small amount of data once every few milliseconds to several seconds within a radius of several tens of meters is called a beacon. This signal is used for watching terminals, indoor navigation, position detection, movement management of moving objects, coupon issuance, etc. Most beacon transmitters run on coin-type or small batteries. Since radio waves are always transmitted at regular intervals, it is required to consume as little power as possible.
The Bluetooth LE MCU RL78/G1D realizes low power consumption operation that is optimal for beacon terminals.
- Basic operation sample program
- Connecting and updating beacon data sample program
Multi-Hop Sample Program:
Multi-Hop uses a beacon stack for the advertising and scanning. Relay equipment executes both transmission and reception for Multi-Hop frame relay via the flooding method. It's possible to communicate data via more than one appliance. You can execute broadcasting a command (e.g. lighting control) and gathering data (e.g. sensor data) by using Multi-Hop. And, you can either select or not select security for prevention of eavesdropping and falsifying.

Renesas offers Bluetooth LE software solutions corresponding to a wide variety of application development. See the protocol stack product page for more information.
GUI Tool - Windows Application
Even if you are not familiar with Bluetooth Low Energy, you can easily conduct Bluetooth Low Energy communication using the GUI tool without writing a program. You can confirm the API execution procedure and the setting values for various parameters while actually conducting communication activities. Additionally, you can also develop a program smoothly while referring to the results (logs) of the operation check.
Download GUI Tool: Bluetooth® Low Energy Protocol Stack GUI Tool Rev.1.13 - Sample Code (ZIP | English, 日本語) (PDF + Windows application)
GATTBrowser - Generic Data Communication Application
The GATTBrowser is a generic data communication application for checking the operation of Bluetooth LE. You can experience data communication with Bluetooth LE by scanning Bluetooth LE devices operating in the vicinity and connecting to those devices. It can be used not only for checking the operation of sample applications provided by Renesas Electronics, but also for debugging development products that implement the RL78/G1D device and module.
The GATTBrowser supports various operating systems (iOS, Android, Windows).
The GATTBrowser for iOS and Android can be downloaded from the App Store and Google Play respectively.
Download GATTBrowser for iOS and Android :
- GATTBrowser for iOS Smartphone Application Instruction manual Rev.1.16 (PDF | English, 日本語)
- GATTBrowser for Android Smartphone Application Instruction manual Rev.1.02 (PDF | English, 日本語)
- GATTBrowser (for iOS) (App Store)
- GATTBrowser (for Android) (Google Play)
Download GATTBrowser for Windows :
Windows 10 Bluetooth LE Application - Windows Application Example
The Windows 10 Bluetooth LE application can communicate with "Virtual UART application" running on the RL78/G1D evaluation board. This is an application example for Windows 10 that sends and receives character data to and from the terminal software on a PC connected to the evaluation board via USB.
In addition, a set of projects that can be launched and used in Visual Studio 2017 are provided, so you can use this application example as a base for developing Bluetooth LE communication apps that run on Windows in a Proof of Concept (PoC) phase.
Download Windows 10 Bluetooth LE Application: Bluetooth LE microcomputer / module Windows 10 Bluetooth LE Application Rev.1.00 - Sample Code (ZIP) (PDF + set of projects for Visual Studio 2017)
QE for BLE - Development Assistance Tool
The QE for BLE (for RL78 Family) is a dedicated tool for developing embedded software in systems which support the Bluetooth Low Energy protocol stack. This solution toolkit runs in the e² studio integrated development environment (IDE). The combination of the e² studio and QE for BLE makes it easy to test the communications features of Renesas' RL78/G1D Bluetooth LE MCU, thus reducing development periods for products being placed on the market. It can also design and generate the custom profile.
Please refer to the QE for BLE: Development Assistance Tool for Bluetooth Low Energy page for more information.
QE for BLE: Development Assistance Tool for Bluetooth Low Energy Page
Applied Solutions
RL78 Quick Solutions
The RL78 Quick Solutions demonstrate how RL78 low power MCUs combined with Renesas' analog and power products can create high-performance solutions for a wide variety of applications. Quick Solutions for the Industrial IoT, infrastructure, healthcare, and home and office are fully developed reference designs with a user’s manual, application details, schematic, bill-of-materials (BOM), and source code/project files that enable you to develop these solutions quickly.
| Solution Title | Overview |
|---|---|
| Healthcare | |
| Smart Medicine Box with BLE | Build a solution for managing personal medication with the Smart Medicine Box with Bluetooth LE reference design featuring the RL78/G13 and RL78/G1D MCUs. |
| Smart Blood Pressure Monitor | Build a solution for tracking blood pressure and other vitals with the Smart Blood Pressure Monitor reference design featuring the RL78/L1A and RL78/G1D MCUs. |
| Smart Body Fat Scale | Build a solution for body composition management with the Smart Body Fat Scale reference design featuring the RL78/L1A and RL78/G1D MCUs. |
| Industrial IoT | |
| Smart Moisture Sensor | Build a solution for monitoring soil moisture with the Smart Moisture Sensor reference design featuring the RL78/G11 and RL78/G1D MCUs. |
| Home & Office | |
| PowerPoint Presenter | Build a solution for presentation control with the PowerPoint Presenter reference design featuring the RL78/G1D MCU. |
| Smart LED | Build a solution for LED lighting control with the Smart LED reference design featuring the RL78/G1D MCU. |
| Smart Lock | Build a solution for home security with the Smart Lock reference design featuring the RL78/G1D MCU. |
Bluetooth Low Energy Utilization Proposals
Renesas proposes the utilization of Bluetooth LE wireless communication in various scenes.
- Wireless Update of Parameters (PDF | English, 日本語)
- Beacons Used for Monitoring and Other Applications (PDF | English, 日本語)
- Sensor Devices Keep Life Comfortable (PDF | English, 日本語)
- Multi-hop Communication of Sensor Data (PDF | English, 日本語)
FAQ
Please refer to the Knowledge Base for FAQs on Bluetooth specifications, MCUs, modules, protocol stacks, development environments, qualification, and more.
Comparison
Applications
Software
Software & Tool Pages
| Software title | Software type | Company |
|---|---|---|
| Bluetooth® Low Energy Protocol Stack for RL78 Family Bluetooth v4.2 certified protocol stack (Target device: RL78/G1D) | Protocol Stack | Renesas |
| QE for BLE: Development Assistance Tool for Bluetooth® Low Energy Debugging support tool that specializes in Bluetooth® Low Energy system development [Plugin for Renesas IDE "e² studio"] [Support MCU/MPU: RA, RX, RL78] | Solution Toolkit | Renesas |
| e² studio Eclipse-based Renesas integrated development environment (IDE).
[Support MCU/MPU: RA, RE, RX, RL78, RH850, Renesas Synergy, RZ] | IDE and Coding Tool | Renesas |
| Renesas Flash Programmer (Programming GUI) Flash memory programming software [Support MCU/MPU and devices: RA, RE, RX, RL78, RH850, RISC-V MCU, Renesas Synergy, DA1453x, DA1459x, DA1469x, DA1470x, DA148xx, Power Management, Renesas USB Power Delivery Family, ICs for Motor Driver/Actuator Driver, V850, 78K0R, 78K0] | Programmer (Unit/SW) | Renesas |
4 items | ||
Resources
Videos & Training
Wireless communication IC for Bluetooth Low energy and Sub-GHz by using RL78 and pre-amplifier