Skip to main content
Renesas Electronics Corporation

Overview

Description

Renesas Flash Programmer V3

Topics

  • The Renesas Flash Programmer supports the new device RX14T.

Renesas Flash Programmer V3 provides usable and functional support for programming the on-chip flash memory of Renesas microcontrollers in each phase of development and mass production.

Features

  • A simple GUI makes operations easy, even for first-time developers
  • PC-controlled programming via the E2 emulator, E2 emulator Lite, E20 emulator, Segger J-Link debug probes, a serial or USB connection
  • Interoperation with other software.
    • The efficiency of work can be improved by, for example, writing data to many boards consecutively and retaining logs of the written data in files.
  • Auto-programming from the command line
    • In the mass-production phase, a programming instruction can be easily run repeatedly from the command line (rather than using the GUI) for efficient mass production.
  • Programming a unique code to a designated area of flash memory
  • Enhanced security against theft through the encryption of program files [Learn More]
  • Easier creation of projects (compared with V2) [Learn More]
    • Easy selection of type names. No need to select detailed type names for products of the RL78 family.
    • Easy setting of mode pins for RX family products.
  • Improvements in processing speed (compared with V2)
    • The programming time has been shortened by approximately 10 percent.
    • In the case of the RL78 family, programming times have been shortened by up to 50 percent.(These data were gathered under specific conditions, and we do not guarantee a specific increase in speed.)
  • Learn More

Release Information

Number of licensesOrderable part nameRelease dateDownload
1RTCZZZZZZFD0AWNJLatest Ver. : V3.23.00 
Released : Apr 20, 2026 
Details of upgrade (Tool News)
evaluation software
5RTCZZZZZZFD0AWNJ#L5

Note:

  1. Each license is for use of the software on a single PC.
  2. From V3.08.02, the free-of-charge edition and upgrade program of the Renesas Flash Programmer are consolidated in a single file for downloading that serves as the form of delivery for the evaluation software. You can download the evaluation software from this link whether you are trying out the Renesas Flash Programmer for the first time or are already using an older version of the Renesas Flash Programmer.
  3. V3.09.00 and later versions of the Renesas Flash Programmer are no longer provided on a CD-ROM as the medium. The type names for ordering have been changed to reflect this change in the product configuration.
  4. The function to activate/deactivate license has been removed from V3.09.00 and later versions of the Renesas Flash Programmer. In addition, the users are eligible to receive the technical support by showing the PID in the product license certificate.
     

Software Licenses and Technical Support

The Renesas Flash Programmer is available for download as free evaluation software. 
We do not provide technical support for the free version, so will not be able to answer any questions you may have regarding the evaluation software and send to our technical support center via the Renesas web site. 
If you require technical support, we recommend that you purchase a software license through one of our sales offices or distributors.

 Before purchasing a licenseAfter purchasing a license
Technical SupportNot availableAvailable
Function and PerformanceNo difference (Renesas Flash Programmer can be used not only for evaluation, but also for programming finished products through the product development.)

FAQ

Title
MCU Flash Erasure at Connection with Flash Programming Tool (PG-FP5/PG-FP6/RFP/FDT)
Several MCUs "Read (R)" command is grayed and cannot be selected.
Writing to an MCU with a different ROM/RAM size (RFP/PG-FP5/PG-FP6)

See all related FAQs

See also Error Guide.

See Error Guide

Target Devices

Target Family

Note:

  1. The V3 does not support the V850 family, 78K0, and 78K0R. Use Renesas Flash Programmer V2 if you are using products of these families.
  2. For details of support for individual device part numbers, see List of MCUs supported by Renesas Flash Programmer V3 (PDF | English, 日本語).

Downloads

Documentation

Design & Development

Sample Code

Explore

Videos & Training

Additional Details

Functions

  • Supported file formats for programming: Intel HEX for HEX and HCUHEX files, Motorola S for HEX and HCUHEX files, binary, and RPI for RPI file
  • Check sum of program files
  • Execute commands such as erase, writing, verification, read-out, setup and acquisition of flash options, and acquisition of checksum
  • Sequential execution of multiple commands (for erasure, programming, verification, etc.)
  • Multiple files for programming selectable simultaneously

 

 

Enhanced security against theft through the encryption of program files

The new function for encrypting program files enhances security against theft.   
You can run this function by using the encryption utility program (RPE.exe) from the command line. The file is among those installed by the Renesas Flash Programmer installer.

Image
rfp_key-en

 

 

Easier Creation of Projects

Easy selection of type names

No need to select detailed type names for products of the RL78 family.

Image
easyselection

Easy setting of mode pins for RX family products

No need for mode pin setting, when the recommended connection examples are used.

Image
easysetting

 

System Configuration

The system configuration in programming with Renesas Flash Programmer V3 is as follows.

Image
rfp_config202206-en

Note:

  1. The E1 emulator is also usable.
  2. Renesas Flash Programmer can use certain models of Segger J-Link to provide a serial communication with the boot mode functionality of RA Family MCUs. Please refer to the Renesas Flash Programmer Information for Users for applicable hardware, recommended firmware, appropriate debug connection to the target MCUs.

 

Target Devices by Connection Methods

For details, refer to the List of MCUs supported by Renesas Flash Programmer V3 (PDF | English, 日本語).

 Connections
Supported devicesThrough on-chip debugging emulators Note1Serial   
(RS-232C)
USB
E2 emulatorE2 emulator LiteE20 emulatorSegger   
J-Link debug probes
RAlenslenslenslenslens   
MCUs with USB boot
RL78lenslenslensNote2lens
RXlenslenslenslenslens   
MCUs with USB boot
RH850lenslensNote2lensNote2
RISC-V MCU(R9A02G020, R9A06G150)lens
RISC-V MCU(R9A02G021)lenslenslenslens
Renesas Synergylenslens   
MCUs with USB boot
DA1453x, DA1459x, DA1469x, DA1470x, DA148xxlens
RElenslenslens   
MCUs with USB boot
Battery Fuel Gauge ICslenslenslenslens
Renesas USB Power Deliverylenslenslenslens
ICs for Motor Driver/Actuator Driverlenslenslenslens

lens Available | — Not Available

Note:

  1. When using with the on-chip debugging emulators, conversion adapter is required depending on the number of pins on the target board.
  2. Some devices of this product family are not supported. For details, refer to the List of MCUs supported by Renesas Flash Programmer V3 (PDF | English, 日本語).

 

Information on the discontinuation of E1 emulator production and on its successor products

We have already discontinued production of the E1 emulator due to components of the product having reached their EOL (end of life, i.e. end of production). Please click on the following link to confirm the details and our successor products.

[Notification] End of Life (EOL) Notice for E1 Emulator (PDF | English, 日本語)

Support

Support Communities

  1. PE-MHI and Renesas Flash Tools GUI

    I'have ordered a PE-MHI and want to use Renesas Flash Tools GUI to download example. Normaly the GUI should connect using the uart (or throught the jliink provided). when creating a new projet from the Flash Tools GUI, I only see a uart over Bluetooth. According to the ...

    Jan 15, 2018
  2. Enabling Renesas Flash Programmer for J Link

    Hi team, We are trying to flash the Renesas RA6M1 controller using J-Link with Renesas Flasher tool... But could not succeed in doing it.... Please find the error details mentioned below : Connecting the toolError(E30002FE): This tool is not supported.Operation failed. Kindly help us on how it solve ...

    Feb 21, 2023
  3. The Renesas Flash Programmer: Setting up the hardware and software

    ... Renesas Flash Programmer V3.03.00 Home Page: https://www.renesas.com/en-us/products/software-tools/tools/programmer/renesas-flash-programmer-programming-gui.htmlRenesas Flash Programmer V3.03.00 User’s Manual: https://www.renesas.com/en ...

    Nov 11, 2017
View All Results from Support Communities (335)

Knowledge Base

  1. Renesas Programming Solutions for RA Family Devices

    ... circuit-programmer/ , Renesas provides programming solutions as well. The Renesas Flash Programmer (RFP) and PG-FP6 are two popular solutions for RA Family MCUs.RFP is a GUI-based tool for PC hosted Flash MCU programming during development and for small production runs. It requires the Renesas E2 Emulator ...

    Jun 22, 2021
  2. RL78/L23: Boot cluster resizing, bank swap settings

    It can be configured using the dedicated flash memory programmer PG-FP6 or Renesas Flash Programmer (Programming GUI).The bank swap settings can also be set in the properties of the e2 studio and CS+ debugger, but the boot cluster size must be done in a dedicated flash memory programmer.

    Aug 27, 2025
  3. CS+ Update Manager is Terminated While Updating is in Progress

    ... RLhttps://www.renesas.com/rl78-c-download CC-RHhttps://www.renesas.com/rh850-c-downloadSmart Configuratorhttps://www.renesas.com/software-tool/smart-configuratorRenesas Flash Programmerhttps://www.renesas.com/software-tool/renesas-flash-programmer-programming-gui# ...

    Mar 9, 2023
View All Results from Knowledge Base (23)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?