On any street in China, it is common to see electronic bikes (e-bikes) being used as a mode of transportation. Over the past 10 years, manufacturers have steadily produced more than 20 million e-bikes per year. Because of the high demand, there is a need for complete solutions with high reliability and innovative features, such as new battery management solutions for features like control or electronic locks.

This design uses a combination of an advanced MCU, power and battery management system (BMS) devices to provide a complete solution for any kind of e-bike.

System Benefits

  • Mature solution support with motor control algorithm, supports both square and sinewave drivers
  • High accuracy battery charge monitor that improves distance
System Block Diagram

E-bike System Solution

Winning Combinations

Renesas and IDT’s complementary product portfolios work together to deliver comprehensive solutions to our customers. This is just the beginning, with the combination of the Renesas and IDT development teams, there will more integrated solutions that provide significant advantages over traditional solutions.

See the benefits immediately with our “Winning Combinations” solutions