Skip to main content
Renesas Electronics Corporation

SLG47105 HVPAK Portable Washing Machine Demonstration

SLG47105 HVPAK Portable Washing Machine Demonstration
Mar 28, 2023

About This Video

The video demonstrates a working Portable Washing Machine. The device is created using the SLG47105 HVPAK as a control module to drive a 12V DC/DC Motor. In addition, the device has three timer modes, a constant number of revolutions per minute regardless of the load, and undervoltage protection with indication. For full description and design files, see the application note.