Dec 20, 2025
About This Video
Learn how to use the low voltage detector (LVD) on the RA0E1 fast prototyping board (FPB). The LVD module monitors the voltage input to the VCC pin, with detection levels selectable through register settings at various thresholds. The r_lvd module in FSP provides full support for configuring and using the Low Voltage Detector.