Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Overview

Description

The EK-RA6M5 evaluation kit enables users to effortlessly evaluate the features of the RA6M5 MCU Group and develop embedded systems applications using the Flexible Software Package (FSP) and e2 studio IDE. Utilize rich on-board features along with your choice of popular ecosystem add-ons to bring your big ideas to life.

Getting Started

Running the Quick Start Example Project

  1. The EK-RA6M5 comes pre-programmed with a quick start example project (source code provided in the EK-RA6M5 Example Project Bundle).
  2. Power up the EK-RA6M5 board through the debug USB port (J10) using the micro USB device cable connected to a 5V power source. The white power LED will light up.
  3. The quick start example project will begin to execute blinking the blue user LED.
  4. Refer to the EK-RA6M5 Quick Start Guide to explore additional functionality of the quick start example project.

Developing Embedded Applications

  1. Modifying the quick start example project – refer to the EK-RA6M5 Quick Start Guide for instructions on importing, modifying, and building the quick start example project
  2. Start with one of the many other example projects – choose from many example projects provided in the EK-RA6M5 Example Project Bundle to learn about different peripherals of the RA6M5 MCU Group. These example projects can serve as excellent starting points for you to develop your custom applications.

Building a Custom Hardware

  1. Start by building a functional prototype – utilize the EK-RA6M5 board with your choice of hundreds of popular ecosystem add-ons.
  2. Build custom hardware – develop custom hardware by referring to the design and manufacturing information provided in the EK-RA6M5 Design Package.

Features

  • Ecosystem & System Control Access
    • USB full speed host and device
    • Multiple 5V input sources
      • USB (debug, high speed, full speed)
      • External power supply
    • SEGGER J-LinkTM on-board programmer and debugger
    • Debug modes
    • User LEDs and buttons
      • Three user LEDs (red, blue, green)
      • Power LED (white) indicating availability of regulated power
      • Debug LED (yellow) indicating the debug connection
      • Two user buttons
      • One reset button
    • Five most popular ecosystem expansions
    • MCU boot configuration jumper
  • Special Feature Access
    • Ethernet (RMII and PHY)
    • 64MB External Octo-SPI Flash
    • 32MB External Quad-SPI Flash
    • CAN FD
    • USB High Speed host and device
  • MCU Native Pin Access
    • R7FA6M5BH3CFC MCU
    • 200MHz, Arm Cortex®-M33 core
    • 2MB Code Flash, 512kB SRAM
    • 176 pins, LQFP package, 24mm x 24mm x 1.70mm, 0.5mm pitch
    • Native pin access through 4x 40-pin male headers
    • MCU and USB current measurement points

Applications

Documentation

Design & Development

Software & Tools

Sample Code

Related Boards & Kits

Product Options

Part NumberStatusStockBudgetary Price (USD)Sampleable
RTK7EKA6M5S00001BEActiveIn Stock1u | $54.38Available

Videos & Training

Certifications

The EK-RA6M5 meets the following certifications/standards. Refer to the EK-RA6M5 user manual for the disclaimer, precautions, and more details on the certifications.

EMC/EMI Standards

  • FCC Notice (Class A) – Part 15
  • Innovation, Science and Economic Development Canada ICES-003 Compliance:  CAN ICES-3 (A)/NMB-3(A)
  • CE Class A (EMC Directive 2004/108/EEC)
  • Taiwan Chinese National Standard 13438, C6357 compliance, Class A limits
  • Australia/New Zealand AS/NZS CISPR 32:2015, Class A

Material Selection, Waste, Recycling, and Disposal Standards 

  • EU RoHS
  • China SJ/T 113642014, 10-year environmental protection use period.

Safety Standards

  • UL 94V-0

Partners

Zephyr Logo
Zephyr Project

The Zephyr Project is an open-source, scalable real‑time operating system (RTOS) designed for resource-constrained embedded systems and supports a wide range of hardware architectures and development boards. For the Renesas RA6M5 Evaluation Kit, Zephyr provides focused documentation covering board features, supported peripherals, and basic build, flashing, and debugging workflows to help developers quickly get started.

See the Zephyr Project RA6M5 Evaluation Kit Documentation

Support

Support Communities

  1. Pantronics PTX100 compatibility issue with EK-RA6M5

    Hello  I want to integrate Renesas PTX100R  with RA6M5 kit.Currently, I am getting error in "ptxPOS_Init_NSC" function. I am getting error "Initialization of the NSC: FAILED "I have attached screenshot for it.   kindly guide meRegardsSami This thread was automatically locked due to age.

    Sep 7, 2022
  2. EK-RA6M5 SPI Communication Error

    Hello all, I just tried to communicate with external flash (MX25L25645G [not on the board we connected externally]) using SPI and I used the sample code in FSP document. Only thing that I did is actually just using WriteRead method. However, when I tried to read the related part, I ...

    Oct 2, 2023
  3. Need help reviewing EK-RA6M5 e2 studio project files and FSP setup

    Hi everyone, I am at the point where I think I need someone to look directly at my project files, because I honestly don't know what to do. I am using an EK-RA6M5 and trying to move a working Arduino sensor prototype into e2 studio. My long term ...

    Mar 24, 2026
View All Results from Support Communities (186)

Knowledge Base

  1. RA Family: How to use the Debug Out function of J-Link OB on EK (Evaluation Kit)

    ... as EK-RA2E1, EK-RA2E2, EK-RA2L1, EK-RA2A1, etcEK-RA4M1、EK-RA4M2、EK-RA4M3、EK-RA4W1、EK-RA6M1、EK-RA6M2, EK-RA6M3, EK-RA6M4, EK-RA6M5, etc., all EKs come with J-Link OB (On-Board Debugger), which means that the user can evaluate, debug, and test the MCU ...

    Dec 14, 2023
  2. How to Use Event Link Controller to Link Peripherals on RA6M5 Evaluation Kit

    Last updated on 2nd June 2026   Summary of the video   This video demonstrates how to use the Event Link Controller (ELC) to link the General PWM Timer (GPT) with the Analog-to-Digital Converter (ADC) on the EK-RA6M5 board. Flexible Software Package (FSP) supports event linking with the r ...

  3. RA6M4, RA6M5: CPU Performance Difference when C-/S-caches are on/off

    ... if C-cache is hit. For the C-Cache is missed while C-Cache operation is enabled, or C-cache is disabled, the read access is three cycles. Reference Attachments: Example project on EK-RA6M4 for above benchmark testing (below) Example project on EK-RA6M5 for above benchmark testing (below)

    Dec 18, 2023
View All Results from Knowledge Base (9)