Skip to main content
Renesas Electronics Corporation

Renesas Blog

Read and Execute: Prevent System Bottlenecks with Read While Write (RWW)

Whether performing high-speed data transfer or executing code directly out of memory, a key system design requirement for edge devices is the selection of the right non-volatile memory.

Silicon Wafer Under Microscope

ADCs for Broadband Communication ASICs

Time interleaved ADCs and SAR-assisted pipeline ADCs provide the data rates needed to service the higher sample rate data converter requirements for delivering wireless or wired broadband.

How Renesas' Low Energy Solutions Can Help Curb the Spread of COVID-19 Blog

How Renesas' Low Energy Solutions Can Help Curb the Spread of COVID-19

With our SmartBond Bluetooth Low Energy portfolio, Renesas is working closely with our customers/partners to develop the solutions needed to support social distancing and contact tracing needs.

SmartBond TINY Module Blog

The SmartBond TINY Module Gets IoT Devices to Market Quicker & Easier Than Ever Before

The SmartBond TINY module boasts a highly configurable, easy-to-use design that empowers customers to quickly and intuitively create highly functional Bluetooth Low Energy connected devices.

Debugging Crosses the Hardware-Software Divide in the IoT Blog

Debugging Crosses the Hardware-Software Divide in the IoT

While a high level of integration and configuration is clearly an enabling factor and one that is delivering massive advancements in product design, it can present engineers with unforeseen issues.

SAR ADCs for High Sampling Rate Applications Blog

SAR ADCs for High Sampling Rate Applications

When looking at applications requiring low latency and low power consumption, the successive approximation register (SAR) ADC provides the best overall solution versus other architectures.

Keyless Future for Drivers

Ask the Experts: How Bluetooth Low Energy is Enabling A Keyless Future for Drivers

In this “Ask the Experts” blog, we look at the current – and future – role and impact that Bluetooth Low Energy (LE) technology will have for cars, drivers and the automotive market in general.

DA14531 is Ready to Connect the Next 1 Billion IoT Devices

Renesas' DA14531 is Ready to Connect the Next 1 Billion IoT Devices

Suited for IoT applications, the SmartBond TINY Bluetooth LE SoC balances a small chip size and power footprint, and boasts performance levels unmatched by anything else on the market.

The Importance of ADCs in the Industrial Internet of Things Blog

The Importance of ADCs in the Industrial Internet of Things

On the SmartEdge platform, the analog front end is the workhorse that converts the analog signals to the digital world. Central to this processing function is the analog-to-digital converter (ADC).

Things to Consider When Developing an ASIC Blog

Things to Consider When Developing an ASIC

Due to the non-homogenous nature of IIoT requirements, one size does not fit all in the IIoT. ASICs offer many advantages to a customer and working with the correct supplier is key to achieving these benefits.