Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Renesas Blog

Certified for G3-Hybrid on CPX3 - Optimal Coverage with PLC or RF

CPX3 Goes “G3-PLC Hybrid”

The R9A06G037 Cool Phoenix 3 Power Line Modem (CPX3) in combination with the RAA604S00 TsuRuGi sub-GHz transceiver has received the certification for the G3-PLC Hybrid specification.

Introducing the RX Family Firmware Update Middleware that can easily realize FOTA (Firmware Update Over-The-Air) implementation

Introducing the RX Family Firmware Update Middleware that Can Easily Realize FOTA (Firmware Update Over-The-Air) Implementation

With the increase in IoT device deployment, the number of inquiries for Over-the-Air firmware updates has been increasing. This blog introduces Firmware Update Over-the-Air middleware for the RX MCU Family.

DSP Experience with RX Family MCU! Visualizing DSP Behavior with Free Sample Program! Blog

DSP Experience with RX Family MCU! Visualizing DSP Behavior with Free Sample Program!

Introducing a low cost and easy way to realize Digital Signal Processing (DSP), which is often thought to be expensive and difficult, with the RX Family of MCUs.

Triac-Based Motor Controller Blog

Cool Off and Reduce Time-to-Market with the Triac-Based Motor Control Solution

Renesas’ triac-based motor controller is a compact air conditioning system solution that offers optimized triac control for a simplified compressor motor control system design.

Model-Based Development Product of Renesas RH850/C1M-Ax Specializing in HEV/EV Motor Control Blog

Model-Based Development Product of Renesas RH850/C1M-Ax Specializing in HEV/EV Motor Control

The model-based development software for Renesas’ RH850/C1M-Ax in-vehicle microcontroller specializes in HEV/EV motor control and is available as in a paid or free version.

Do You Want to Develop a Touchless Button? Introducing a Solution with a General-Purpose MCU Blog

Do You Want to Develop a Touchless Button? Introducing a Solution Using a General-Purpose MCU

To meet the increasing demands for touchless control, Renesas offers a cost-efficient Touchless Button Demo Solution using Renesas microcontrollers with a built-in capacitive touch sensor unit (CTSU).

Renesas’ New R-Car Gen3e Series Upgrades the Popular R-Car Gen3 for Automotive Infotainment, Cockpit and Digital Cluster Blog

Renesas’ New R-Car Gen3e Series Upgrades the Popular R-Car Gen3 for Automotive Infotainment, Cockpit and Digital Cluster

The new R-Car Gen3e series offers a seamless upgrade path from the popular R-Car Gen3 with higher system performance and enhanced integration, fast boot and Functional Safety (FuSa) capabilities.

Try Building an Evaluation Environment for a WVGA LCD Display Using a General-Purpose 32-Bit MCU and a Commercial LCD Panel Blog

Try Building an Evaluation Environment for a WVGA LCD Display Using a General-Purpose 32-Bit MCU and a Commercial LCD Panel

This blog walks through building an evaluation environment for a WVGA display from hardware construction to actual displaying with a commercially available general-purpose MCU kit and a WVGA LCD panel.

Introducing the RX MCU Product Longevity Program (PLP) that Goes Beyond 15 years of Support! Blog

Introducing the RX MCU Product Longevity Program (PLP) that Goes Beyond 15 years of Support!

Looking for a microcontroller that can support you in terms of supply and long life cycle even after 10 years into production? Renesas' RX microcontroller is the right answer for you.

New Automotive High-Definition Link Lowers High-Definition Camera System Costs Blog

New Automotive High-Definition Link Lowers High-Definition Camera System Costs

Introducing the new Automotive High-Definition Link (AHL) that will accelerate the expansion of high-resolution cameras into economy vehicle models.