- Dual-side cooling (DSC) shrinks package footprint by 57% compared with TOLT, packing more power into space-constrained megawatt-scale racks.
- One of the lowest on resistances in the 650V class, at 20 mΩ in an 8x8 mm package.
- Single-source path to 800V designs with industry-standard PQFN footprint plus full controller, driver and MCU lineup. These solutions will be on display at OCP Global Summit in San Jose, CA, October 12-15.
TOKYO, Japan — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today launched the industry's first 650V GaN device with dual-side cooling for high-density power conversion in 800V high-voltage DC (HVDC) AI data center architectures. The new TP65H020G4PLSGBD D-Mode device delivers 20 milliohms (mΩ) on-resistance — one of the lowest in its class — in an ultra-compact, dual-side-cooled (DSC) PQFN package that handles more power in less space. Renesas is currently sampling the device to major AI Datacenter OEMs and ODMs.
Built on its Gen IV Plus GaN architecture, the device is purpose-built for the megawatt-scale demands driving next-generation AI data centers supporting up to 700V operation. It targets the 800V DC/DC intermediate bus converter (IBC) stage that steps down to 48V, 12V or 6V, along with the battery backup (BBU) and capacitor bank (CBU) stages of the sidecar power rack.
As rack power climbs from roughly 120 kW toward megawatt scale, space and heat have become critical factors in sustaining the power level. Unlike conventional top-side-cooled packages, the new device dissipates heat from both top and bottom, lowering top-side thermal impedance by 10%. Its 8 x 8mm PQFN footprint is also 57% smaller than the existing 10 x 15mm TOLT package.
The device incorporates the full strength of Renesas Gen IV Plus 650V GaN technology: low gate charge and output capacitance, a built-in freewheeling diode with minimal reverse recovery and a high threshold voltage that runs without a negative gate bias. Engineers can drive it with a standard silicon gate driver, switch into the MHz frequency range to minimize passive components and cut overall BOM cost without requiring a specialized E-mode driver.
"Customers building megawatt-scale AI data centers are running out of board space and thermal headroom before they hit their power limits," said John Wiggenhorn, Senior Product Line Director of High-Voltage GaN at Renesas. "With the industry's first dual-side-cooled 650V GaN, we cool the device from both sides and cut the footprint significantly, so designers can move more power through the intermediate bus without redrawing the board or adding more cooling hardware. And because it keeps the operational simplicity of the silicon gate drive customers already use, it's an extremely easy upgrade."
The new dual-side-cooled (DSC) PQFN package is defined in collaboration with major AI infrastructure customers, enabling an industry-standard footprint for sourcing flexibility. When paired with Renesas AUX controllers, gate drivers and MCUs, the GaN device creates Renesas a one-stop-shop power solution for OEMs, ODMs and hyperscalers moving to 800V architectures.
Renesas has already validated the approach in silicon. A 6kW, 800V-to-48V LLC DC transformer (DCX) reference design built on the new device and controlled by a Renesas RA6T3 MCU reaches a power density of 2.6 kW/in³ with per-module testing measuring full-load efficiency 0.21% higher than an equivalent TOLT-based board. The smaller package also saves PCB space and enables a better-matched layout across the FETs. 800V-to-12V and 6V DC/DC IBC reference designs also leverage the new DSC 8x8 platform, delivering similar enhanced performance, scalability and power density levels.
Renesas will showcase the new TP65H020G4PLSGBD GaN device as part of its 800V power solutions at OCP Global Summit, October 12-15 in San Jose, California.
Availability
The TP65H020G4PLSGBD is sampling today. Mass production is planned for mid-2027. More information about Renesas GaN solutions is available at: renesas.com/gan-fets.
Get Powered by Renesas
Driven by innovation, quality and reliability, Renesas leads the way in power electronics, shipping more than four billion parts per year from our portfolio of power management ICs, discrete and wide-bandgap GaN products, computing power devices and many more. These products span all major segments including automotive, IoT, infrastructure and industrial applications. Our power portfolio seamlessly attaches to our leading MCU, MPU, SoC and analog solutions, simplifying and accelerating the design process with hundreds of engineering-vetted Winning Combinations and innovative tools such as PowerCompass™ and PowerNavigator™ design software. Find out more at renesas.com/power.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.
(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.