Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Motor Workbench (Analyzer): Status Indicator Tutorial

Motor Workbench (Analyzer): Status Indicator Tutorial
Aug 4, 2022

About This Video

The system notifies you with a change in the rotating light color when a variable matches a user-defined condition (variable + threshold condition)!

  • Multiple variables can be monitored.
  • Multiple conditions can be set for one variable.
  • Information that matches the conditions is displayed as a log on the list screen.