Skip to main content
Renesas Electronics Corporation

RX FIT Tips: How to Operate the CAN API Module Demo Program Using RX671 Start Kit+

RX FIT Tips: How to Operate the CAN API Module Demo Program Using RX671 Start Kit+
Dec 14, 2025

About This Video

Learn how to run the demo program with the CAN API module on RX microcontrollers using the Starter Kit+ for RX671. The CAN API makes it simple to work with the built-in CAN bus interface, and the demo highlights the different modes it supports, including internal loopback, external loopback, and listen-only.